Changelog

Table of Contents

 

New Features

BLE5-Stack

ID Summary
BLE_AGAMA-4952 [SDAA] Expose Reduced Configuration Option to Sysconfig
BLE_AGAMA-4926 [EXAMPLE] Add Examples Support for CC2674-P10

Proprietary RF

ID Summary
PROPRF-1310 Add support for LP_CC2674P10

TI 15.4-Stack

ID Summary
TI154STACK-4483 TI 15.4-Stack FH low power broadcast mode

TI Wi-SUN FAN

ID Summary
WISUN-1170 Enable TCP protocol packet forwarding and passthrough
WISUN-1154 Wi-SUN FAN 1.1 (Wi-SUN FAN 1.0+ Certified)
WISUN-1146 Add support for enabling / disabling external servers in the .cfg file when using the Linux Host
WISUN-1134 Enable Linux NanoStack Host Application for Router node
WISUN-1133 Add RCP examples for CC1311 device family
WISUN-1132 Support custom PHY configuration at runtime
WISUN-1128 WiSUN PHY configuration follows PHY Technical Profile Specification 2V03

TI Wireless Solar Management System

ID Summary
None None

TI Z-Stack

ID Summary
ZIGBEE-2101 Add support for LP_CC2674P10

DMM

ID Summary
DMM-1423 Add support for LP_EM_CC2674P10 for DMM examples
DMM-1416 Add ability to close registered DMM Client
ID Summary
SCCM-422 Generate MCUboot examples for CC2674x10
SCCM-410 Enable image encryption using ECIES for MCUboot
SCCM-409 MCUBoot update from 1.8 to 2.0
SCCM-225 Add SysConfig Support to MCUboot Examples

TI-RTOS and Drivers

ID Summary
TIPOSIX-30 Return error when POSIX timer overflows FreeRTOS ticks
TIDRIVERS-6562 Update GCC version to 12.3
TIDRIVERS-6509 Hide GPIO Configurations in SysConfig module if marked as do not configure.
TIDRIVERS-6464 Add board support for LP_EM_CC2674P10
TIDRIVERS-6342 Add support for 64-bit getSystemTicks API

Radio Software Bundle (RFLib)

ID Summary
RFCORE-1041 CC2674P10: PA Table Update - 10 dBm: Characterized
RFCORE-1042 CC2674P10: PA Table Update - 20 dBm: Characterized
RFCORE-1043 CC1354P: PA Table Update - 20 dBm: Improved Performance
RFCORE-1044 CC1354P: PA Table Update - 10 dBm: Improved Performance
RFCORE-1039 CC1354P: PA Table Update - 5 dBm: Improved Performance
RFCORE-1037 CC1354R10: PA Table Update - 5 dBm: Improved Performance
RFCORE-1040 CC2674R10: PA Table Update - 5 dBm: Characterized

 

Fixed Issues

BLE5-Stack

ID Summary
BLE_AGAMA-4943 Peripheral not checking RPA in CONN_IND packet from Central
BLE_AGAMA-4927 MR stop responding when connecting multiple bonded devices at once
BLE_AGAMA-4907 When Scanning is set to high priority and Advertisement is off, there will be only scan operation, no connection event will be maintained.
BLE_AGAMA-4902 [SWAT][BBR] Basic Broadcaster Fail To Advertise in TIRTOS
BLE_AGAMA-4884 After connecting/disconnecting multiple times, CC26xx will send pin/key missing at the last step of the encryption procedure
BLE_AGAMA-4810 Connection param and channel map update call backs are coming earlier than the actual instant where the change is reflected in the connection causing CM instability
BLE_AGAMA-3427 System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued

Proprietary RF

ID Summary
PROPRF-1310 Add support for LP_CC2674P10

TI 15.4-Stack

ID Summary
TI154STACK-4491 CUI_DISABLE does not exclude all status line prints in the sensor_oad_onchip_secure example
TI154STACK-4490 Joining devices crash when no nearby networks have permit join enabled
TI154STACK-4487 Typo in SBL Binary File Generation section of example readme
TI154STACK-4485 Sysconfig does not support migration from CC1311R3 RGZ to RKP package TI15.4
TI154STACK-4484 There is a memory leak when App sends large packet (more than limited size) or MAC is in bad state
TI154STACK-4482 Zero Data Frame not sent out even though FP bit is set
TI154STACK-4480 aborting RX command even when no RX command has been scheduled after a reset - race condition
TI154STACK-4477 15.4 MAC must clear source matching table entries during MAC_RESET
TI154STACK-4476 Low temp causes radio to fail
TI154STACK-4472 When receiving a broadcast message every 1 s the sleepy sensor is sometimes staying in RX for a full broadcast interval instead of going to sleep after receiving the broadcast message

TI Wi-SUN FAN

ID Summary
WISUN-1198 Fix lower MAC memory leak when ACK with wrong sequence number is received
WISUN-1191 Fix discrepancy between mpx_id in mpx_class_t and llc_message_t.
WISUN-1143 Disable debug GPIO outputs (ENABLE_GPIO_MPL) in out-of-box examples

TI Wireless Solar Management System

ID Summary
None None

TI Z-Stack

ID Summary
ZIGBEE-2089 Fix migration path for CC1354x10RGZ device

DMM

ID Summary
None None
ID Summary
SCCM-403 [nvocmp.c] Compilation warnings due to unused variables
SCCM-402 [BIM] Bootloader fails when using optimization -O0 with TIClang

TI-RTOS and Drivers

ID Summary
TIDRIVERS-6757 UART2 Driver Race Condition on Blocking or Callback Mode Write
TIDRIVERS-6741 CAN examples dereference NULL pointer if UART2_open fails.
TIDRIVERS-6735 UART2_EVENT_TX_BEGIN called several times in one transmit
TIDRIVERS-6709 CAN driver does not provide userArg to event callback
TIDRIVERS-6708 Fix a race condition in SPI DMA (start a new transfer right before the end of the existing transfer)
SYSBIOS-1613 Hwi_construct2 returns ‘0’ as hwi handle for GCC compiler
FREERTOS-37 Lowest interrupt priority is miscalculated

Radio Software Bundle (RFLib)

ID Summary
RFCORE-1036 cc13x4_cc26x4: Non-reentrant code in Coex patch causes IEEE CSMA command to stall indefinitely

 

Known Issues

BLE5-Stack

ID Summary
BLE_AGAMA-4995 [Build][Debug][IAR]-Error For Persistent_app App In CC26X2PSIP Platform: Error[Lp015]: section placement failure: overcommitted content in [0x3'80d0-0x5'5fff]
BLE_AGAMA-4936 When there are two ADV with different RPAs generating from the same IRK, CC2642 can hardly scan the ADVs
BLE_AGAMA-4855 [Multi Connect] CC2651P3 Central fails to connect to more than 5 testers with privacy enable
BLE_AGAMA-4846 [Data Stream][Display] display_printf() is fail when try to print data larger then threshold of 300-500 bytes
BLE_AGAMA-4837 [IOP][Android 14][One Plus 11] With privacy enabled, reconnection fails after after Pairing & Bonding
BLE_AGAMA-4830 [SWAT] Scanner failes after receiving an incorrect event type
BLE_AGAMA-4484 multi_role FreeRTOS support removed from CC13XX / CC26XX
BLE_AGAMA-4354 Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager
BLE_AGAMA-4324 [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar
BLE_AGAMA-4029 Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set.
BLE_AGAMA-4009 [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands
BLE_AGAMA-3896 [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands
BLE_AGAMA-3774 Under certain conditions the CC2652R1 failed to synchronize to periodic advertising
BLE_AGAMA-3752 [CC2651] Host_test memory limitation using CCS+TI-CLANG
BLE_AGAMA-3540 [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC
BLE_AGAMA-3486 Device asserts upon connection when HeapMem and HeapTrack is used
BLE_AGAMA-3381 Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration
BLE_AGAMA-3107 [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms
BLE_AGAMA-3077 [RTLS] CTE reception on the 2M PHY do not meet spec requirements
BLE_AGAMA-3076 [RTLS] CTEs sent on the 2M PHY do not meet spec requirements
BLE_AGAMA-2266 Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms
BLE_AGAMA-2033 [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release)
BLE_AGAMA-1675 IOP: Device fails to pair with Meizu Pro 7
BLE_AGAMA-139 When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection
BLE_AGAMA-80 The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases.

Proprietary RF

ID Summary
None None

TI 15.4-Stack

ID Summary
None None

TI Wi-SUN FAN

ID Summary
None None

TI Wireless Solar Management System

ID Summary
None None

TI Z-Stack

ID Summary
None None

DMM

ID Summary
None None
ID Summary
None None

TI-RTOS and Drivers

ID Summary
TIDRIVERS-7244 Changing the muxing on an IO can cause glitches under some conditions
TIDRIVERS-6863 JSON library unstable for gcc 12.3
TIDRIVERS-4127 ADCBuf causes jitter when switching clock sources
SYSBIOS-642 Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field
SYSBIOS-446 Reported CPU load is not 100% when a task is in “while 1 {}” loop
SYSBIOS-98 Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432

Radio Software Bundle (RFLib)

ID Summary
RFDRIVER-862 RF_ratDispatchTime() doesn't check if RF_currClient is null before derefencing it, causing a fault