OAD Process¶
This section explains the Over-the-Air Download (OAD) process in a proprietary RF application when using the TI BIM bootloader. It explains the available software modules that enable the OAD process.The OAD process can be integrated in a custom RF application. The TI BLE stack and the TI 15.4 stack for CC13xx share the same OAD image format, but implement the update process in different ways.
The following steps are part of the update process:
Creating an OAD-able binary image for the target. This step is identical to OAD with BLE or TI 15.4 Stack.
Uploading the target image to the distributor device.
Reading the firmware version from the remote target.
Downloading the image from the distributor to the target device.
Invoking the BIM and replacing the existing firmware image.
The OAD message protocol between distributor and target is characterized by various requests and responses. The next graph shows all relevant message types:
Figure 77. High-level communication protocol¶
Proprietary RF OAD software architecture¶
The update process involves two participants:
One server device acting as OAD distributor
One or many nodes acting as OAD target
Note
In the Proprietary RF OAD system, the OAD Client refers to the Target side software OAD server refers to the Distributor side software.
There are two tools involved in the oad process:
oad_img_tool.py- Prepares the target image for over the air transferoad_write_bin.py- Writes a target image on to the server’s storage
The OAD distributor buffers new firmware target images using the OAD Storage service. The OAD target responds to the distributor’s requests and may download a new firmware. The firmware is then stored using the OAD Storage service. After the download process, the target invokes the BIM to copy the image to its final position and to boot the new firmware.
The whole Proprietary RF OAD system can be visualized as shown in the figure.
OAD Client¶
The behavior of the OAD client during the OAD process is explained in this state machine.
OAD Client Protocol Functions and Callbacks¶
The functions and callbacks used in the OAD client application is listed in this section. These functions fucntions and callbacks are picked from oad_protocol.h which is included in the project.
/** @brief Function to initialize the OADProtocol_Params struct to its defaults
*
* @param params An pointer to RF_Params structure for
* initialization
*
* Defaults values are:
* pRadioAccessFxns = {0}
* pCallbacks = {0}
*/
extern void OADProtocol_Params_init(OADProtocol_Params_t *params);
/** @brief Function to send a FW version response packet
*
* @param pDstAddress Address to send the response to
* @param fwVersion Firmware version string to send
*
* @return Status
*/
extern OADProtocol_Status_t OADProtocol_sendFwVersionRsp(void* pDstAddress, char *fwVersion);
/** @brief Function to send an OAD image identify request packet
*
* @param pDstAddress Address to send the response to
* @param status status to send
*
* @return Status
*/
extern OADProtocol_Status_t OADProtocol_sendOadIdentifyImgRsp(void* pDstAddress, uint8_t status);
/** @brief Function to send an OAD block request packet
*
* @param pDstAddress Address to send the request to
* @param imgId image ID of image blocks
* @param blockNum block Number to request
* @param multiBlockSize Numer of blocks in the multi Block transfer (0 or 1 for none-multiblock)
*
* @return Status
*
*/
extern OADProtocol_Status_t OADProtocol_sendOadImgBlockReq(void* pDstAddress, uint8_t imgId, uint16_t blockNum, uint16_t multiBlockSize);
/** @brief Function to send a OAD reset response packet
*
* @param pDstAddress Address to send the response to
*
* @return Status
*/
extern OADProtocol_Status_t OADProtocol_sendOadResetRsp(void* pDstAddress);
OAD Server¶
The behavior of the OAD server during the OAD process is explained in this state machine.
OAD Server Protocol Functions and Callbacks¶
The functions and callbacks used in the OAD server application is listed in this section These functions fucntions and callbacks are picked from oad_protocol.h which is included in the project.
/** @brief Function to initialize the OADProtocol_Params struct to its defaults
*
* @param params An pointer to RF_Params structure for
* initialization
*
* Defaults values are:
* pRadioAccessFxns = {0}
* pCallbacks = {0}
*/
extern void OADProtocol_Params_init(OADProtocol_Params_t *params);
/** @brief Function to send a FW version request packet
*
* @param pDstAddress Address to send the request to
*
* @return Status
*/
extern OADProtocol_Status_t OADProtocol_sendFwVersionReq(void* pDstAddress);
/** @brief Function to send an OAD image identify request packet
*
* @param pDstAddress Address to send the request to
* @param imgId image ID used for requesting image blocks
* @param pImgInfoData Image header
*
* @return Status
*/
extern OADProtocol_Status_t OADProtocol_sendImgIdentifyReq(void* pDstAddress, uint8_t imgId, uint8_t *pImgInfoData);
/** @brief Function to send an OAD image identify request packet
*
* @param pDstAddress Address to send the response to
* @param status status to send
*
* @return Status
*/
extern OADProtocol_Status_t OADProtocol_sendOadIdentifyImgRsp(void* pDstAddress, uint8_t status);
OAD Storage¶
The OAD storage module provides the APIs to store and retrieve images and version number of images from flash memory. The APIs are used in both the server and the client oad projects. These functions fucntions and callbacks are picked from oad_storage.h which is included in the project.
/*********************************************************************
* @fn OADStorage_init
*
* @brief Initialise the OAD Target Profile.
*
* @param None.
*
* @return None.
*/
extern void OADStorage_init(void);
/*********************************************************************
* @fn OADStorage_imgIdentifyRead
*
* @brief Read Image header and return number of blocks.
*
* @param imageType - image type indicating which image to read
* @param pImgHdr - pointer to image header data
*
* @return Total Blocks if image accepted, 0 if Image invalid
*/
uint16_t OADStorage_imgIdentifyRead(uint8_t imageType, OADStorage_imgIdentifyPld_t* pImgId);
/*********************************************************************
* @fn OADStorage_imgIdentifyWrite
*
* @brief Process the Image Identify Write. Determine from the received OAD
* Image Header if the Downloaded Image should be acquired.
*
* @param pValue - pointer to data to be written
*
* @return Total Blocks if image accepted, 0 if Image rejected
*/
extern uint16_t OADStorage_imgIdentifyWrite(uint8_t *pValue);
/*********************************************************************
* @fn OADStorage_imgBlockRead
*
* @brief Read Image Block.
*
* @param blockNum - block number to be written
* @param pBlockData - pointer for data to be read
*
* @return none
*/
extern void OADStorage_imgBlockRead(uint16_t blockNum, uint8_t *pBlockData);
/*********************************************************************
* @fn OADStorage_imgInfoRead
*
* @brief Read an Image info.
*
* @param pimgInfo - pointer for data to be read
*
* @return none
*/
extern void OADStorage_imgInfoRead(uint8_t *pimgInfo);
/*********************************************************************
* @fn OADStorage_imgBlockWrite
*
* @brief Write Image Block.
*
* @param blockNum - block number to be written
* @param pBlockData - pointer to data to be written
* @param len - length fo block
*
* @return status
*/
extern uint8_t OADStorage_imgBlockWrite(uint32_t blockNum, uint8_t *pBlockData, uint8_t len);
/*********************************************************************
* @fn OADStorage_eraseImgPage
*
* @brief Erases an Image page. Note this is only needed if an image
* page has been corrupted typically OADStorage_imgBlockWrite
* pre-erase all pages
*
* @param none
*
* @return OADStorage_Status_t
*/
extern OADStorage_Status_t OADStorage_eraseImgPage(uint32_t page);
/*********************************************************************
* @fn OADStorage_imgFinalise
*
* @brief Process the Image Block Write.
*
* @param none
*
* @return status
*/
extern OADStorage_Status_t OADStorage_imgFinalise(void);
/*********************************************************************
* @fn OADStorage_close
*
* @brief Releases the resource required for OAD stoarage.
*
* @param none
*
* @return none
*/
extern void OADStorage_close(void);