Amazon Sidewalk Quick Start Guide

This section serves as a road map for users developing applications and products using the TI SimpleLink CC13xx or CC26xx wireless MCU platform for Sidewalk applications. Whether a seasoned developer or just getting started, TI has created a variety of resources to simplify development on the CC13xx or CC26xx platform. These resources will enhance your experience with the Sidewalk stack from the out-of-the-box demo to production.

Figure 136. shows the suggested workflow for getting started with the Sidewalk development environment.

../_images/sidewalk-suggestedworkflow.png

Figure 136. Suggested Workflow

If you have already evaluated Sidewalk in the past, you can skip most of the following section and skip directly to the Flashing the edge device section. If not, please read about Sidewalk on Amazon’s website and follow the guide thoroughly.

Prerequisites

Hardware

Software

FreeRTOS installation

Download FreeRTOSv202104.00 from GitHub. Copy the FreeRTOSv202104.00 folder contained in the archive to, for instance, C:/. We now want to let Code Composer Studio where FreeRTOS is installed. To do so, in Code Composer Studio, go to Window -> Preferences. Once the window opens, on the left most menu, click on Code Composer Studio* -> **Build -> Variables. Click on Add…. Now fill in the information as follows:

  • Variable FREERTOS_INSTALL_DIR

  • Type: Path

  • Value: path to the FreeRTOS folder you extracted

../_images/sidewalk-freertos-ccs-var.png

Figure 137. FREERTOS_INSTALL_DIR variable configuration.

FreeRTOS is now installed in Code Composer Studio.

Get started

Once you have gathered the required components, you can evaluate Sidewalk through the TI Amazon Sidewalk Sample IoT App. This app will provide you with prebuilt firmware so that you can focus on learning more about Sidewalk. It should take you around 1 hour to follow that tutorial. Please return to this quick start guide when it is time to flash the binaries you have generated, as it provides more in-depth instructions on how to flash the edge devices.

Flashing the edge device

The provisioning script should now have generated one folder containing binary personalisation data. Open UniFlash and create a new session. Now go to Settings & Utilities, and under Manual Erase, click on Erase Entire Flash. Once the mass erase is finished, it is now time to flash the following two binaries, in that order:

  1. Under EdgeDeviceProvisioning/DeviceProfile_xxxxxx/WirelessDevice_xxxx, please select the TI.bin binary. Check Binary and set Load Addr: to 0xAE000 (0x56000 for P1 devices).

  2. Under EdgeDeviceBinaries/ti/, please select either binary:

    • ble_sid_demo_cc1352p7_asl.hex is using the BLE (2.4 GHz frequency band).

    • fsk_sid_demo_cc1352p7_asl.hex is using FSK (900 MHz frequency band)

Note

You can use both fsk and ble binaries for that demo. The Web app will display the medium used.

Here is a recapitulative of what your UniFlash window is supposed to look like.

../_images/sidewalk-uniflash-2bins.png

Figure 138. UniFlash window after the instructions have been followed correctly.

If it looks like that, click Load Images. Once the edge device has been flashed with the 2 aforementioned binary files, please proceed immediately to the next section.

Checking debug logs

Open a serial console, such as PuTTY with the following parameters:

UART Param

Default Values

Baud Rate

921600

Data length

8 bits

Parity

None

Stop bits

1 bit

Flow Control

None

Now, please reset your CC13xx or CC26xx LaunchPad. You should now see similar data logs in the console.

[00000000003] <info> Sidewalk example started
[00000002368] <info> DR state [3]
[00000002420] <info> status changed: 1
[00000002420] <info> Registration Status = 0, Time Sync Status = 1 and Link Status Mask = 0
[00000002420] <info> Link 0 Mode 0
[00000002421] <info> Link 1 Mode 0
[00000002421] <info> Link 2 Mode 0
[00000005871] <info> ama_gateway_set_state Gateway [01 47] state changing from 0 to 1
[00000005906] <info> New Rx S:0 T:0
[00000005906] <info> Rx S:0 T:0 (5/5)
[00000005907] <info> Tx Start (6)
[00000005908] <info> Tx S:0 T:0 (0) I:0
[00000005910] <info> Delete rx_buffer :: Gateway [01 47] :: Stream [0] :: Transaction [0]
[00000005934] <info> New Rx S:0 T:1
[00000005934] <info> Rx S:0 T:1 (5/5)
[00000005935] <info> Tx Start (6)
[00000005935] <info> Tx S:0 T:1 (0) I:0
[00000005937] <info> Delete rx_buffer :: Gateway [01 47] :: Stream [0] :: Transaction [1]
[00000005975] <info> New Rx S:0 T:2
[00000005975] <info> Rx S:0 T:2 (5/5)
[00000005976] <info> Tx Start (9)
[00000005976] <info> Tx S:0 T:2 (0) I:0
[00000005978] <info> Delete rx_buffer :: Gateway [01 47] :: Stream [0] :: Transaction [2]
[00000005985] <info> ama_gateway_set_state Gateway [01 47] state changing from 1 to 2
[00000005985] <info> [MET] B:200 N:0
[00000006017] <info> New Rx S:7 T:0
[00000006018] <info> Rx S:7 T:0 (55/55)
[00000006021] <info> RX CRID: 00000000245E6B04C8
[00000006021] <info> [PAD]DL:0
[00000006021] <info> DEC: M:7 [0:108:3]
[00000006021] <info> on_recv_ready [CMD:0:108:3]
[00000006021] <info> on_recv_ready [RT:LOCAL]
[00000006022] <info> Updated time: 1366506644.580169
[00000006022] <info> [MET] B:200 N:0
[00000006022] <info> SID_API: Unknown Sender Using cloud address
[00000006022] <info> status changed: 0
[00000006023] <info> Registration Status = 0, Time Sync Status = 0 and Link Status Mask = 1
[00000006023] <info> Link 0 Mode 1
[00000006023] <info> Link 1 Mode 0
[00000006023] <info> Link 2 Mode 0
[00000006025] <info> Time Sync Counter = 2
[00000006025] <info> RESP_TIME: remote_drift[0 secs] curr_drift[-1 secs]
[00000006026] <info> Delete rx_buffer :: Gateway [01 47] :: Stream [7] :: Transaction [0]
[00000006062] <info> ama_gateway_set_state Gateway [01 47] state changing from 2 to 0
[00000006073] <info> [MET] B:0 N:0
[00000006073] <info> status changed: 1
[00000006073] <info> Registration Status = 0, Time Sync Status = 0 and Link Status Mask = 0
[00000006074] <info> Link 0 Mode 0
[00000006074] <info> Link 1 Mode 0
[00000006074] <info> Link 2 Mode 0

Next steps

Now that your setup is functional, you can check out the sid_demo example, located in the SDK, and start building your application upon it using the SimpleLink CC13xx/CC26xx SDK.