Execution flow of MCUBoot Based Proprietary RF OAD¶
This section briefly describes how the MCUBoot and the Client application work together to enable OAD functionality.
When using the MCUBoot, there is no need for a peristent app, since the slots for incoming image and existing image are predefined.
The functional flow of an On-chip Flash OAD process is shown in the diagram.

Note
Proprietary RF OAD uses the overwrite method of managing images on Flash. The newly updated image is overwritten onto the primary slot and then executed from the primary slot.