Changelog
Table of Contents
New Features
BLE5-Stack
ID | Summary |
---|---|
BLE_AGAMA-4952 | [SDAA] Expose Reduced Configuration Option to Sysconfig |
BLE_AGAMA-4926 | [EXAMPLE] Add Examples Support for CC2674-P10 |
Proprietary RF
ID | Summary |
---|---|
PROPRF-1310 | Add support for LP_CC2674P10 |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-4457 | Add migration support for CC2674P10 |
TI154STACK-4445 | Support for MCUBoot 2.0 |
TI154STACK-4443 | Add NV erase CUI message and update BTN/GPIO documentation |
TI154STACK-4442 | Support CC2674P10 device and stack examples |
TI154STACK-4440 | Support CC1354R10RGZ device migration |
TI154STACK-4429 | Implement SILK TI Logging in MAC and application examples |
TI Wi-SUN FAN
ID | Summary |
---|---|
WISUN-1016 | Support for MCUBoot 2.0 |
WISUN-1009 | Allow External Linux Radius Servers to be used for Wi-SUN networks |
WISUN-997 | Allow External Linux DHCP Servers to be used for Wi-SUN networks |
WISUN-991 | Implement network profile Sysconfig configurations |
WISUN-943 | Add wfantund and wfanctl support for router nodes |
TI Wireless Solar Management System
ID | Summary |
---|---|
None | None |
TI Z-Stack
ID | Summary |
---|---|
ZIGBEE-2101 | Add support for LP_CC2674P10 |
DMM
ID | Summary |
---|---|
DMM-1423 | Add support for LP_EM_CC2674P10 for DMM examples |
DMM-1416 | Add ability to close registered DMM Client |
SimpleLink Common Components Module (SCCM)
ID | Summary |
---|---|
SCCM-422 | Generate MCUboot examples for CC2674x10 |
SCCM-410 | Enable image encryption using ECIES for MCUboot |
SCCM-409 | MCUBoot update from 1.8 to 2.0 |
SCCM-225 | Add SysConfig Support to MCUboot Examples |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIPOSIX-30 | Return error when POSIX timer overflows FreeRTOS ticks |
TIDRIVERS-6562 | Update GCC version to 12.3 |
TIDRIVERS-6509 | Hide GPIO Configurations in SysConfig module if marked as do not configure. |
TIDRIVERS-6464 | Add board support for LP_EM_CC2674P10 |
TIDRIVERS-6342 | Add support for 64-bit getSystemTicks API |
Radio Software Bundle (RFLib)
ID | Summary |
---|---|
RFCORE-1037 | CC1354R10: PA Table Update - 5 dBm: Improved Performance |
RFCORE-1040 | CC2674R10: PA Table Update - 5 dBm: Characterized |
RFCORE-1043 | CC1354P: PA Table Update - 20 dBm: Improved Performance |
RFCORE-1041 | CC2674P10: PA Table Update - 10 dBm: Characterized |
RFCORE-1042 | CC2674P10: PA Table Update - 20 dBm: Characterized |
RFCORE-1044 | CC1354P: PA Table Update - 10 dBm: Improved Performance |
RFCORE-1039 | CC1354P: PA Table Update - 5 dBm: Improved Performance |
Fixed Issues
BLE5-Stack
ID | Summary |
---|---|
BLE_AGAMA-4943 | Peripheral not checking RPA in CONN_IND packet from Central |
BLE_AGAMA-4927 | MR stop responding when connecting multiple bonded devices at once |
BLE_AGAMA-4907 | When Scanning is set to high priority and Advertisement is off, there will be only scan operation, no connection event will be maintained. |
BLE_AGAMA-4902 | [SWAT][BBR] Basic Broadcaster Fail To Advertise in TIRTOS |
BLE_AGAMA-4884 | After connecting/disconnecting multiple times, CC26xx will send pin/key missing at the last step of the encryption procedure |
BLE_AGAMA-4810 | Connection param and channel map update call backs are coming earlier than the actual instant where the change is reflected in the connection causing CM instability |
BLE_AGAMA-3427 | System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued |
Proprietary RF
ID | Summary |
---|---|
PROPRF-1310 | Add support for LP_CC2674P10 |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-4439 | Beacon response corrupted with16+ indirect pending messages |
TI154STACK-4434 | Crash during PA switching in LNT environment on CC2652P device |
TI154STACK-4433 | Collector polling interval not updated on WB-DSSS custom PHY |
TI154STACK-4428 | With multiple collectors, sensor may join collector with incorrect PANID |
TI154STACK-4410 | Description of max devices field in SysConfig is incorrect |
TI154STACK-4360 | FH broadcast interval cannot be set to more than 130 seconds |
TI Wi-SUN FAN
ID | Summary |
---|---|
WISUN-1034 | CoAP service 1 sec periodic timer does not trigger |
WISUN-1015 | Not possible to migrate to CC1314R10RGZ |
WISUN-1013 | ns_trace may crash program due to unchecked boundaries |
WISUN-1001 | Wi-SUN stack uses incorrect trace pins on CC1354P10_1 and CC1354P10_6 |
WISUN-996 | Invalid channels may be used at end of US-IE excluded channel range |
WISUN-994 | BZ PHY uses wrong channels when configured to use channels 90-128 |
WISUN-990 | Enabling minTxOff for JP PHY fixed channel mode causes async cnf to not be sent |
WISUN-967 | dodagroute pyspinel command fails to complete when called repeatedly |
TI Wireless Solar Management System
ID | Summary |
---|---|
None | None |
TI Z-Stack
ID | Summary |
---|---|
ZIGBEE-2089 | Fix migration path for CC1354x10RGZ device |
DMM
ID | Summary |
---|---|
None | None |
SimpleLink Common Components Module (SCCM)
ID | Summary |
---|---|
SCCM-403 | [nvocmp.c] Compilation warnings due to unused variables |
SCCM-402 | [BIM] Bootloader fails when using optimization -O0 with TIClang |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-6757 | UART2 Driver Race Condition on Blocking or Callback Mode Write |
TIDRIVERS-6741 | CAN examples dereference NULL pointer if UART2_open fails. |
TIDRIVERS-6735 | UART2_EVENT_TX_BEGIN called several times in one transmit |
TIDRIVERS-6709 | CAN driver does not provide userArg to event callback |
TIDRIVERS-6708 | Fix a race condition in SPI DMA (start a new transfer right before the end of the existing transfer) |
SYSBIOS-1613 | Hwi_construct2 returns ‘0’ as hwi handle for GCC compiler |
FREERTOS-37 | Lowest interrupt priority is miscalculated |
Radio Software Bundle (RFLib)
ID | Summary |
---|---|
RFCORE-1036 | cc13x4_cc26x4: Non-reentrant code in Coex patch causes IEEE CSMA command to stall indefinitely |
Known Issues
BLE5-Stack
ID | Summary |
---|---|
BLE_AGAMA-4995 | [Build][Debug][IAR]-Error For Persistent_app App In CC26X2PSIP Platform: Error[Lp015]: section placement failure: overcommitted content in [0x3'80d0-0x5'5fff] |
BLE_AGAMA-4936 | When there are two ADV with different RPAs generating from the same IRK, CC2642 can hardly scan the ADVs |
BLE_AGAMA-4855 | [Multi Connect] CC2651P3 Central fails to connect to more than 5 testers with privacy enable |
BLE_AGAMA-4846 | [Data Stream][Display] display_printf() is fail when try to print data larger then threshold of 300-500 bytes |
BLE_AGAMA-4837 | [IOP][Android 14][One Plus 11] With privacy enabled, reconnection fails after after Pairing & Bonding |
BLE_AGAMA-4830 | [SWAT] Scanner failes after receiving an incorrect event type |
BLE_AGAMA-4484 | multi_role FreeRTOS support removed from CC13XX / CC26XX |
BLE_AGAMA-4354 | Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager |
BLE_AGAMA-4324 | [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar |
BLE_AGAMA-4029 | Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set. |
BLE_AGAMA-4009 | [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands |
BLE_AGAMA-3896 | [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands |
BLE_AGAMA-3774 | Under certain conditions the CC2652R1 failed to synchronize to periodic advertising |
BLE_AGAMA-3752 | [CC2651] Host_test memory limitation using CCS+TI-CLANG |
BLE_AGAMA-3540 | [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC |
BLE_AGAMA-3486 | Device asserts upon connection when HeapMem and HeapTrack is used |
BLE_AGAMA-3381 | Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration |
BLE_AGAMA-3107 | [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms |
BLE_AGAMA-3077 | [RTLS] CTE reception on the 2M PHY do not meet spec requirements |
BLE_AGAMA-3076 | [RTLS] CTEs sent on the 2M PHY do not meet spec requirements |
BLE_AGAMA-2266 | Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
Proprietary RF
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
None | None |
TI Wi-SUN FAN
ID | Summary |
---|---|
None | None |
TI Wireless Solar Management System
ID | Summary |
---|---|
None | None |
TI Z-Stack
ID | Summary |
---|---|
None | None |
DMM
ID | Summary |
---|---|
None | None |
SimpleLink Common Components Module (SCCM)
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-7070 | CRC post-build step fails if folder-name contains spaces |
TIDRIVERS-6863 | JSON library unstable for gcc 12.3 |
SYSBIOS-642 | Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field |
SYSBIOS-446 | Reported CPU load is not 100% when a task is in “while 1 {}” loop |
SYSBIOS-98 | Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432 |
FREERTOS-8 | Tasks view in ROV for FreeRTOS does not show if a task is blocked on a semaphore or mutex |
Radio Software Bundle (RFLib)
ID | Summary |
---|---|
RFDRIVER-862 | RF_ratDispatchTime() doesn't check if RF_currClient is null before derefencing it, causing a fault |