SimpleLink™ CC13xx CC26xx SDK 8.30.00.121 Release Notes
Table of Contents
Introduction
The SimpleLink™ Low Power F2 Software Development Kit (SDK), formerly known as the CC13xx and CC26xx SDK, delivers components that enable engineers to develop applications on the Texas Instruments SimpleLink CC13xx and CC26xx family of wireless microcontrollers (MCUs). This software toolkit provides a cohesive and consistent software experience for all SimpleLink CC13xx and CC26xx wireless MCU users by packaging essential software components, such as a Bluetooth® Low Energy (BLE) protocol stack supporting Bluetooth 5.2, Zigbee 3.0 compliant protocol suite, RF-Proprietary examples, TI’s 15.4 Stack, TI Wi-SUN FAN Stack, Amazon Sidewalk examples, as well as the TI-RTOS7 and FreeRTOS™ kernels and TI Drivers in one easy-to-use software package along with example applications and documentation. In addition, the Dynamic Multi-Protocol Manager (DMM) software component enables multiprotocol development on a single SimpleLink wireless MCU.
Although not included in the SDK, SimpleLink CC13xx and CC26xx wireless MCUs are also capable of supporting the following wireless solutions: Please refer to their respective repositories for resources and more information.
- The Matter standard: https://github.com/TexasInstruments/matter
- Thread 1.1.1 networking stack based on OpenThread: https://github.com/TexasInstruments/ot-ti
The SimpleLink MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth Low Energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit allows you to reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.
This is version 8.30.00.121 of the SimpleLink Low Power F2 SDK. This SDK is also available on GitHub at https://github.com/TexasInstruments/simplelink-lowpower-f2-sdk
Documentation
What’s New
- Example projects and RF settings for the upcoming CC2674P10 LaunchPad™ development kit for SimpleLink multi-standard wireless MCU.
- CCS Theia, now supports all SimpleLink F2 devices. Please use version 1.5.0 or newer. For more information, see Upcoming Features.
- The new TI Log driver simplifies adding log statements to your application without compromising on memory or processing power. The following SW modules are instrumented: Power driver, UART2 driver, TI 15.4-Stack.
- The Wi-SUN gateway example for Linux, wfantund, now supports using external authentication server and/or external DHCP server. It also supports Router Node configuration for the first time.
- The TI Wi-SUN Stack has three new Network Profiles which simplify network configuration.
- MCUboot is updated to version 2.0 and now supports using an encrypted image. You can now configure MCUboot in SysConfig.
- DMM now supports closing a handle, opening the possibility of using more than two handles in one application.
Refer to the Document Overview for the individual release notes and details for starting development with each SDK component.
Refer to the included Change Log for a summary of new features and fixed issues since the last SDK release.
If you want to download or install a subset of the SimpleLink F2 SDK components, please use SDK composer on TI Resource Explorer. This feature lets you select only the SDK components you need and save up to 1.1 GB on the installation size.
- Navigate to this SDK on TI Resource Explorer
- In the left panel containing the folder tree, hover over the SDK. This displays three dots.
- Click on the three dots and then on download. Now, select only the components you need!
Upcoming Features
We are thrilled to announce the release of Code Composer Studio v20, the culmination of years of dedication and hard work from our team! This release represents a significant milestone in our journey to provide best-in-class IDEs for our customers. CCS is now based on the Theia framework, which allows us to provide a ‘VS Code’ like experience for both desktop and cloud – a first in the embedded industry! CCSv20 supersedes the CCSv12.8 release stream for all supported TI Devices. No further releases of the Eclipse based product are planned, see the Transition Roadmap for more details. CCSv20 downloads can be accessed from the ti.com tools folder: https://www.ti.com/tool/download/CCSTUDIO Documentation and Video collateral to support the release can be found here:
- Getting Started Video
- CCS Academy
- Migration Guide
- CCS User’s Guide
- Getting Started Video
- Quick Tip Videos
We recommend customers who are starting new development programs to leverage CCS Theia from the start, and existing users of CCS Eclipse to take the time to transition to CCS Theia, see Migration Guide for help migrating from CCS Eclipse IDE to CCS Theia IDE.
Please note the following features are not yet supported in CCS Theia:
- TI RTOS Run-time Object Viewer (ROV)
- Energy Trace running without an active debug session
Upgrade and Compatibility Information
- If you want to migrate from one device to another within the same SDK, you can use the SysConfig Migration Tool. Learn more about it in the Migration documentation.
GPIO_setMux()has been deprecated for being unsafe regarding pin output stability when called under certain conditions. It has been replaced byGPIO_setConfigAndMux()which applies a pin configuration and mux setting at the same time.
Operating System Support
- Windows® Windows 10
- Ubuntu 20.04 LTS 64-bit
- macOS 13.x
Dependencies
SimpleLink Low Power F2 SDK 8.30.00.121 was built & tested on a Windows host platform using the following Integrated Development Environments (IDEs) and components. Using an IDE or toolchain version not listed below may result in compatibility issues with this SDK release. Refer to the individual component release notes in the Document Overview for each component’s supported code generation tools. CCS Theia 1.5.0 does not include TI Clang v. 3.2.2 LTS which is needed for this SDK. TI Clang v. 3.2.2 LTS can be downloaded separately: https://www.ti.com/tool/download/ARM-CGT-CLANG
- IAR Embedded Workbench: EWARM-9.60.2
- TI Code Composer Studio: CCS-12.8.0
- CCS Theia: 1.5.0
- TI ARM Clang Compiler tools: 3.2.2.LTS
- XDCTools: 3.62.01.15
- ARM GCC: gcc-arm-none-eabi-9-2019-q4-major
- SysConfig Standalone tool for IAR IDE: 1.21.1
FreeRTOS: 202104.00. Please note that FreeRTOS source now ships with the SDK installer
Amazon Sidewalk examples should be built with GCC 12.3
Device Support
This SDK supports the following SimpleLink CC13xx and CC26xx wireless MCUs:
| Sub-1GHz Devices | 2.4GHz Devices | Dual Band Devices |
|---|---|---|
| CC1311P3 | CC2642R | CC1352P |
| CC1311R3 | CC2642R-Q1 | CC1352P7 |
| CC1312R | CC2651P3 | CC1352R |
| CC1312R7 | CC2651R3 | CC1354P10 |
| CC1312PSIP | CC2652P | CC1354R10 |
| CC1314R10 | CC2652P7 | |
| CC2652R | ||
| CC2652RB | ||
| CC2652R7 | ||
| CC2652RSIP | ||
| CC2652PSIP | ||
| CC2651RS3IPA | ||
| CC2674R10 | ||
| CC2674P10 |
Development Board Support
The following table lists the supported development boards for each device supported in this SDK. Note: LaunchPad™ Development kits are not available for all device variants. As such, alternative options for development are presented in this table.
A Modular LaunchPad™ must be used together with the Modular LaunchPad™ Emulator (an LP-XDS110 or LP-XDS110ET).
Known Issues
- It is not possible to re-build the TF-M secure image. It is provided as a binary in the SDK.
- For all SDK components, the importing of IAR projects through dev.ti.com is currently not supported
- Refer to the Document Overview for known issues and limitations as published in each SDK component’s release notes
Versioning
This product follows a version format, M.mm.pp.bb, where:
- M is a 1 digit major number,
- mm is a 2 digit minor number,
- pp is a 2 digit patch number,
- bb is a 2 digit incrementing build counter.