References¶
TI Wi-SUN FAN-Stack User’s Guide
Terms and Acronyms¶
Wireless Solar Management System Terms and Acronyms¶
General Terms and Acronyms¶
- CCFG¶
- Customer Configuration¶
- Customer Configuration Area¶
Customer Configuration is set by the application and contains configuration parameters for the ROM boot code, device hardware, and device firmware. It contains lock-bits on the last page of flash. You can read more in the Customer Configuration section in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- CCS¶
- Code Composer Studio¶
An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio
- cJTAG¶
- compact JTAG¶
Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG.
- GCC¶
- GNU Compiler Collection¶
A compiler system produced by the GNU Project, which support various programming languages such as C and C++.
- GPRAM¶
- General purpose RAM¶
This memory area is used for the cache per default, but can be configured to be used as RAM.
- IAR¶
Refers to IAR Systems’ IAR Embedded Workbench, which is an integrated development environment used for building and debugging embedded applications.
- JTAG¶
- Joint Test Action Group¶
IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG.
- MCU¶
- Microcontroller Unit¶
A small computer on a single integrated circuit.
- NVS¶
- Non-Volatile Storage¶
Storage of data in non-volatile memory (NVM). NVM retains saved data during power cycles. In the context of CC13xx and CC26xx devices, NVM either refers to the internal flash or some external flash.
- ROM¶
- Read-only Memory¶
Type of non-volatile memory used in computers. Once data is written to ROM, the data cannot be removed and can only be read.
- RTSC¶
- Real Time Software Components¶
A toolset for creating reusable code, used by TI-RTOS. See RTSC and RTSC-Pedia.
- SysConfig¶
- System Configuration Tool¶
SysConfig is a graphical interface for configuring software projects. Configuration files, C source files and header files are generated based on the parameters configured in the SysConfig dashboard. See sysconfig-sysconfig.
- TI-CLANG¶
- TI Arm Clang Compiler Toolchain¶
The TI Arm Clang Compiler Toolchain (tiarmclang) is the next generation TI Arm compiler, replacing the previous TI Arm Compiler Tools (armcl). You can use the tiarmclang compiler toolchain to build applications from C, C++, and/or assembly source files to be loaded and run on one of the Cortex-M or Cortex-R Arm processors that are supported by the toolchain. You can find more information here.
- VIMS¶
- Versatile Instruction Memory System¶
A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- .bss¶
Block started by symbol. This memory section usually contains uninitialized variables including the task stacks.