39 #ifndef ti_drivers_TRNG_TRNGCC26X4_ns__include 40 #define ti_drivers_TRNG_TRNGCC26X4_ns__include 64 } TRNGCC26X4_ns_Object;
Definition: TRNGCC26X4_s.h:80
TRNG Global configuration.
Definition: TRNG.h:328
Definition: TRNGCC26X4_s.h:89
void(* TRNG_CryptoKeyCallbackFxn)(TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy)
The definition of a callback function used by the TRNG driver when TRNG_generateKey() is called with ...
Definition: TRNG.h:394
TRNG_ReturnBehavior
The way in which TRNG function calls return after generating the requested entropy.
Definition: TRNG.h:363
int_fast16_t TRNGCC26XX_setSamplesPerCycle(TRNG_Handle handle, uint32_t samplesPerCycle)
Sets the number of entropy generation cycles before the results are returned.
SemaphoreP structure.
Definition: SemaphoreP.h:84
void(* TRNG_RandomBytesCallbackFxn)(TRNG_Handle handle, int_fast16_t returnValue, uint8_t *randomBytes, size_t randomBytesSize)
The definition of a callback function used by the TRNG driver when TRNG_getRandomBytes() is called wi...
Definition: TRNG.h:409