690 #ifndef ti_drivers_spi_SPICC26X4DMA__include 691 #define ti_drivers_spi_SPICC26X4DMA__include 739 #define SPICC26X4DMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 748 #define SPICC26X4DMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 756 #define SPICC26X4DMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 763 #define SPICC26X4DMA_CMD_CLEAR_CSN_PIN (SPI_CMD_RESERVED + 3) 778 #define SPICC26X4DMA_CMD_SET_MANUAL (SPI_CMD_RESERVED + 4) 789 #define SPICC26X4DMA_CMD_CLR_MANUAL (SPI_CMD_RESERVED + 5) 801 #define SPICC26X4DMA_CMD_MANUAL_START (SPI_CMD_RESERVED + 6) 822 #define SPICC26X4DMA_CMD_SET_SAMPLE_DELAY (SPI_CMD_RESERVED + 7) 827 #define SPICC26X4DMA_RETURN_PARTIAL_ENABLE SPICC26X4DMA_CMD_RETURN_PARTIAL_ENABLE 828 #define SPICC26X4DMA_RETURN_PARTIAL_DISABLE SPICC26X4DMA_CMD_RETURN_PARTIAL_DISABLE 829 #define SPICC26X4DMA_SET_CSN_PIN SPICC26X4DMA_CMD_SET_CSN_PIN volatile tDMAControlTable * dmaTxTableEntryPri
Definition: SPICC26X4DMA.h:959
Definition: SPICC26X4DMA.h:850
uint32_t baseAddr
SPI Peripheral's base address.
Definition: SPICC26X4DMA.h:925
uint_least8_t csnPin
Definition: SPICC26X4DMA.h:981
HwiP structure.
Definition: HwiP.h:78
Serial Peripheral Interface (SPI) Driver Interface.
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:587
SPICC26X4DMA Object.
Definition: SPICC26X4DMA.h:992
uint8_t intNum
Definition: SPICC26X4DMA.h:927
SPICC26X4DMA_ReturnPartial returnPartial
Definition: SPICC26X4DMA.h:1024
PowerCC26XX_Resource powerMngrId
Definition: SPICC26X4DMA.h:951
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:624
volatile tDMAControlTable * dmaRxTableEntryAlt
Definition: SPICC26X4DMA.h:965
Definition: SPICC26X4DMA.h:864
Definition: SPICC26X4DMA.h:851
int32_t txPinMux
Definition: SPICC26X4DMA.h:967
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:253
Power manager interface for CC26XX/CC13XX.
uint8_t intPriority
SPI CC26X4DMA Peripheral's interrupt priority.
Definition: SPICC26X4DMA.h:942
int32_t clkPinMux
Definition: SPICC26X4DMA.h:971
uint32_t bitRate
Definition: SPICC26X4DMA.h:1011
UDMACC26XX_Handle udmaHandle
Definition: SPICC26X4DMA.h:1003
uint32_t transferTimeout
Definition: SPICC26X4DMA.h:1013
Semaphore module for the RTOS Porting Interface.
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:713
int32_t csnPinMux
Definition: SPICC26X4DMA.h:973
SPICC26X4DMA Hardware attributes.
Definition: SPICC26X4DMA.h:922
SPICC26X4DMA_ReturnPartial
Definition: SPICC26X4DMA.h:861
volatile tDMAControlTable * dmaTxTableEntryAlt
Definition: SPICC26X4DMA.h:963
uint8_t format
Definition: SPICC26X4DMA.h:1022
SPI_Transaction * completedTransfers
Definition: SPICC26X4DMA.h:1002
size_t altTransferSize
Definition: SPICC26X4DMA.h:1008
int32_t rxPinMux
Definition: SPICC26X4DMA.h:969
SwiP_Struct swi
Definition: SPICC26X4DMA.h:996
UDMACC26XX driver implementation.
Software Interrupt module for the RTOS Porting Interface.
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:565
Power notify object structure.
Definition: Power.h:441
uint32_t txChannelBitMask
Definition: SPICC26X4DMA.h:957
Definition: SPICC26X4DMA.h:865
SPI_Mode
Definitions for various SPI modes of operation.
Definition: SPI.h:592
uint32_t activeChannel
Definition: SPICC26X4DMA.h:1010
uint_least8_t pociPin
Definition: SPICC26X4DMA.h:977
SPI_TransferMode transferMode
Definition: SPICC26X4DMA.h:1020
uint32_t minDmaTransferSize
Definition: SPICC26X4DMA.h:984
SPI_Mode mode
Definition: SPICC26X4DMA.h:1021
uint32_t dataSize
Definition: SPICC26X4DMA.h:1012
uint_least8_t picoPin
Definition: SPICC26X4DMA.h:975
size_t framesQueued
Definition: SPICC26X4DMA.h:1005
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26X4DMA.h:999
SPI_Transaction * headPtr
Definition: SPICC26X4DMA.h:1000
uint16_t defaultTxBufValue
Definition: SPICC26X4DMA.h:953
uint32_t busyBit
Definition: SPICC26X4DMA.h:1014
const SPI_FxnTable SPICC26X4DMA_fxnTable
uint32_t rxChannelBitMask
Definition: SPICC26X4DMA.h:955
size_t priTransferSize
Definition: SPICC26X4DMA.h:1007
size_t framesTransferred
Definition: SPICC26X4DMA.h:1006
HwiP_Struct hwi
Definition: SPICC26X4DMA.h:994
uint16_t rxScratchBuf
Definition: SPICC26X4DMA.h:1017
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26X4DMA.h:949
uint_least8_t csnPin
Definition: SPICC26X4DMA.h:1023
bool manualStart
Definition: SPICC26X4DMA.h:1026
Definition: SPICC26X4DMA.h:863
Hardware Interrupt module for the RTOS Porting Interface.
volatile tDMAControlTable * dmaRxTableEntryPri
Definition: SPICC26X4DMA.h:961
SemaphoreP structure.
Definition: SwiP.h:68
uint16_t txScratchBuf
Definition: SPICC26X4DMA.h:1018
uint32_t dsample
Definition: SPICC26X4DMA.h:1015
SPI_Transaction * tailPtr
Definition: SPICC26X4DMA.h:1001
SemaphoreP_Struct transferComplete
Definition: SPICC26X4DMA.h:997
SemaphoreP structure.
Definition: SemaphoreP.h:84
uint_least8_t clkPin
Definition: SPICC26X4DMA.h:979
SPICC26X4DMA_FrameSize
Definition: SPICC26X4DMA.h:848
Power_NotifyObj spiPostObj
Definition: SPICC26X4DMA.h:995
bool isOpen
Definition: SPICC26X4DMA.h:1025