33 #ifndef ti_display_DisplayDogm1286__include 34 #define ti_display_DisplayDogm1286__include 57 char lcdBuffer0[1024];
69 #endif // ti_display_DisplayDogm1286__include void DisplayDogm1286_close(Display_Handle handle)
ADC_Params params
Definition: Driver_Init.h:11
Serial Peripheral Interface (SPI) Driver Interface.
LCD_Buffer used to store data to be printed on the LCD display.
Definition: LCDDogm1286.h:407
void DisplayDogm1286_init(Display_Handle handle)
void DisplayDogm1286_vprintf(Display_Handle handle, uint8_t line, uint8_t column, const char *fmt, va_list va)
struct DisplayDogm1286_HWAttrs DisplayDogm1286_HWAttrs
struct DisplayDogm1286_Object * DisplayDogm1286_Handle
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementatio...
Definition: LCDDogm1286.h:466
Display Parameters.
Definition: Display.h:485
LCD driver implementation for a DOGM128W-6 LCD display.
Semaphore module for the RTOS Porting Interface.
void DisplayDogm1286_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
Generic interface for text output.
Definition: DisplayDogm1286.h:52
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:535
LCD_Handle lcdHandle
Definition: DisplayDogm1286.h:48
Display_Handle DisplayDogm1286_open(Display_Handle handle, Display_Params *params)
SemaphoreP_Struct lcdMutex
Definition: DisplayDogm1286.h:56
LCD_Handle hLcd
Definition: DisplayDogm1286.h:54
const Display_FxnTable DisplayDogm1286_fxnTable
void DisplayDogm1286_clear(Display_Handle handle)
uint_least8_t powerPin
Definition: DisplayDogm1286.h:49
Definition: DisplayDogm1286.h:46
Display Global configuration.
Definition: Display.h:558
int DisplayDogm1286_control(Display_Handle handle, unsigned int cmd, void *arg)
Display_LineClearMode lineClearMode
Definition: DisplayDogm1286.h:55
Display_LineClearMode
How to treat existing elements on a line when writing text.
Definition: Display.h:469
SemaphoreP structure.
Definition: SemaphoreP.h:84
struct DisplayDogm1286_Object DisplayDogm1286_Object
unsigned int DisplayDogm1286_getType(void)