39 #ifndef ti_drivers_crypto_CryptoCC26X4_ns__include 40 #define ti_drivers_crypto_CryptoCC26X4_ns__include 46 #include <ti/devices/DeviceFamily.h> 47 #include DeviceFamily_constructPath(inc/hw_types.h) 49 #include <psa/client.h> 67 psa_status_t CryptoPSACC26X4_call(int32_t type, psa_invec *invecs, psa_outvec *outvecs);
72 void CryptoPSACC26X4_init(
void);
83 bool CryptoPSACC26X4_acquireLock(uint32_t timeout);
90 __STATIC_INLINE
void CryptoPSACC26X4_releaseLock(
void)
void SemaphoreP_post(SemaphoreP_Handle handle)
Function to post (signal) a semaphore from task of ISR context.
Semaphore module for the RTOS Porting Interface.
SemaphoreP structure.
Definition: SemaphoreP.h:84