AESCMACCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
71 #ifndef ti_drivers_aescmac_AESCMACCC26XX__include
72 #define ti_drivers_aescmac_AESCMACCC26XX__include
73 
74 #include <stdint.h>
75 #include <stdbool.h>
76 
77 #include <ti/drivers/AESCMAC.h>
78 
79 #include <ti/drivers/dpl/SwiP.h>
80 
81 #include <ti/devices/DeviceFamily.h>
82 #include DeviceFamily_constructPath(driverlib/aes.h)
83 
84 #ifdef __cplusplus
85 extern "C" {
86 #endif
87 
94 typedef struct
95 {
110  uint8_t intPriority;
112 
118 typedef struct
119 {
120  uint32_t intermediateTag[AES_TAG_LENGTH_BYTES / 4];
121  uint32_t buffer[AES_BLOCK_SIZE / 4];
126  volatile int_fast16_t returnStatus;
130  bool isOpen;
132  volatile bool cryptoResourceLocked;
133  volatile bool hwBusy;
134  volatile bool operationInProgress;
136 
142 bool AESCMAC_acquireLock(AESCMAC_Handle handle, uint32_t timeout);
143 void AESCMAC_releaseLock(AESCMAC_Handle handle);
144 void AESCMAC_enableThreadSafety(AESCMAC_Handle handle);
145 void AESCMAC_disableThreadSafety(AESCMAC_Handle handle);
148 #ifdef __cplusplus
149 }
150 #endif
151 
152 #endif /* ti_drivers_aescmac_AESCMACCC26XX__include */
AESCMAC_ReturnBehavior returnBehavior
Definition: AESCMACCC26XX.h:127
AES Global configuration.
Definition: AESCommon.h:154
CryptoKey datastructure.
Definition: CryptoKey.h:196
AESCMAC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCMAC.h:715
volatile int_fast16_t returnStatus
Definition: AESCMACCC26XX.h:126
AESCMACCC26XX Hardware Attributes.
Definition: AESCMACCC26XX.h:94
AESCMAC_CallbackFxn callbackFxn
Definition: AESCMACCC26XX.h:123
void(* AESCMAC_CallbackFxn)(AESCMAC_Handle handle, int_fast16_t returnValue, AESCMAC_Operation *operation, AESCMAC_OperationType operationType)
The definition of a callback function used by the AESCMAC driver when used in AESCMAC_RETURN_BEHAVIOR...
Definition: AESCMAC.h:739
AESCMACCC26XX Object.
Definition: AESCMACCC26XX.h:118
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESCMACCC26XX.h:110
AESCMAC_OperationalMode
Defines the operation modes for the AESCMAC driver.
Definition: AESCMAC.h:652
AESCMAC_Operation * operation
Definition: AESCMACCC26XX.h:124
volatile bool operationInProgress
Definition: AESCMACCC26XX.h:134
Software Interrupt module for the RTOS Porting Interface.
AESCMAC_OperationType operationType
Definition: AESCMACCC26XX.h:128
CryptoKey key
Definition: AESCMACCC26XX.h:125
volatile bool cryptoResourceLocked
Definition: AESCMACCC26XX.h:132
bool isOpen
Definition: AESCMACCC26XX.h:130
bool threadSafe
Definition: AESCMACCC26XX.h:131
AESCMAC (CMAC and CBC-MAC) driver header.
uint32_t semaphoreTimeout
Definition: AESCMACCC26XX.h:122
Struct containing the parameters required for signing or verifying a message.
Definition: AESCMAC.h:661
AESCMAC_ReturnBehavior
The return behavior of AESCMAC functions.
Definition: AESCMAC.h:622
AESCMAC_OperationalMode operationalMode
Definition: AESCMACCC26XX.h:129
volatile bool hwBusy
Definition: AESCMACCC26XX.h:133
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale