AESCCMCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
70 #ifndef ti_drivers_aesccm_AESCCMCC26XX__include
71 #define ti_drivers_aesccm_AESCCMCC26XX__include
72 
73 #include <stdint.h>
74 #include <stdbool.h>
75 
76 #include <ti/drivers/Power.h>
77 #include <ti/drivers/AESCCM.h>
79 
80 #include <ti/drivers/dpl/HwiP.h>
81 #include <ti/drivers/dpl/SwiP.h>
83 
84 #ifdef __cplusplus
85 extern "C" {
86 #endif
87 
94 typedef struct
95 {
109  uint8_t intPriority;
111 
117 typedef struct
118 {
119  bool isOpen;
122  int_fast16_t returnStatus;
129 
130 #ifdef __cplusplus
131 }
132 #endif
133 
134 #endif /* ti_drivers_aesccm_AESCCMCC26XX__include */
AESCCMCC26XX Hardware Attributes.
Definition: AESCCMCC26XX.h:94
The CryptoKey type is an opaque representation of a cryptographic key.
uint32_t semaphoreTimeout
Definition: AESCCMCC26XX.h:125
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a me...
Definition: AESCCM.h:870
bool operationInProgress
Definition: AESCCMCC26XX.h:120
Power Manager.
bool isOpen
Definition: AESCCMCC26XX.h:119
Semaphore module for the RTOS Porting Interface.
AESCCM_ReturnBehavior returnBehavior
Definition: AESCCMCC26XX.h:123
AESCCM_CallbackFxn callbackFxn
Definition: AESCCMCC26XX.h:126
Software Interrupt module for the RTOS Porting Interface.
bool operationCanceled
Definition: AESCCMCC26XX.h:121
void(* AESCCM_CallbackFxn)(AESCCM_Handle handle, int_fast16_t returnValue, AESCCM_OperationUnion *operation, AESCCM_OperationType operationType)
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_C...
Definition: AESCCM.h:1059
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESCCMCC26XX.h:109
int_fast16_t returnStatus
Definition: AESCCMCC26XX.h:122
AESCCMCC26XX Object.
Definition: AESCCMCC26XX.h:117
AESCCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESCCM.h:1029
AESCCM_ReturnBehavior
The way in which CCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESCCM.h:836
AESCCM_Operation * operation
Definition: AESCCMCC26XX.h:127
AESCCM driver header.
Hardware Interrupt module for the RTOS Porting Interface.
AESCCM_OperationType operationType
Definition: AESCCMCC26XX.h:124
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale