Instance: SPI0
Component: SPI
Base address: 0x40000000
Serial Peripheral Interface (SPI) with master and slave capabilities
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RO |
32 |
0x0000 0000 |
0x0000 0020 |
0x4000 0020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x4000 0028 |
|
RO |
32 |
0x0000 0000 |
0x0000 0030 |
0x4000 0030 |
|
RO |
32 |
0x0000 0000 |
0x0000 0038 |
0x4000 0038 |
|
WO |
32 |
0x0000 0000 |
0x0000 0040 |
0x4000 0040 |
|
WO |
32 |
0x0000 0000 |
0x0000 0048 |
0x4000 0048 |
|
RW |
32 |
0x0000 0001 |
0x0000 00E0 |
0x4000 00E0 |
|
RO |
32 |
0x1411 0010 |
0x0000 00FC |
0x4000 00FC |
|
RW |
32 |
0x0000 0000 |
0x0000 0100 |
0x4000 0100 |
|
RW |
32 |
0x0000 0004 |
0x0000 0104 |
0x4000 0104 |
|
RW |
32 |
0x0000 0000 |
0x0000 0108 |
0x4000 0108 |
|
RW |
32 |
0x0000 0012 |
0x0000 010C |
0x4000 010C |
|
RO |
32 |
0x0000 000F |
0x0000 0110 |
0x4000 0110 |
|
RW |
32 |
0x0000 0000 |
0x0000 0114 |
0x4000 0114 |
|
RW |
32 |
0x0000 0000 |
0x0000 0118 |
0x4000 0118 |
|
RO |
32 |
0x0000 0000 |
0x0000 0130 |
0x4000 0130 |
|
RW |
32 |
0x0000 0000 |
0x0000 0140 |
0x4000 0140 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x4000 0020 | Instance | 0x4000 0020 |
Description | This register provides the highest priority enabled interrupt index. Value 0x00 means no event pending. Interrupt 1 is the highest priority, and 31 is the least priority. That is, the least bit position that is set to 1 denotes the highest priority pending interrupt. The priority order is fixed. However, users can implement their own prioritization schemes using other registers that expose the full set of interrupts that have occurred. On each read, only one interrupt is indicated. On a read, the current interrupt (highest priority) is automatically cleared by the hardware and the corresponding interrupt flag in RIS and MIS are cleared as well. After a read from the CPU (not from the debug interface), the register is updated with the next highest priority interrupt, if none are pending, then it would display 0x0. |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||||||||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | |||||||||||||||||||||||||||||||||||
7:0 | STAT | Interrupt index status
|
RO | 0x00 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x4000 0028 | Instance | 0x4000 0028 |
Description | Interrupt Mask. If a bit is set, then corresponding interrupt is un-masked. Un-masking the interrupt causes the raw interrupt to be visible in IIDX, as well as MIS. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||
8 | DMA_DONE_TX | DMA Done event for TX event mask.
|
0 | ||||||||||||
7 | DMA_DONE_RX | DMA Done event for RX event mask.
|
0 | ||||||||||||
6 | IDLE | SPI Idle event mask.
|
0 | ||||||||||||
5 | TXEMPTY | Transmit FIFO Empty event mask.
|
0 | ||||||||||||
4 | TX | Transmit FIFO event mask.
|
0 | ||||||||||||
3 | RX | Receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached
|
0 | ||||||||||||
2 | RTOUT | SPI Receive Time-Out event mask.
|
0 | ||||||||||||
1 | PER | Parity error event mask.
|
0 | ||||||||||||
0 | RXFIFO_OVF | RXFIFO overflow event mask.
|
0 |
Address Offset | 0x0000 0030 | ||
Physical Address | 0x4000 0030 | Instance | 0x4000 0030 |
Description | Raw interrupt status. Reflects all pending interrupts, regardless of masking. The RIS register allows the user to implement a poll scheme. A flag set in this register can be cleared by writing 1 to the ICLR register bit even if the corresponding IMASK bit is not enabled. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||
8 | DMA_DONE_TX | DMA Done event for TX. This interrupt is set if the TX DMA channel sends the DONE signal. This allows the handling of the DMA event inside the mapped peripheral.
|
0 | ||||||||||||
7 | DMA_DONE_RX | DMA Done event for RX. This interrupt is set if the RX DMA channel sends the DONE signal. This allows the handling of the DMA event inside the mapped peripheral.
|
0 | ||||||||||||
6 | IDLE | SPI has completed transfers and changed into IDLE mode. This bit is set when STAT.BUSY goes low.
|
0 | ||||||||||||
5 | TXEMPTY | Transmit FIFO Empty interrupt mask. This interrupt is set if all data in the Transmit FIFO have been move to the shift register.
|
0 | ||||||||||||
4 | TX | Transmit FIFO event. This interrupt is set if the selected Transmit FIFO level has been reached.
|
0 | ||||||||||||
3 | RX | Receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached
|
0 | ||||||||||||
2 | RTOUT | SPI Receive Time-Out event.
|
0 | ||||||||||||
1 | PER | Parity error event: this bit is set if a parity error has been detected
|
0 | ||||||||||||
0 | RXFIFO_OVF | RXFIFO overflow event. This interrupt is set if an RX FIFO overflow has been detected.
|
0 |
Address Offset | 0x0000 0038 | ||
Physical Address | 0x4000 0038 | Instance | 0x4000 0038 |
Description | Masked interrupt status. This is an AND of the IMASK and RIS registers. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||
8 | DMA_DONE_TX | Masked DMA Done event for TX.
|
0 | ||||||||||||
7 | DMA_DONE_RX | Masked DMA Done event for RX.
|
0 | ||||||||||||
6 | IDLE | Masked SPI IDLE mode event.
|
0 | ||||||||||||
5 | TXEMPTY | Masked Transmit FIFO Empty event.
|
0 | ||||||||||||
4 | TX | Masked Transmit FIFO event. This interrupt is set if the selected Transmit FIFO level has been reached.
|
0 | ||||||||||||
3 | RX | Masked receive FIFO event. This interrupt is set if the selected Receive FIFO level has been reached
|
0 | ||||||||||||
2 | RTOUT | Masked SPI Receive Time-Out Interrupt.
|
0 | ||||||||||||
1 | PER | Masked Parity error event: this bit if a parity error has been detected
|
0 | ||||||||||||
0 | RXFIFO_OVF | Masked RXFIFO overflow event. This interrupt is set if an RX FIFO overflow has been detected.
|
0 |
Address Offset | 0x0000 0040 | ||
Physical Address | 0x4000 0040 | Instance | 0x4000 0040 |
Description | Interrupt set. Allows interrupts to be set by software (useful in diagnostics and safety checks). Writing a 1 to a bit in ISET will set the event and therefore the related RIS bit also gets set. If the interrupt is enabled through the mask, then the corresponding MIS bit is also set. | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||
8 | DMA_DONE_TX | Set DMA Done event for TX.
|
0 | ||||||||||||
7 | DMA_DONE_RX | Set DMA Done event for RX.
|
0 | ||||||||||||
6 | IDLE | Set SPI IDLE mode event.
|
0 | ||||||||||||
5 | TXEMPTY | Set Transmit FIFO Empty event.
|
0 | ||||||||||||
4 | TX | Set Transmit FIFO event.
|
0 | ||||||||||||
3 | RX | Set Receive FIFO event.
|
0 | ||||||||||||
2 | RTOUT | Set SPI Receive Time-Out event.
|
0 | ||||||||||||
1 | PER | Set Parity error event.
|
0 | ||||||||||||
0 | RXFIFO_OVF | Set RXFIFO overflow event.
|
0 |
Address Offset | 0x0000 0048 | ||
Physical Address | 0x4000 0048 | Instance | 0x4000 0048 |
Description | Interrupt clear. Write a 1 to clear the corresponding Interrupt. | ||
Type | WO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||
8 | DMA_DONE_TX | Clear DMA Done event for TX.
|
0 | ||||||||||||
7 | DMA_DONE_RX | Clear DMA Done event for RX.
|
0 | ||||||||||||
6 | IDLE | Clear SPI IDLE mode event.
|
0 | ||||||||||||
5 | TXEMPTY | Clear Transmit FIFO Empty event.
|
0 | ||||||||||||
4 | TX | Clear Transmit FIFO event.
|
0 | ||||||||||||
3 | RX | Clear Receive FIFO event.
|
0 | ||||||||||||
2 | RTOUT | Clear SPI Receive Time-Out event.
|
0 | ||||||||||||
1 | PER | Clear Parity error event.
|
0 | ||||||||||||
0 | RXFIFO_OVF | Clear RXFIFO overflow event.
|
0 |
Address Offset | 0x0000 00E0 | ||
Physical Address | 0x4000 00E0 | Instance | 0x4000 00E0 |
Description | Event mode register. It is used to select whether each line is disabled, in software mode (software clears the RIS) or in hardware mode (hardware clears the RIS) Note: The recommendation is to use SPI in the software mode |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | ||||||||||||||
1:0 | INT0_CFG | Event line mode select for event corresponding to IPSTANDARD.INT_EVENT0
|
RW | 0b01 |
Address Offset | 0x0000 00FC | ||
Physical Address | 0x4000 00FC | Instance | 0x4000 00FC |
Description | This register identifies the peripheral and its exact version. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:16 | MODULEID | Module identification contains a unique peripheral identification number. The assignments are maintained in a central database for all of the platform modules to ensure uniqueness. | 0x1411 | |||
15:12 | FEATUREVER | Feature set version for this module instance. | 0x0 | |||
11:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | ||
7:4 | MAJREV | Major revision of the IP | 0x1 | |||
3:0 | MINREV | Minor revision of the IP | 0x0 |
Address Offset | 0x0000 0100 | ||
Physical Address | 0x4000 0100 | Instance | 0x4000 0100 |
Description | SPI Control Register 0 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
31:15 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
14 | CSCLR | Clear shift register counter when CS gets inactive. This bit is relevant only in the slave mode, CTL1.MS = 0.
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
13:12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
11:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
9 | SPH | CLKOUT phase (Motorola SPI frame format only) This bit selects the clock edge that captures data and enables it to change state. It has the most impact on the first bit transmitted by either permitting or not permitting a clock transition before the first data capture edge.
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
8 | SPO | CLKOUT polarity (Motorola SPI frame format only)
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
7 | RESERVED7 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
6:5 | FRF | Frame format Select
|
RW | 0b00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
4:0 | DSS | Data Size Select. Note: Master mode: Values 0 - 2 are reserved and shall not be used. This will map to 4 bit mode. A value of 3h corresponds to 4-bit data (and so on). Slave mode: DSS should be no less than 6 which means the minimum frame length is 7 bits.
|
RW | 0b0 0000 |
Address Offset | 0x0000 0104 | ||
Physical Address | 0x4000 0104 | Instance | 0x4000 0104 |
Description | SPI Control Register 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:30 | RESERVED30 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | |||||||||||
29:24 | RXTIMEOUT | Receive Timeout (only for Slave mode). This register defines the number of clock cycles after which the Receive Timeout interrupt is set. A value of 0 disables this function.
|
RW | 0b00 0000 | |||||||||||
23:16 | REPEATTX | Counter to repeat last transfer. A value of 0 disables this feature. After a non-zero value (X) is written to this register, SPI transfer can be started with writing a data into the TX Buffer. The data will be transferred X+1 times in total. The behavior is identical as if the data were be written into the TX Buffer that many times as defined by the value here additionally. It can be used to clean a transfer or to pull a certain amount of data by a slave. This feature can be used only in the master mode.
|
RW | 0x00 | |||||||||||
15:11 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 | |||||||||||
10 | FIFORST | This bit is used to reset transmit and receive FIFO pointers. The pointers are held at a reset value until this bit is cleared to zero.
|
RW | 0 | |||||||||||
9:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | |||||||||||
7 | PBS | Parity Bit Select
|
RW | 0 | |||||||||||
6 | PES | Even Parity Select
|
RW | 0 | |||||||||||
5 | PEN | Parity enable if enabled the last bit will be used as parity to evaluate the right transmission of the previous bits. In case of a parity mismatch the parity error flag RIS.PER will be set.
|
RW | 0 | |||||||||||
4 | MSB | MSB first select. Controls the direction of the receive and transmit shift register.
|
RW | 0 | |||||||||||
3 | SOD | Slave-mode: Data output disabled This bit is relevant only in the slave mode, MS=0. In multiple-slave systems, it is possible for an SPI master to broadcast a message to all slaves in the system while ensuring that only one slave drives data onto its serial output line. In such systems the RX lines from multiple slaves could be tied together. To operate in such systems, this bitfield can be set if the SPI slave is not supposed to drive the TX line.
|
RW | 0 | |||||||||||
2 | MS | Master or slave mode select. This bit can be modified only when SPI is disabled, CTL1.ENABLE = 0.
|
RW | 1 | |||||||||||
1 | LBM | Loop back mode
|
RW | 0 | |||||||||||
0 | ENABLE | SPI enable
|
RW | 0 |
Address Offset | 0x0000 0108 | ||
Physical Address | 0x4000 0108 | Instance | 0x4000 0108 |
Description | Clock prescaler and divider register. This register contains the settings for the Clock prescaler and divider settings. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:28 | DSAMPLE | Delayed sampling. In master mode the data on the input pin will be sampled after the defined clock cycles. Note: As an example, if the SPI transmit frequency is set to 12 MHz in the master mode, DSAMPLE should be set to a value of 2 | RW | 0x0 | |||||||||||
27:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 | |||||||||||
9:0 | SCR | Serial clock divider: This is used to generate the transmit and receive bit rate of the SPI. The SPI bit rate is (SPI's functional clock frequency)/((SCR+1)*2). SCR is a value from 0-1023.
|
RW | 0b00 0000 0000 |
Address Offset | 0x0000 010C | ||
Physical Address | 0x4000 010C | Instance | 0x4000 010C |
Description | The IFLS register is the interrupt FIFO level select register. This register can be used to define the levels at which the TX, RX FIFO interrupt flags are triggered. Out of reset, the TXIFLSEL and RXIFLSEL bits are configured so that the FIFOs trigger an interrupt at the half-way mark. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
31:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 | |||||||||||||||||||||||||||||
5:3 | RXIFLSEL | SPI Receive Interrupt FIFO Level Select The trigger points for the receive interrupt are as follows:
|
RW | 0b010 | |||||||||||||||||||||||||||||
2:0 | TXIFLSEL | SPI Transmit Interrupt FIFO Level Select The trigger points for the transmit interrupt are as follows:
|
RW | 0b010 |
Address Offset | 0x0000 0110 | ||
Physical Address | 0x4000 0110 | Instance | 0x4000 0110 |
Description | Status Register | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 | |||||||||||
4 | BUSY | Busy
|
0 | ||||||||||||
3 | RNF | Receive FIFO not full
|
1 | ||||||||||||
2 | RFE | Receive FIFO empty.
|
1 | ||||||||||||
1 | TNF | Transmit FIFO not full
|
1 | ||||||||||||
0 | TFE | Transmit FIFO empty.
|
1 |
Address Offset | 0x0000 0114 | ||
Physical Address | 0x4000 0114 | Instance | 0x4000 0114 |
Description | This register is used to specify a divide ratio of the SPI functional clock. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||||||||||||||||||||
2:0 | RATIO | Selects divide ratio of module clock
|
RW | 0b000 |
Address Offset | 0x0000 0118 | ||
Physical Address | 0x4000 0118 | Instance | 0x4000 0118 |
Description | DMA Control Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 0000 0000 0000 | ||
1 | TXDMAE | Transmit FIFO DMA enable when set. | RW | 0 | ||
0 | RXDMAE | Receive FIFO DMA enable when set. | RW | 0 |
Address Offset | 0x0000 0130 | ||
Physical Address | 0x4000 0130 | Instance | 0x4000 0130 |
Description | RXDATA Register. Reading this register returns value in the RX FIFO pointed by the current FIFO read pointer. If the RX FIFO is empty, the last read value is returned. Writing has not effect and is ignored. | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:0 | DATA | Received Data | RO | 0x0000 0000 |
Address Offset | 0x0000 0140 | ||
Physical Address | 0x4000 0140 | Instance | 0x4000 0140 |
Description | TXDATA Register. Writing into this register puts the data into the TX FIFO. Reading this register returns the last written value, pointed by the current FIFO write pointer. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | DATA | Transmit Data | RW | 0x0000 0000 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |