TI BLE5-Stack API Documentation  2.02.09.00
bcomdef.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  Group: WCS, BTS
4  $Target Device: DEVICES $
5 
6  ******************************************************************************
7  $License: TI_TEXT 2009 $
8  ******************************************************************************
9  $Release Name: PACKAGE NAME $
10  $Release Date: PACKAGE RELEASE DATE $
11  *****************************************************************************/
12 
18 #ifndef BCOMDEF_H
19 #define BCOMDEF_H
20 
21 #ifdef __cplusplus
22 extern "C"
23 {
24 #endif
25 
26 
27 /*********************************************************************
28  * INCLUDES
29  */
30 
31 #include "comdef.h"
32 
33 /*********************************************************************
34  * CONSTANTS
35  */
36 
38 #if defined ( HOST_CONFIG )
39  // Set the Controller Configuration
40  #if ( HOST_CONFIG == ( CENTRAL_CFG | PERIPHERAL_CFG ) )
41  #define CTRL_CONFIG ( ADV_NCONN_CFG | ADV_CONN_CFG | SCAN_CFG | INIT_CFG )
42  #elif ( HOST_CONFIG == ( CENTRAL_CFG | BROADCASTER_CFG ) )
43  #define CTRL_CONFIG ( ADV_NCONN_CFG | SCAN_CFG | INIT_CFG )
44  #elif ( HOST_CONFIG == ( PERIPHERAL_CFG | OBSERVER_CFG ) )
45  #define CTRL_CONFIG ( ADV_NCONN_CFG | ADV_CONN_CFG | SCAN_CFG )
46  #elif ( HOST_CONFIG == ( BROADCASTER_CFG | OBSERVER_CFG ) )
47  #define CTRL_CONFIG ( ADV_NCONN_CFG | SCAN_CFG )
48  #elif ( HOST_CONFIG == CENTRAL_CFG )
49  #define CTRL_CONFIG ( SCAN_CFG | INIT_CFG )
50  #elif ( HOST_CONFIG == PERIPHERAL_CFG )
51  #define CTRL_CONFIG ( ADV_NCONN_CFG | ADV_CONN_CFG )
52  #elif ( HOST_CONFIG == OBSERVER_CFG )
53  #define CTRL_CONFIG SCAN_CFG
54  #elif ( HOST_CONFIG == BROADCASTER_CFG )
55  #define CTRL_CONFIG ADV_NCONN_CFG
56  #else
57  #if defined ( FLASH_ONLY_BUILD ) || defined ( FLASH_ROM_BUILD )
58  #error "Build Configuration Error: Invalid Host Role!"
59  #endif
60  #endif
61 #else
62  // Controller Sanity Check: Stop build when no configuration is defined.
63  #if !defined( CTRL_CONFIG ) || !( CTRL_CONFIG & ( ADV_NCONN_CFG | \
64  ADV_CONN_CFG | \
65  SCAN_CFG | \
66  INIT_CFG ) )
67  #if defined ( FLASH_ONLY_BUILD ) || defined ( FLASH_ROM_BUILD )
68  #error "Build Configuration Error: At least one Controller build component required!"
69  #endif
70  #endif // no Controller build components defined
71 #endif
72 
73 // If BLE_V41_FEATURES is defined, map it to CTRL_V41_CONFIG
74 #if defined ( BLE_V41_FEATURES ) && !defined ( CTRL_V41_CONFIG )
75  #define CTRL_V41_CONFIG ( ( BLE_V41_FEATURES ) & CTRL_V41_MASK )
76 #elif defined ( BLE_V41_FEATURES ) && defined ( CTRL_V41_CONFIG )
77  #error "Build Configuration Error: Cannot define both BLE_V41_FEATURES and CTRL_V41_CONFIG!"
78 #endif // BLE_V41_FEATURES
79 
80 // If BLE_V50_FEATURES is defined, map it to CTRL_V50_CONFIG
81 #if defined ( BLE_V50_FEATURES ) && !defined ( CTRL_V50_CONFIG )
82  #define CTRL_V50_CONFIG BLE_V50_FEATURES
83 #elif defined ( BLE_V50_FEATURES ) && defined ( CTRL_V50_CONFIG )
84  #error "Build Configuration Error: Cannot define both BLE_V50_FEATURES and CTRL_V50_CONFIG!"
85 #endif // BLE_V41_FEATURES
86 
87 #if defined(CC2540) || defined(CC2541) || defined(CC2541S)
88  #if !defined ( MAX_NUM_BLE_CONNS )
89  #if ( CTRL_CONFIG & INIT_CFG )
90  #define MAX_NUM_BLE_CONNS 3
91  #elif ( !( CTRL_CONFIG & INIT_CFG ) && ( CTRL_CONFIG & ADV_CONN_CFG ) )
92  #define MAX_NUM_BLE_CONNS 1
93  #else // no connection needed
94  #define MAX_NUM_BLE_CONNS 0
95  #endif // CTRL_CONFIG=INIT_CFG
96  #endif // !MAX_NUM_BLE_CONNS
97 #endif // CC2540 | CC2541 | CC2541S
98 
100 
102 #define B_ADDR_LEN 6
103 
105 #define KEYLEN 16
106 
109 #define LSB_2_BYTES 2
110 
112 #define MSB_4_BYTES 4
113 
115 #define B_CHANNEL_MAP_LEN 5
116 
118 #define B_EVENT_MASK_LEN 8
119 
121 #define B_LOCAL_NAME_LEN 248
122 
124 #define B_MAX_ADV_LEN 31
125 
127 #define B_RANDOM_NUM_SIZE 8
128 
130 #define B_FEATURE_SUPPORT_LENGTH 8
131 
133 #define B_APP_DEFAULT_PASSCODE 123456
134 
136 #define EXTENDED_STACK_SETTINGS_DEFAULT 0x00
137 
139 #define MASTER_GUARD_TIME_ENABLE 0x01
140 #define CC2652RB_OVERRIDE_USED 0x02
141 
142 #define bleInvalidTaskID INVALID_TASK
143 #define bleNotReady 0x10
144 #define bleAlreadyInRequestedMode 0x11
145 #define bleIncorrectMode 0x12
146 #define bleMemAllocError 0x13
147 #define bleNotConnected 0x14
148 #define bleNoResources 0x15
149 #define blePending 0x16
150 #define bleTimeout 0x17
151 #define bleInvalidRange 0x18
152 #define bleLinkEncrypted 0x19
153 #define bleProcedureComplete 0x1A
154 #define bleInvalidMtuSize 0x1B
155 #define blePairingTimedOut 0x1C
156 #define bleMemFreeError 0x1D
157 #define bleInternalError 0x1E
158 
159 // GAP Status Return Values - returned as bStatus_t
160 #define bleGAPUserCanceled 0x30
161 #define bleGAPConnNotAcceptable 0x31
162 #define bleGAPBondRejected 0x32
163 #define bleGAPBufferInUse 0x33
164 #define bleGAPNotFound 0x34
165 #define bleGAPFilteredOut 0x35
166 
167 // ATT Status Return Values - returned as bStatus_t
168 #define bleInvalidPDU 0x40
169 #define bleInsufficientAuthen 0x41
170 #define bleInsufficientEncrypt 0x42
171 #define bleInsufficientKeySize 0x43
172 
173 // L2CAP Status Return Values - returned as bStatus_t
174 
175 #define INVALID_TASK_ID 0xFF
176 
177 // Note: Maximum NVID index is 0x03FF (10 bits) - this is a NV driver limitation
178 
179 // Device NV Items - Range 0 - 0x1F
180 #define BLE_NVID_IRK 0x02
181 #define BLE_NVID_CSRK 0x03
182 #define BLE_NVID_ADDR_MODE 0x04
183 #define BLE_LRU_BOND_LIST 0x05
184 #define BLE_NVID_RANDOM_ADDR 0x06
185 
186 // Bonding NV Items - Range 0x20 - 0xDF - This allows for 32 bonds
187 #define BLE_NVID_GAP_BOND_START 0x20
188 #define BLE_NVID_GAP_BOND_END 0xDF
189 
190 // GATT Configuration NV Items - Range 0xE0 - 0xFF - This must match the number of Bonding entries
191 #define BLE_NVID_GATT_CFG_START 0xE0
192 #define BLE_NVID_GATT_CFG_END 0xFF
193 
194 // Customer NV Items - Range 0x100 - 0x11F - This must match the number of Bonding entries
195 #define BLE_NVID_CUST_START 0x100
196 #define BLE_NVID_CUST_END 0x11F
197 
198 // BLE Mesh NV IDs Start
199 #define BLE_NVID_MESH_START BLE_NVID_CUST_END + 1
200 
201 /*********************************************************************
202  * BLE OSAL GAP GLOBAL Events
203  */
204 #define GAP_EVENT_SIGN_COUNTER_CHANGED 0x4000
205 
206 // GAP - Messages IDs (0xD0 - 0xDF)
207 #define GAP_MSG_EVENT 0xD0
208 
209 // SM - Messages IDs (0xC1 - 0xCF)
210 #define SM_NEW_RAND_KEY_EVENT 0xC1
211 #define SM_MSG_EVENT 0xC2
212 
213 // GATT - Messages IDs (0xB0 - 0xBF)
214 #define GATT_MSG_EVENT 0xB0
215 #define GATT_SERV_MSG_EVENT 0xB1
216 
217 // L2CAP - Messages IDs (0xA0 - 0xAF)
218 #define L2CAP_DATA_EVENT 0xA0
219 #define L2CAP_SIGNAL_EVENT 0xA2
220 
221 // HCI - Messages IDs (0x90 - 0x9F)
222 #define HCI_DATA_EVENT 0x90
223 #define HCI_GAP_EVENT_EVENT 0x91
224 #define HCI_SMP_EVENT_EVENT 0x92
225 #define HCI_EXT_CMD_EVENT 0x93
226 #define HCI_SMP_META_EVENT_EVENT 0x94
227 #define HCI_GAP_META_EVENT_EVENT 0x95
228 
229 // ICall and Dispatch - Messages IDs (0x80 - 0x8F)
230 #define ICALL_EVENT_EVENT 0x80
231 #define ICALL_CMD_EVENT 0x81
232 #define DISPATCH_CMD_EVENT 0x82
233 
234 #ifdef __TI_COMPILER_VERSION__
235 #define PRAGMA_OPTIMIZE_NONE
236 #elif defined(__IAR_SYSTEMS_ICC__)
237 #define PRAGMA_OPTIMIZE_NONE _Pragma("optimize=none")
238 #endif
239 
240 /*********************************************************************
241  * TYPEDEFS
242  */
243 
245 typedef Status_t bStatus_t;
246 
247 
248 /*********************************************************************
249  * System Events
250  */
251 
252 /*********************************************************************
253  * Global System Messages
254  */
255 
256 /*********************************************************************
257  * MACROS
258  */
259 
261 #define TI_BASE_UUID_128( uuid ) 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0xB0, \
262  0x00, 0x40, 0x51, 0x04, LO_UINT16( uuid ), HI_UINT16( uuid ), 0x00, 0xF0
263 
264 /*********************************************************************
265  * GLOBAL VARIABLES
266  */
267 
268 /*********************************************************************
269  * FUNCTIONS
270  */
271 
272 /*********************************************************************
273 *********************************************************************/
274 
275 #ifdef __cplusplus
276 }
277 #endif
278 
279 #endif /* BCOMDEF_H */
Common Defines.
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:245
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale