Changelog
Table of Contents
New Features
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-4505 | [BASIC BLE] [Profiles] Included Glucose Profile support in Basic BLE Profiles on CC13X4 |
| BLE_AGAMA-4129 | [BASIC BLE] [Profiles] Included Health Thermometer Profile support in Basic BLE Profiles on CC13X4 |
Proprietary RF
| ID | Summary |
|---|---|
| PROPRF-1228 | Improvements targeting SysConfig migration |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-4408 | Add a Set PIB attribute support for PTA statistics pib |
| TI154STACK-4397 | [SPS] 15.4 stack with PHY-Plugin supports other customer PHYS |
| TI154STACK-4388 | TI154Stack to support sending PTA Counters through Co-Processor Interface |
TI Wi-SUN FAN
| ID | Summary |
|---|---|
| WISUN-954 | Enable ARIB regulatory compliance for JP/EU PHYs |
TI Wireless Solar Management System
| ID | Summary |
|---|---|
| WISUN-971 | Add Wireless Solar Management System examples |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-2063 | Improvements targeting SysConfig migration |
DMM
| ID | Summary |
|---|---|
| DMM-1383 | Improvements targeting SysConfig migration |
SimpleLink Common Components Module (SCCM)
| ID | Summary |
|---|---|
| SCCM-375 | Updated the mcuboot readme file |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-6194 | Add I2S SysConfig support for “not in use” GPIO state and deprecate controllerTargetSelection |
| TIDRIVERS-6178 | Add volatile key KeyStore support to ECJPAKE drivers |
| TIDRIVERS-6134 | Include FreeRTOS kernel source files in Core SDK |
| TIDRIVERS-6099 | Add MessageQueueP DPL module |
| TIDRIVERS-6075 | Remove unused Power function prototypes |
| TIDRIVERS-5998 | Update Power driver APIs to use uint32_t for resource IDs instead of uint_fast16_t |
| TIDRIVERS-5993 | Port SimpleLink KeyStore to mbedTLS 3.4.0 |
| TIDRIVERS-5964 | Migrate to TF-M v1.8 including Key Store |
| TIDRIVERS-5935 | Add CANFD driver support for CC26x1 and CC26x2 |
| TIDRIVERS-5913 | Add Power_getConstraintCount |
| TIDRIVERS-5495 | Add LogSinkUART |
| TIDRIVERS-5342 | Add ECJPAKE driver to TFM v1.8 |
| FREERTOS-12 | Allow configuration of FreeRTOS source location |
| FREERTOS-10 | Add support for custom tickrate in FreeRTOS Sysconfig Module |
| FREERTOS-6 | FreeRTOS GCC standard library re-entrancy support causes task control block size of 340 bytes |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFCORE-1031 | cc13x4_cc26x4: Settings Release - 10 dBm: BLE 1M, 2M and Coded - Characterized |
| RFCORE-1032 | cc13x4_cc26x4: Settings Release - 10 dBm: IEEE 802.15.4 (ZigBee) - Characterized |
| RFCORE-1011 | cc13x4: PA Table Update - Increased Sub-1GHz Granularity |
| RFCORE-1033 | CC1354R: Settings Release - 5 dBm: ZigBee Frontend ID - Characterized |
Fixed Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-4839 | Critical Section order not optimal in ICall_leaveCSImpl & ICall_enterCSImpl functions |
| BLE_AGAMA-4785 | In rare occasions, DUT does not respond to LLCP Encryption Request |
| BLE_AGAMA-4724 | Extended disconnect/reconnect test sometimes leads to exception in Multirole with one peripheral and two centrals |
| BLE_AGAMA-4723 | Stack generates unexpected RPA |
| BLE_AGAMA-4710 | [Multi-Connection] CC1354P10-1 Fails to save 16th bond as peripheral and 15th bond as central |
| BLE_AGAMA-4585 | Connection handle and timestamp for GAP_CB_PHY_UPDATE may be incorrect when multiple connections are maintained |
| BLE_AGAMA-4580 | Connection Event Report reports incorrect channel |
| BLE_AGAMA-4573 | [CC2642] Peripheral fails to respond to CON_IND when using GAP_ADV_WL_POLICY_WL_ALL_REQ and connected to Central using RPA with Random ID |
| BLE_AGAMA-4559 | Under certain conditions, incorrect channel is calculated for connection event as peripheral |
| BLE_AGAMA-4480 | [Basic Example] Basic Broadcaster Doesn't Advertise |
| BLE_AGAMA-4425 | BLE Stack does not dequeue ATT msg during fuzzing test |
| BLE_AGAMA-4250 | The rtls_coordinator mixes up scanned extended advertisements' device address |
| BLE_AGAMA-3838 | host_test may raise a UTIL_SystemErrorEvent with status INVALID_INTERRUPT_ID when UART data overflow |
| BLE_AGAMA-3169 | Connecting twice to the same device causing wrong count of connections and a memory leakage |
Proprietary RF
| ID | Summary |
|---|---|
| None | None |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-4409 | CC1354P10RGZ device migration |
| TI154STACK-4407 | Error at run time with BIOS Assertions enabled |
| TI154STACK-4401 | Background RX command not re-issued after coex settings updated in PIB |
TI Wi-SUN FAN
| ID | Summary |
|---|---|
| WISUN-984 | Fix incorrect PySpinel RSSI calculation |
| WISUN-979 | Enable CC1352P10_1 to CC1354P10RGZ device migration |
| WISUN-973 | PAN ID sysconfig setting on Router node should be greyed out and set to 0xFFFF |
TI Wireless Solar Management System
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| None | None |
DMM
| ID | Summary |
|---|---|
| None | None |
SimpleLink Common Components Module (SCCM)
| ID | Summary |
|---|---|
| SCCM-407 | Build error for iar projects |
| SCCM-404 | Corrected the path to cui.h in cui.c to fix a build issue |
| SCCM-401 | Fixed: Hash is incorrectly calculated for very small images |
| SCCM-395 | Fixed: Incorrect CRC calculation when the image is located at a non-0x0 position |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-6320 | Pregenerated FreeRTOSConfig.h not included in release |
| TIDRIVERS-6062 | Add a critical section for Linked-List manipulation to avoid conflicts |
| TIDRIVERS-5969 | GPIO_resetConfig permanently clears IO callbacks set through SysConfig |
| TIDRIVERS-5968 | The ChipSelect signal gets asserted after SPI_open( ) is called on CC13X4/CC26X4 devices |
| LPRFXXWARE-904 | Fix CPUdelay() compilation issue when TICLANG Link-Time Optimization (LTO) is enabled |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| None | None |
Known Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-4855 | [Multi Connect] CC2651P3 Central fails to connect to more than 5 testers with privacy enable |
| BLE_AGAMA-4846 | [Data Stream][Display] display_printf() is fail when try to print data larger then threshold of 300-500 bytes |
| BLE_AGAMA-4837 | [IOP][Android 14][One Plus 11] With privacy enabled, reconnection fails after after Pairing & Bonding |
| BLE_AGAMA-4830 | [SWAT] Scanner failes after receiving an incorrect event type |
| BLE_AGAMA-4484 | multi_role FreeRTOS support removed from CC13XX / CC26XX |
| BLE_AGAMA-4354 | Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager |
| BLE_AGAMA-4324 | [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar |
| BLE_AGAMA-4029 | Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set. |
| BLE_AGAMA-4009 | [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands |
| BLE_AGAMA-3896 | [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands |
| BLE_AGAMA-3774 | Under certain conditions the CC2652R1 failed to synchronize to periodic advertising |
| BLE_AGAMA-3752 | [CC2651] Host_test memory limitation using CCS+TI-CLANG |
| BLE_AGAMA-3540 | [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC |
| BLE_AGAMA-3486 | Device asserts upon connection when HeapMem and HeapTrack is used |
| BLE_AGAMA-3427 | System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued |
| BLE_AGAMA-3381 | Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration |
| BLE_AGAMA-3107 | [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms |
| BLE_AGAMA-3077 | [RTLS] CTE reception on the 2M PHY do not meet spec requirements |
| BLE_AGAMA-3076 | [RTLS] CTEs sent on the 2M PHY do not meet spec requirements |
| BLE_AGAMA-2266 | Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
| BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
| BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
| BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
| BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
Proprietary RF
| ID | Summary |
|---|---|
| None | None |
TI 15.4-Stack
| ID | Summary |
|---|---|
| None | None |
TI Wi-SUN FAN
| ID | Summary |
|---|---|
| None | None |
TI Wireless Solar Management System
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| None | None |
DMM
| ID | Summary |
|---|---|
| None | None |
SimpleLink Common Components Module (SCCM)
| ID | Summary |
|---|---|
| None | None |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-4844 | Implement restrictions in errata note IOC_01 in SysConfig |
| TIDRIVERS-4127 | ADCBuf causes jitter when switching clock sources |
| SYSBIOS-642 | Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field |
| SYSBIOS-446 | Reported CPU load is not 100% when a task is in “while 1 {}” loop |
| SYSBIOS-98 | Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432 |
| FREERTOS-8 | Tasks view in ROV for FreeRTOS does not show if a task is blocked on a semaphore or mutex |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| None | None |