rfOADClientIntFlashUApp
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
Example Summary
The rfOADClientIntFlashUApp project, together with the rfOADServer project, illustrates how on-chip over-the-air download works. This example works by receiving a firmware image from the OAD Server, invalidating the current firmware, and placing the new firmware where the old one was (internal flash). On reset, the bootloader then validates the new user firmware and boots into it.
Peripherals Exercised
CONFIG_GPIO_GLED
- Toggled when data is transmitted over the RF interfaceCONFIG_GPIO_RLED
- Toggled when data is received over the RF interface
Board Specific Settings
- The default frequency is:
- 433.92 MHz for the CC1350-LAUNCHXL-433 and the CC1352P-4-LAUNCHXL
- 2440 MHz on the CC2640R2-LAUNCHXL and the CC26X2R1-LAUNCHXL
- 868.0 MHz for other launchpads In order to change frequency, modify the ti_radio_config.c file. This can be done using the code export feature in Smart RF Studio, or directly in the file
- On the CC1352P1 the high PA is enabled (high output power) for all Sub-1 GHz modes by default.
- On the CC1352P-2 and CC1352P-4 the high PA operation for Sub-1 GHz modes is not supported
- The CC2640R2 is setup to run all proprietary physical modes at a center frequency of 2440 MHz, at a data rate of 250 Kbps
Required Firmware Images
The rfOADClientIntFlashUApp example requires three firmware images to be flashed onto the client:
1. BIM Image
* Prebuilt: <SDK_INSTALL_DIR>/examples/nortos/<PLATFORM>/bim/hexfiles/bim_onchip/Release/bim_onchip.hex
* Project (Release Configuration): <SDK_INSTALL_DIR>/examples/nortos/<PLATFORM>/bim/bim_onchip
2. A Signed rfOADClientIntFlashUApp Image
* Run oad_image_tool.py on the rfOADClientIntFlashUApp image that was built from this example. The oad_image_tool.py tool will sign the image.
```
cd <SDK_INSTALL_DIR>/tools/common/oad
```
```
python oad_image_tool.py -hex1 <CCS_WORKSPACE>\rfOADClientIntFlashUApp_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClientIntFlashUApp_<PLATFORM>_tirtos7_ticlang.hex -o rfOADClientIntFlashUApp_<PLATFORM>_tirtos7_ticlang_signed_v1 -k private.pem ccs output_directory 7
```
NOTE: For UApp, the BinaryType is "Application + Merged" or 7. Run ```python oad_image_tool.py -h``` for more information on the script's usage.
* Create a version 2 of the rfOADClientIntFlashUApp
* Make your firmware updates
* Modify the value of ```#define SOFTWARE_VER``` in ```oad_image_header_app.c```
* Rebuild the rfOADClientIntFlashUApp project to get a new image
* Run **oad_image_tool.py** again on the new image
```
python oad_image_tool.py -hex1 <CCS_WORKSPACE>\rfOADClientIntFlashUApp_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClientIntFlashUApp_<PLATFORM>_tirtos7_ticlang.hex -o rfOADClientIntFlashUApp_<PLATFORM>_tirtos7_ticlang_signed_v2 -k private.pem ccs output_directory 7
```
3. A Signed rfOADClientIntFlashPApp Image
* Project: <SDK_INSTALL_DIR>/examples/rtos/<PLATFORM>/prop_rf/rfOADClientIntFlashPApp
* Run oad_image_tool.py on the rfOADClientIntFlashPApp that was built from the rfOADClientIntFlashPApp example. The oad_image_tool.py tool will sign the image.
NOTE: For PApp, the BinaryType is "Persistent App" or 0. Run python oad_image_tool.py -h
for more information on the script's usage.
cd <SDK_INSTALL_DIR>/tools/common/oad
python oad_image_tool.py -hex1 <CCS_WORKSPACE>\rfOADClientIntFlashPApp_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClientIntFlashPApp_<PLATFORM>_tirtos7_ticlang.hex -o rfOADClientIntFlashPApp_<PLATFORM>_tirtos7_ticlang_signed -k private.pem ccs output_directory 0
Flashing the Images
Once you have the BIM, the signed rfOADClientIntFlashUApp image, and the signed rfOADClientIntFlashPApp image, use Uniflash to load all three images onto the target device. Depending on the target device, the locations where these images must be flashed vary. Refer to the flash layout below.
CC13x2_CC26x2
CC13x1_CC26x1 CC13x2x7_CC26x2x7
+-----------------------+ +-----------------------+
| BIM + CCFG | | BIM + CCFG |
+-----------------------+ 0x00056000 +-----------------------+ 0x000AE000: BIM Flash Location
| | | |
| | | |
| PersistentApp | | PersistentApp |
+-----------------------+ +-----------------------+
| PApp Image Header | | PApp Image Header |
+-----------------------+ 0x00044000 +-----------------------+ 0x0009C000: PApp Flash Location
| NVS | | NVS |
+-----------------------+ +-----------------------+
| | | |
| | | |
| UserApp | | UserApp |
+-----------------------+ +-----------------------+
| UApp Image Header | | UApp Image Header |
+-----------------------+ 0x00000000 +-----------------------+ 0x00000000: UApp Flash Location
Example Usage
Once the rfOADClientIntFlashUApp application starts up, it waits for OAD packets from the OAD Server. On another board then, run the OAD Server example. Refer to rfOADServer README for information on how to use it.
Application Design Details
Init
|
|
+---------> Wait for OAD/Radio Events
| |
| V
| Process OAD Client & Radio Events
| |
| V
| +-----------+----------+---------------------+------------------------+-------------------+
| | | | | |
| V V V V V
| Block Rsp FW Version Req Img Identify Req Block Req Reset Req
| | | | | |
| | V V V V
| | Send FW Version Send Img Identify Rsp Send Block Req Send Reset Rsp
| | | | | |
| V | | | |
| Write Img Block | | | |
| to Internal Flash | | | |
| +---------------------+------------------------+-------------------+
| |
| V
+-----> Packet RX Packet TX