HCI Extension Vendor Specific API

HCI Extension Commands

In addition to the BLE HCI commands, the following HCI Extension vendor specific commands are also available.

HCI_EXT_SetRxGainCmd

Opcode:

0xFC00

Command Description:

Set the receiver gain.

Command Parameters

RX Gain:

Set RX gain to standard or high.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

RX Gain Standard

1

RX Gain High

Events Generated

When this command has completed, an HCI_EXT_SetRxGainDone event shall be generated.

HCI_EXT_SetTxPowerCmd

Opcode:

0xFC01

Command Description:

This command is used to set the RF transmitter output power.

Command Parameters

TX Power:

Tx power to use.

Size:

1 byte(s)

Default:

2

Range:

Value

Description

0

-20 dBm

1

-18 dBm

2

-15 dBm

3

-12 dBm

4

-10 dBm

5

-9 dBm

6

-6 dBm

7

-5 dBm

8

-3 dBm

9

0 dBm

10

1 dBm

11

2 dBm

12

3 dBm

13

4 dBm

14

5 dBm

15

CC26xx: N/A CC13x2P_2: 14 dBm CC13x2P_4: 6 dBm

16

CC26xx: N/A CC13x2P_2: 15 dBm CC13x2P_4: 7 dBm

17

CC26xx: N/A CC13x2P_2: 16 dBm CC13x2P_4: 8 dBm

18

CC26xx: N/A CC13x2P_2: 17 dBm CC13x2P_4: 9 dBm

19

CC26xx: N/A CC13x2P_2: 18 dBm CC13x2P_4: 10 dBm

20

CC26xx: N/A CC13x2P_2: 19 dBm CC13x2P_4: N/A

21

CC26xx: N/A CC13x2P_2: 20 dBm CC13x2P_4: N/A

Events Generated

When this command has completed, an HCI_EXT_SetTxPowerDone event shall be generated.

HCI_EXT_OnePktPerEvtCmd

Opcode:

0xFC02

Command Description:

This command is used to configure the Link Layer to only allow one packet per connection event. This command can be used to trade-off throughput and power consumption during a connection. When enabled, power can be conserved during a connection by limiting the number of packets per connection event to one, at the expense of more limited throughput. When disabled, the number of packets transferred during a connection event is not limited, at the expense of higher power consumption. Note that when set, all connections will be restricted to one packet per event.

Command Parameters

Control:

Enable or disable allowing only one packet per event.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Disable

1

Enable

Events Generated

When this command has completed, an HCI_EXT_OnePacketPerEventDone event shall be generated.

HCI_EXT_DecryptCmd

Opcode:

0xFC05

Command Description:

This command is used to decrypt encrypted text using AES128.

Command Parameters

Key:

128 bit key for the decryption of the data given in the command. The most significant octet of the data corresponds to key[0] using the notation specified in FIPS 197.

Size:

16 byte(s)

Default:

“BF:01:FB:9D:4E:F3:BC:36:D8:74:F5:39:41:38:68:4C”

Range:

Any 16 byte value

Data:

128 bit encrypted data to be decrypted. The most significant octet of the key corresponds to key[0] using the notation specified in FIPS 197.

Size:

16 byte(s)

Default:

“66:C6:C2:27:8E:3B:8E:05:3E:7E:A3:26:52:1B:AD:99”

Range:

Any 16 byte value

Events Generated

When this command has completed, an HCI_EXT_DecryptCommandDone event shall be generated.

HCI_EXT_SetLocalSupportedFeaturesCmd

Opcode:

0xFC06

Command Description:

This command is used to set the Controllers Local Supported Features. For a complete list of supported LE features, please see [1], Part B, Section 4.6. Note: This command can be issued either before or after one or more connections are formed. However, the local features set in this manner are only effective if performed before a Feature Exchange Procedure has been initiated by the Master. Once this control procedure has been completed for a particular connection, only the exchanged feature set for that connection will be used. Since the Link Layer may initiate the feature exchange procedure autonomously, it is best to use this command before the connection is formed.

Command Parameters

FeatureSet:

Write LL local supported features.

Size:

8 byte(s)

Default:

0x0000000000000001

Range:

Value

Description

0x0000000000000000

No Events Specified

0x0000000000000001

Encryption

0x0000000000000002

Connection Parameters Request

0x0000000000000004

Reject Extended Indication

0x0000000000000008

Slave Features Exchange

0x0000000000000010

Ping

0x0000000000000020

Data Packet Length Extension

0x0000000000000040

Privacy

0x0000000000000080

Extended Scanner Filter Policies

0x0000000000000100

2M PHY

0x0000000000000200

Stable Modulation Index Tx

0x0000000000000400

Stable Modulation Index Rx

0x0000000000000800

Coded PHY

0x0000000000001000

Extended Advertising

0x0000000000002000

Periodic Advertising

0x0000000000004000

Channel Selection Algorithm #2

0x0000000000008000

LE Power Class 1

0x0000000000010000

Minimum Number of Used Channels

0x0000000000020000

Connection CTE Request

0x0000000000040000

Connection CTE Response

0x0000000000080000

Connectionless CTE Transmitter

0x0000000000100000

Connectionless CTE Receiver

0x0000000000200000

Antenna Switching During CTE Tx

0x0000000000400000

Antenna Switching During CTE Rx

0x0000000000800000

Receiving CTE

Events Generated

When this command has completed, an HCI_EXT_WriteLocalFeatureSupportDone event shall be generated.

HCI_EXT_ModemTestTxCmd

Opcode:

0xFC08

Command Description:

This API is used to start a continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel. Use the HCI_EXT_EndModemTest command to end the test. Note: The RF channel, not the BLE frequency, is specified! You can obtain the RF channel from the BLE frequency as follows: RF Channel = (BLE Frequency - 2402) / 2. Note: When the HCI_EXT_EndModemTest is issued to stop this test, a Controller reset will take place. Note: The device will transmit at the default output power (0 dBm) unless changed by HCI_EXT_SetTxPowerCmd. Note: This modem test can be used to satisfy in part radio regulation requirements as specific in standards such as ARIB STD-T66.

Command Parameters

CW Mode:

Set Modem Test CW modulation.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Modulated Transmit Carrier

1

Unmodulated Transmit Carrier

TX RF Channel:

RF channel of transmit frequency.

Size:

1 byte(s)

Default:

0

Range:

0-39

Events Generated

When this command has completed, an HCI_EXT_ModemTestTxDone event shall be generated.

HCI_EXT_ModemHopTestTxCmd

Opcode:

0xFC09

Command Description:

This API is used to start a continuous transmitter direct test mode test using a modulated carrier wave and transmitting a 37 byte packet of pseudo-random 9 bit data. A packet is transmitted on a different frequency (linearly stepping through all RF channels 0..39) every 625us. Use the HCI_EXT_EndModemTest command to end the test. Note: When the HCI_EXT_EndModemTest is issued to stop this test, a Controller reset will take place. Note: The device will transmit at the default output power (0 dBm) unless changed by HCI_EXT_SetTxPowerCmd. Note: This modem test can be used to satisfy in part radio regulation requirements as specific in standards such as ARIB STD-T66.

Events Generated

When this command has completed, an HCI_EXT_ModemHopTestTxDone event shall be generated.

HCI_EXT_ModemTestRxCmd

Opcode:

0xFC0A

Command Description:

This API is used to start a continuous receiver modem test using a modulated carrier wave tone, at the frequency that corresponds to the specific RF channel. Any received data is discarded. Receiver gain may be adjusted using the HCI_EXT_SetRxGain command. RSSI may be read during this test by using the HCI_ReadRssi command. Use HCI_EXT_EndModemTest command to end the test. Note: The RF channel, not the BLE frequency, is specified! You can obtain the RF channel from the BLE frequency as follows: RF Channel = (BLE Frequency - 2402) / 2. Note: When the HCI_EXT_EndModemTest is issued to stop this test, a Controller reset will take place. Note: This modem test can be used to satisfy in part radio regulation requirements as specific in standards such as ARIB STD-T66.

Command Parameters

RX RF Channel:

RF channel of receive frequency.

Size:

1 byte(s)

Default:

0

Range:

0-39

Events Generated

When this command has completed, an HCI_EXT_ModemTestRxDone event shall be generated.

HCI_EXT_EnhancedModemTestTxCmd

Opcode:

0xFC27

Command Description:

This API is used start the enhanced BLE5 continuous transmitter modem test, using either a modulated or unmodulated carrier wave tone, at the frequency that corresponds to the specified RF channel, for a given PHY (1M, 2M, Coded S2, or Coded S8). Use LL_EXT_EndModemTest to end the test.Note: A Controller reset will be issued by the HCI_EXT_EndModemTest command! Note: The BLE device will transmit at the current TX power setting. Note: This API can be used to verify this device meets Japan’s TELEC regulations.

Command Parameters

CW Mode:

Set Enhanced Modem Test Tx CW modulation.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Modulated Transmit Carrier

1

Unmodulated Transmit Carrier

RF PHY:

PHY to transmit on

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

1 Mbps Phy

0x01

2 Mbps Phy

0x02

Coded S8 Phy (125kpbs)

0x06

Coded S2 Phy (500 kbps)

RF Channel:

RF channel of transmit frequency.

Size:

1 byte(s)

Default:

0

Range:

0-39

Events Generated

When this command has completed, an HCI_EXT_EnhancedModemTestTxDone event shall be generated.

HCI_EXT_EnhancedModemHopTestTxCmd

Opcode:

0xFC28

Command Description:

This API is used to start the enhanced continuous transmitter direct test mode test using a modulated carrier wave. A test reference data packet is transmitted on a different frequency (linearly stepping through all RF channels 0..39), for a given PHY (1M, 2M, Coded S2, or Coded S8), every period (depending on the payload length, as given Vol. 6, Part F, section 4.1.6). Use LL_EXT_EndModemTest to end the test. Note: A Controller reset will be issued by the HCI_EXT_EndModemTest command! Note: The BLE device will transmit at the current TX power setting. Note: This API can be used to verify this device meets Japan’s TELEC regulations.

Command Parameters

Payload Length:

Data payload length in bytes

Size:

1 byte(s)

Default:

37

Range:

0-37

Payload Type:

DTM Packet Pattern Type

Size:

1 byte(s)

Default:

0x00

Range:

Value

Description

0x00

PRBS9

0x01

0x0F

0x02

0x55

0x03

PRBS15

0x04

0xFF

0x05

0x00

0x06

0xF0

0x07

0xAA

RF PHY:

PHY to transmit on

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

1 Mbps Phy

0x01

2 Mbps Phy

0x02

Coded S8 Phy (125kpbs)

0x06

Coded S2 Phy (500 kbps)

Events Generated

When this command has completed, an HCI_EXT_EnhancedModemHopTestTxDone event shall be generated.

HCI_EXT_EnhancedModemTestRxCmd

Opcode:

0xFC29

Command Description:

This API is used to start the enhanced BLE5 continuous receiver modem test using a modulated carrier wave tone, at the frequency that corresponds to the specific RF channel, for a given PHY (1M, 2M, Coded S2, or Coded S8). Any received data is discarded. RSSI may be read during this test by using the LL_ReadRssi command. Use LL_EXT_EndModemTest command to end the test. Note: A Controller reset will be issued by LL_EXT_EndModemTest!

Command Parameters

RF PHY:

PHY to transmit on

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

1 Mbps Phy

0x01

2 Mbps Phy

0x02

Coded S8 Phy (125kpbs)

0x06

Coded S2 Phy (500 kbps)

RF Channel:

RF Channel

Size:

1 byte(s)

Default:

0

Range:

0 to 39

Events Generated

When this command has completed, an HCI_EXT_EnhancedModemTestRxDone event shall be generated.

HCI_EXT_EndModemTestCmd

Opcode:

0xFC0B

Command Description:

This API is used to end a modem test. A Controller reset will take place.

Events Generated

When this command has completed, an HCI_EXT_EndModemTestDone event shall be generated.

HCI_EXT_SetBDADDRCmd

Opcode:

0xFC0C

Command Description:

This command is used to set this devices BLE address (BDADDR). This address will override the devices address determined when the device is reset (i.e. a hardware reset, not an HCI Controller Reset). To restore the devices initialized address, issue this command with an invalid address. Note: This command is only allowed when the Controller is in the Standby state. Note: This command is intended to only be used during initialization. Changing the devices BDADDR after various BLE operations have already taken place may cause unexpected problems.

Command Parameters

BDADDR:

BLE Public Address (MSB..LSB). Use “FF:FF:FF:FF:FF:FF” to restore the device address to that which was determined at initialization.

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

Events Generated

When this command has completed, an HCI_EXT_SetBDADDRDone event shall be generated.

HCI_EXT_SetVirtualAdvAddrCmd

Opcode:

0xFC73

Command Description:

This API is used to set the advertiser’s virtual public address. Note: This command is only allowed when the advertise set is not active and its PDU type is Legacy Non-Connectable and Non-Scanable.

Command Parameters

Handle:

Adv handle to which address will be assigned

Size:

1 byte(s)

Default:

“0”

Range:

From 0 to 20 sets

BDADDR:

Advertiser’s virtual public address

Size:

6 byte(s)

Default:

“00:00:00:00:00:00”

Range:

Any 6 byte value

Events Generated

When this command has completed, an HCI_EXT_SetVirtualAdvAddrDone event shall be generated.

HCI_EXT_SetQOSParameters

Opcode:

0xFC75

Command Description:

This API is used to set the QOS Parameters according to the entered parameter type.

Command Parameters

taskType:

The type of task: 0=LL_QOS_CONN_TASK_TYPE, 1=LL_QOS_ADV_TASK_TYPE, 2=LL_QOS_SCN_TASK_TYPE, 3=LL_QOS_INIT_TASK_TYPE, 4=LL_QOS_PERIODIC_ADV_TASK_TYPE, 5=LL_QOS_PERIODIC_SCN_TASK_TYPE.

Size:

1 byte(s)

Default:

“0”

Range:

From 0 to 5.

paramType:

The type of parameter: 0=LL_QOS_TYPE_PRIORITY, 1=LL_QOS_TYPE_CONN_MIN_LENGTH, 2=LL_QOS_TYPE_CONN_MAX_LENGTH.

Size:

1 byte(s)

Default:

“0”

Range:

From 0 to 2: LL_QOS_TYPE_PRIORITY, LL_QOS_TYPE_CONN_MIN_LENGTH, LL_QOS_TYPE_CONN_MAX_LENGTH.

ParamVal:

The parameter value. For LL_QOS_TYPE_PRIORITY: 0=Low, 1=Medium, 2=High. For LL_QOS_TYPE_CONN_MIN_LENGTH/LL_QOS_TYPE_CONN_MAX_LENGTH: time in [us].

Size:

4 byte(s)

Default:

“0”

Range:

For LL_QOS_TYPE_PRIORITY: LL_QOS_LOW_PRIORITY (=0), LL_QOS_MED_PRIORITY (=1), LL_HIGH_LOW_PRIORITY (=2). For LL_QOS_TYPE_CONN_MIN_LENGTH: For coded connection the range LL_MIN_LINK_DATA_TIME_CODED (2704 us) - LL_MAX_LINK_DATA_TIME_CODED (17040 us).For uncoded connection the range LL_MIN_LINK_DATA_TIME (328 us) - LL_MAX_LINK_DATA_TIME_UNCODED (2120 us). For LL_QOS_TYPE_CONN_MAX_LENGTH: For coded connection the range LL_MIN_LINK_DATA_TIME_CODED (2704 us) - connection’s interval (us). For uncoded connection the range LL_MIN_LINK_DATA_TIME (328 us) - connection’s interval.

taskHandle:

The task handle to be changed (secondary and primary tasks). For connection enter the connection’s Id.

Size:

2 byte(s)

Default:

“0”

Range:

From 0 to 20

Events Generated

When this command has completed, an HCI_EXT_SetQOSParametersDone event shall be generated.

HCI_EXT_SetQOSDefaultParameters

Opcode:

0xFC76

Command Description:

This API is used to set the default QOS Parameters values.

Command Parameters

paramDefaultVal:

The parameter default value. For LL_QOS_TYPE_PRIORITY: 0=Low, 1=Medium, 2=High.

Size:

4 byte(s)

Default:

“0”

Range:

For LL_QOS_TYPE_PRIORITY: LL_QOS_LOW_PRIORITY (=0), LL_QOS_MED_PRIORITY (=1), LL_HIGH_LOW_PRIORITY (=2).

paramType:

The type of parameter: 0=LL_QOS_TYPE_PRIORITY

Size:

1 byte(s)

Default:

“0”

Range:

From 0 to 0: LL_QOS_TYPE_PRIORITY

taskType:

The type of task: 0=LL_QOS_CONN_TASK_TYPE, 1=LL_QOS_ADV_TASK_TYPE, 2=LL_QOS_SCN_TASK_TYPE, 3=LL_QOS_INIT_TASK_TYPE, 4=LL_QOS_PERIODIC_ADV_TASK_TYPE, 5=LL_QOS_PERIODIC_SCN_TASK_TYPE.

Size:

1 byte(s)

Default:

“0”

Range:

From 0 to 5

Events Generated

When this command has completed, an HCI_EXT_SetQOSDefaultParameters event shall be generated.

HCI_EXT_SetHostDefChanClassificationCmd

Opcode:

0xFC79

Command Description:

This API is used to set the default channel map to use in future connections.

Command Parameters

Channel Map:

The channel map to set as default. bit map for each channel. 1 to use channel, 0 to not use.

Size:

5 byte(s)

Default:

“00:00:00:00:01”

Range:

Any 6 byte value, will use only 37 LSb, one for each channel.

Events Generated

When this command has completed, an HCI_EXT_SetHostDefChanClassificationCmd event shall be generated.

HCI_EXT_SetHostConnChanClassificationCmd

Opcode:

0xFC7A

Command Description:

This API is used to set the channel map of a specific active connection.

Command Parameters

Channel Map:

The channel map to set as default. bit map for each channel. 1 to use channel, 0 to not use.

Size:

5 byte(s)

Default:

“00:00:00:00:01”

Range:

Any 6 byte value, will use only 37 LSb, one for each channel.

Handle:

Local identifier of the LL connection

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

Events Generated

When this command has completed, an HCI_EXT_SetHostConnChanClassificationCmd event shall be generated.

HCI_EXT_SetSCACmd

Opcode:

0xFC0D

Command Description:

This command is used to set this devices Sleep Clock Accuracy (SCA) value, in parts per million (PPM), from 0 to 500. For a Master device, the value is converted to one of eight ordinal values representing a SCA range (per [1], Volume 6, Part B, Section 2.3.3.1, Table 2.2), which will be used when a connection is created. For a Slave device, the value is directly used. The system default value for a Master and Slave device is 50ppm and 40ppm, respectively. Note: This command is only allowed when the device is not in a connection. Note: The devices SCA value remains unaffected by an HCI Reset.

Command Parameters

SCA:

BLE Device Sleep Clock Accuracy (PPM).

Size:

2 byte(s)

Default:

“40”

Range:

(0..500)

Events Generated

When this command has completed, an HCI_EXT_SetSCADone event shall be generated.

HCI_EXT_EnablePTMCmd

Opcode:

0xFC0E

Command Description:

This command is used to enable Production Test Mode (PTM). This mode is used by the customer during assembly of their product to allow limited access to the BLE Controller for testing and configuration. This command is only available when the BLE Controller is built without external access to the Controller (i.e. when no transport interface such as RS232 is permitted). This mode will remain enabled until the device is reset. Please see the related application note for additional details. Note: This command is only allowed as a direct function call, and is only intended to be used by an embedded application. No vendor specific Command Complete event will be generated.

Events Generated

When this command has completed, will simply return. No vendor specific Command Complete event will be generated.

HCI_EXT_SetMaxDtmTxPowerCmd

Opcode:

0xFC11

Command Description:

This command is used to override the RF transmitter output power used by the Direct Test Mode (DTM). Normally, the maximum transmitter output power setting used by DTM is the maximum transmitter output power setting for the device (i.e. 4 dBm for the CC2540; 0 dBm for the CC2541; 5 dBm for the CC264x). This command will change the value used by DTM. Note: When DTM is ended by a call to HCI_LE_TestEndCmd, or a HCI_Reset is used, the transmitter output power setting is restored to the default value of 0 dBm.

Command Parameters

TX Power:

Set TX power to -23, -6, 0, or 4 dBm.

Size:

1 byte(s)

Default:

3

Range:

Value

Description

0

-20 dBm

1

-18 dBm

2

-15 dBm

3

-12 dBm

4

-10 dBm

5

-9 dBm

6

-6 dBm

7

-5 dBm

8

-3 dBm

9

0 dBm

10

1 dBm

11

2 dBm

12

3 dBm

13

4 dBm

14

5 dBm

15

CC26xx: N/A CC13x2P_2: 14 dBm CC13x2P_4: 6 dBm

16

CC26xx: N/A CC13x2P_2: 15 dBm CC13x2P_4: 7 dBm

17

CC26xx: N/A CC13x2P_2: 16 dBm CC13x2P_4: 8 dBm

18

CC26xx: N/A CC13x2P_2: 17 dBm CC13x2P_4: 9 dBm

19

CC26xx: N/A CC13x2P_2: 18 dBm CC13x2P_4: 10 dBm

20

CC26xx: N/A CC13x2P_2: 19 dBm CC13x2P_4: N/A

21

CC26xx: N/A CC13x2P_2: 20 dBm CC13x2P_4: N/A

Events Generated

When this command has completed, an HCI_EXT_SetMaxDtmTxPowerDone event shall be generated.

HCI_EXT_DisconnectImmedCmd

Opcode:

0xFC13

Command Description:

This command is used to disconnect a connection immediately. This command can be useful for when a connection needs to be ended without the latency associated with the normal BLE Controller Terminate control procedure. Note that the Host issuing the command will still receive the HCI Disconnection Complete event with a Reason status of 0x16 (i.e. Connection Terminated by Local Host), followed by an HCI Vendor Specific Event.

Command Parameters

Connection Handle:

Handle used to identify a connection

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

Events Generated

When this command has completed, an HCI_EXT_DisconnectImmedDone event shall be generated.

HCI_EXT_PacketErrorRateCmd

Opcode:

0xFC14

Command Description:

This command is used to Reset or Read the Packet Error Rate counters for a connection. When Reset, the counters are cleared; when Read, the total number of packets received, the number of packets received with a CRC error, the number of events, and the number of missed events are returned. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended.

Command Parameters

Connection Handle:

Handle used to identify a connection

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

PER Test Command:

Reset or Read the PER counters.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Reset PER Counters

1

Read PER Counters

Events Generated

When this command has completed, an HCI_EXT_PER event shall be generated.

HCI_EXT_SetSlaveLatencyOverrideCmd

Opcode:

0xFC1A

Command Description:

This command is used to enable or disable the Slave Latency Override, allowing the user to ensure that Slave Latency is not applied even though it is active. The default value is Disable. Note: This command will be disallowed for no connection, or the connection is not in the Slave role.

Command Parameters

Control:

Enable or disable suspending slave latency.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Disable

1

Enable

Events Generated

When this command has completed, an HCI_EXT_OverrideSLDone event shall be generated.

HCI_EXT_BuildRevisionCmd

Opcode:

0xFC1B

Command Description:

This command is used to a) allow the embedded user code to set their own 16 bit revision number, and b) to read the build revision number of the BLE stack library software. The default value of the user revision number is zero. When the user updates a BLE project by adding their own code, they may use this API to set their own revision number. When called with mode set to HCI_EXT_SET_APP_REVISION, the stack will save this value. No event will be returned from this API when used this way as it is intended to be called from within the target itself. Note however that this does not preclude this command from being received via the HCI. However, no event will be returned. When this API is used from the HCI, then the second parameter is ignored, and a vendor specific event is returned with the users revision number and the build revision number of the BLE stack.

Command Parameters

Mode:

Set User Revision or Get Build Revision.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Set User Revision Number

1

Read Build Revision

UserRevNum:

User Revision Number.

Size:

2 byte(s)

Default:

0

Range:

Any 16 bit value

Events Generated

When this command has completed, an HCI_EXT_BuildRevisionDone event shall be generated but only when the value of mode is HCI_EXT_READ_BUILD_REVISION.

HCI_EXT_ResetSystemCmd

Opcode:

0xFC1D

Command Description:

This command is used to issue a hard or soft system reset. A hard reset is caused by setting the SYSRESET bit in the System Controller Reset Control register. The soft reset is currently not supported on the CC264x.

Command Parameters

type:

Reset Type

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

Chip Reset

0x01

Soft Reset

Events Generated

When this command has completed, an HCI_EXT_ResetSystemDone event shall be generated.

HCI_EXT_NumComplPktsLimitCmd

Opcode:

0xFC1F

Command Description:

This command is used to set the limit on the minimum number of complete packets before a Number of Completed Packets event is returned by the Controller. If the limit is not reached by the end of a connection event, then the Number of Completed Packets event will be returned (if non-zero) based on the flushOnEvt flag. The limit can be set from one to the maximum number of HCI buffers (please see the LE Read Buffer Size command in the Bluetooth Core specification). The default limit is one; the default flushOnEvt flag is FALSE.

Command Parameters

Limit:

Set Number of Completed Packets Limit.

Size:

1 byte(s)

Default:

1

Range:

0x01 to the value returned from HCI_LE_ReadBufSizeCmd

flushOnEvt:

Enable or disable flush of Number of Completed Packets at end of Event.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Disable

1

Enable

Events Generated

When this command has completed, an HCI_EXT_NumComplPktsLimitDone event shall be generated.

HCI_EXT_GetConnInfoCmd

Opcode:

0xFC20

Command Description:

This command (which replaces Get Number Connections) is used to get the number of allocated connections, the number of active connections, and for each active connection, the connection handle, the connection role, the peer device address and peer device address type. The number of allocated connections is based on a default build value that can be changed in the project using MAX_NUM_BLE_CONNS (please see the software users guide for additional details). The number of active connections refers to active BLE connections. The information per connection is based on the structure hciConnInfo_t provided in hci.h. If all parameters are NULL, then the call to this command is considered a network processor call via a transport layer, and the results will be provided via a vendor specific command complete event.If any parameter is not NULL, then the call to this command is considered a direct function call and the valid pointers will be used to store the result. In this case, it is the users responsibility to ensure there is sufficient memory allocated! Note that partial results can be obtained by selective use of the pointers. For example, if only the number of active connections is desired, this can be obtained as follows:

Events Generated

When this command has completed, an HCI_EXT_GetConnInfoDone event shall be generated.

HCI_EXT_SetMaxDataLenCmd

Opcode:

0xFC21

Command Description:

This command is used to set the Data Length Extension internal variables supportedMaxTxOctets, supportedMaxTxTime, supportedMaxRxOctets and supportedMaxRxTime that are normally set exclusively by the Controller to the maximum data length and duration allowed by this device (default Tx and Rx Octets is 251; default Tx and Rx Time is 2120 us [but note that any future change to support PHYs could alter the default values of Time]).

Command Parameters

Tx Octets:

Maximum number of payload octets that the local Controller supports for transmission of a single Link Layer Data Channel PDU.

Size:

2 byte(s)

Default:

0

Range:

0x001B to 0x00FB

Tx Time:

Maximum time, in microseconds, that the local Controller supports for transmission of a single Link Layer Data Channel PDU.

Size:

2 byte(s)

Default:

0

Range:

0x0148 to 0x0848

Rx Octets:

Maximum number of payload octets that the local Controller supports for reception of a single Link Layer Data Channel PDU.

Size:

2 byte(s)

Default:

0

Range:

0x001B to 0x00FB

Rx Time:

Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer Data Channel PDU.

Size:

2 byte(s)

Default:

0

Range:

0x0148 to 0x0848

Events Generated

When this command has completed, an HCI_EXT_SetMaxDataLengthDone event shall be generated.

HCI_EXT_SetDtmTxPktCntCmd

Opcode:

0xFC24

Command Description:

This API is used to set the DTM TX packet count.

Command Parameters

TX Packet Count:

Number of DTM packets to transmit

Size:

2 byte(s)

Default:

0

Range:

Value

Description

0x0000

Continuous Tx

Events Generated

When this command has completed, an HCI_EXT_SetDtmTxPktCntDone event shall be generated.

HCI_EXT_SetPinOutputCmd

Opcode:

0xFC2A

Command Description:

This API is used to set GPIO as output.

Command Parameters

Pin:

Pin Number

Size:

1 byte(s)

Default:

0

Range:

0x00 to 0x1F

Value:

initialize value 0 or 1

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0x00

Output Low

0x01

Output High

0xFF

Input

Events Generated

When this command has completed, an HCI_EXT_SetPinOutputDone event shall be generated.

HCI_EXT_SetLocationingAccuracyCmd

Opcode:

0xFC2B

Command Description:

This API is used to set CTE accuracy.

Command Parameters

handle:

connection handle (0x0XXX) or periodic advertising train handle (0x1XXX)

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x1EFF

CTE PHY:

Indicate which PHY to configure.

Size:

0 byte(s)

Default:

0x01

Range:

Value

Description

0x01

LE 1M

0x02

LE 2M

1M:sample rate:

Accuracy between 1 (least accuracy as in 5.1 spec) to 4 (most accuracy)

Condition:

( (phyMask & 0x1) == 0x01)

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

1us AoD transmission

0x02

1us AoD reception

0x04

1us AoA reception

1M:sample size:

Size 8 bits (as in 5.1 spec) or 16 bits (more accurate)

Condition:

( (phyMask & 0x1) == 0x01)

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

8 bits

0x02

16 bits

1M:sample rate:
Condition:

( (phyMask & 0x1) != 0x01)

Size:

1 byte(s)

Value:

0

1M:sample size:
Condition:

( (phyMask & 0x1) != 0x01)

Size:

1 byte(s)

Value:

0

2M:sample rate:

Accuracy between 1 (least accuracy as in 5.1 spec) to 4 (most accuracy)

Condition:

( (phyMask & 0x2) == 0x02)

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

1us AoD transmission

0x02

1us AoD reception

0x04

1us AoA reception

2M:sample size:

Size 8 bits (as in 5.1 spec) or 16 bits (more accurate)

Condition:

( (phyMask & 0x2) == 0x02)

Size:

1 byte(s)

Default:

1

Range:

Value

Description

0x01

8 bits

0x02

16 bits

2M:sample rate:
Condition:

( (phyMask & 0x2) != 0x02)

Size:

1 byte(s)

Value:

0

2M:sample size:
Condition:

( (phyMask & 0x2) != 0x02)

Size:

1 byte(s)

Value:

0

sample control:

0x00-default filtering(skip antenna switching samples, …), 0x01-RAW_RF no filtering

Size:

1 byte(s)

Default:

0x00

Range:

0x00 to 0x01

Events Generated

When this command has completed, an HCI_EXT_SetLocationingAccuracyDone event shall be generated.

HCI_EXT_GetActiveConnInfoCmd

Opcode:

0xFC2C

Command Description:

This API is used to get connection information needed to track an active BLE connection.

Command Parameters

connId:
Size:

1 byte(s)

Default:

0

Range:

0x0000 to 0x0EFF

Events Generated

When this command has completed, an HCI_EXT_GetActiveConnInfoDone event shall be generated.

HCI_EXT_GetRxStatisticsCmd

Opcode:

0xFC31

Command Description:

This command is used to Reset or Read the RX statistics counters for a connection. When Reset, the counters are cleared; when Read, the total number of ok packets received, the number of control packets received, the number of control packets received that were ACKed, the number of packets received with a CRC error, the number of packets that were ignored, the number of empty packets that were received, and the number of discarded packets are returned. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended.

Command Parameters

Connection Handle:

Handle used to identify a connection

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

RX Stats Test Command:

Reset or Read the RX statistics counters.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Reset Statistics Counters

1

Read Statistics Counters

Events Generated

When this command has completed, an HCI_EXT_GET_RX_STATS event shall be generated.

HCI_EXT_GetTxStatisticsCmd

Opcode:

0xFC32

Command Description:

This command is used to Reset or Read the RX statistics counters for a connection. When Reset, the counters are cleared; when Read, the total number of ok packets transmitted, the number of transmitted packets ACKed, the number of control packets transmitted, the number of control packets transmitted ACKed, the number of control packets transmitted ACKed that were ACKed, the number of packets retransmissions, and the number of packets on Tx queue that are finished. The system default value upon hardware reset is Reset. Note: The counters are only 16 bits. At the shortest connection interval, this provides a little over 8 minutes of data. Note: This command is only valid for a valid connection handle (i.e. for an active connection). It is therefore not possible to read the packet error rate data once the connection has ended.

Command Parameters

Connection Handle:

Handle used to identify a connection

Size:

2 byte(s)

Default:

0x0000

Range:

0x0000 to 0x0EFF

TX Stats Test Command:

Reset or Read the TX statistics counters.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Reset Statistics Counters

1

Read Statistics Counters

Events Generated

When this command has completed, an HCI_EXT_GET_TX_STATS event shall be generated.

HCI_EXT_GetCoexStatisticsCmd

Opcode:

0xFC33

Command Description:

This command is used to Reset or Read the COEX statistics counters for a connection. When Reset, the counters are cleared; when Read, the total number of grants (CC33xx: grants_asserted), the total number of rejects (CC33xx: request_deassrted), the total number of continuously rejected requests (CC33xx: grants_deasserted), and the number of max continuously rejected requests (CC33xx: request_assrted). The system default value upon hardware reset is Reset.

Command Parameters

Coex Stats Test Command:

Reset or Read the Coex statistics counters.

Size:

1 byte(s)

Default:

0

Range:

Value

Description

0

Reset Statistics Counters

1

Read Statistics Counters

Events Generated

When this command has completed, an HCI_EXT_GET_COEX_STATS event shall be generated.

HCI_EXT_CoexEnableCmd

Opcode:

0xFC2E

Command Description:

This API is used to enable or disable the Coex feature.

Command Parameters

Enable:

1 for enable and 0 for disable

Size:

1 byte(s)

Default:

1

Range:

0x00 to 0x01

Events Generated

When this command has completed, an HCI_EXT_CoexEnableDone event shall be generated.

HCI Extension Events

The HCI Extension vendor specific commands generate the following vendor specific events.

HCI_EXT_SetRxGainDone

Opcode:

0x0400

Event Description:

This event is sent to indicate the RF receiver gain has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetTxPowerDone

Opcode:

0x0401

Event Description:

This event is sent to indicate the RF transmitter power has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_OnePacketPerEventDone

Opcode:

0x0402

Event Description:

This event is sent to indicate the One Packet Per Event feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_DecryptCommandDone

Opcode:

0x0405

Event Description:

This event is sent to indicate Decryption has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

Decrypted Data:

128 bit decrypted data block. The most significant octet of plainTextData corresponds to plainTextData using the notation specified in FIPS 197.

Size:

16 byte(s)

Range:

Any 16 byte value

HCI_EXT_WriteLocalFeatureSupportDone

Opcode:

0x0406

Event Description:

This event is sent to indicate the Set Local Supported Features command has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetFastTxResponseTimeDone

Opcode:

0x0407

Event Description:

This event is sent to indicate the Set Fast Transmit Response Time feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_ModemTestTxDone

Opcode:

0x0408

Event Description:

This event is sent to indicate the Modem Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_ModemHopTestTxDone

Opcode:

0x0409

Event Description:

This event is sent to indicate the Modem Hop Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_ModemTestRxDone

Opcode:

0x040A

Event Description:

This event is sent to indicate the Modem Test Receive test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnhancedModemTestTxDone

Opcode:

0x0427

Event Description:

This event is sent to indicate the enhanced Modem Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnhancedModemHopTestTxDone

Opcode:

0x0428

Event Description:

This event is sent to indicate the enhanced Modem Hop Test Transmit test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnhancedModemTestRxDone

Opcode:

0x0429

Event Description:

This event is sent to indicate the enhanced Modem Test Receive test has started, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EndModemTestDone

Opcode:

0x040B

Event Description:

This event is sent to indicate the modem test has been shutdown, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetBDADDRDone

Opcode:

0x040C

Event Description:

This event is sent to indicate the devices BLE address has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetVirtualAdvAddrDone

Opcode:

0x042D

Event Description:

This event is sent to indicate the advertise’s virtual address has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetSCADone

Opcode:

0x040D

Event Description:

This event is sent to indicate the devices SCA has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_EnablePTMDone

Opcode:

0x040E

Event Description:

There is not a corresponding event opcode (0x040E) and parameters for this command as it is only allowed as a direct function call by the application software.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetMaxDtmTxPowerDone

Opcode:

0x0411

Event Description:

This event is sent to indicate the maximum Direct Test Mode (DTM) RF transmitter power has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_DisconnectImmedDone

Opcode:

0x0413

Event Description:

This event is sent to indicate the Disconnect Immediate command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_PER

Opcode:

0x0414

Event Description:

This event is sent to indicate the Packet Error Rate Reset or Read command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

PER Command Type:

Read or Reset

Size:

1 byte(s)

Range:

Value

Description

0

Reset PER Counters

1

Read PER Counters

RX Pkts:

Number of received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX CRC Fails:

Number of received packets with CRC error.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Events:

Number of connection events.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Missed Events:

Number of missed connection events.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_OverrideSLDone

Opcode:

0x041A

Event Description:

This event is sent to indicate the Set Slave Latency Override feature has been enabled or disabled, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_BuildRevisionDone

Opcode:

0x041B

Event Description:

This event is sent to indicate the user revision number and the build revision of the stack, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

User Revision Number:

The user revision number set by the application software. If no value was ever set, than 0x0000.

Condition:

( cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Build Revision Number:

The build revision number of the BLE stack.

Condition:

( cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_ResetSystemDone

Opcode:

0x041D

Event Description:

This event is sent to indicate the Reset System command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_NumComplPktsLimitDone

Opcode:

0x041F

Event Description:

This event is sent to indicate the Number Completed Packets Limit command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_GetConnInfoDone

Opcode:

0x0420

Event Description:

This event is sent to indicate the Get Connection Information command has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

Alloc Conns:

Total number of allocated connections

Size:

1 byte(s)

Range:

Active Conns:

Number of currently active connections

Size:

1 byte(s)

Range:

An array of size “numConn” will be returned containing the parameters starting here:

Conn Handle:

Connection Handle

Size:

1 byte(s)

Range:

Conn Role:
Size:

1 byte(s)

Range:

Value

Description

0x22

LMP/LL Response Timeout

0x23

LMP Error Transaction Collision

0x24

LMP PDU Not Allowed

0x25

Encryption Mode Not Acceptable

0x26

Link Key Can Not be Changed

0x27

Requested QoS Not Supported

0x28

Instant Passed

0x29

Pairing With Unit Key Not Supported

0x2A

Different Transaction Collision

0x2B

Reserved

0x2C

QoS Unacceptable Parameter

0x2D

QoS Rejected

0x2E

Channel Assessment Not Supported

0x2F

Insufficient Security

0x30

Parameter Out Of Mandatory Range

0x31

Reserved

0x32

Role Switch Pending

0x33

Reserved

0x34

Reserved Slot Violation

0x35

Role Switch Failed

0x36

Extended Inquiry Response Too Large

0x37

Simple Pairing Not Supported By Host

0x38

Host Busy - Pairing

0x39

Connection Rejected Due To No Suitable Channel Found

0x3A

Controller Busy

0x3B

Unacceptable Connection Interval

0x3C

Directed Advertising Timeout

0x3D

Connection Terminated Due To MIC Failure

0x3E

Connection Failed To Be Established

0x3F

MAC Connection Failed

0x40

Coarse Clock Adjust Rejected

0x41

Type0 Submap Not Defined

0x42

Unknown Advertising Identifier

0x43

Limit Reached

0x44

Operation Cancelled by Host

0x45

Packet Too Long

Peer Addr:
Size:

6 byte(s)

Range:

Peer Addr Type:
Size:

1 byte(s)

Range:

Value

Description

0x00

Public

0x01

Random

0x02

Public Identity

0x03

Random Identity

The array of parameters ends here.

HCI_EXT_SetMaxDataLengthDone

Opcode:

0x0421

Event Description:

This event is sent to indicate the Set Max Data Length command has completed.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetDtmTxPktCntDone

Opcode:

0x0424

Event Description:

This event is sent to indicate the DTM TX Packet Count has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_LE_ADV_EVENT

Opcode:

0x0425

Event Description:

Extended advertisement event.

Event Parameters

eventID:
Size:

1 byte(s)

Range:

Value

Description

0x00

Adv Start After Enable

0x01

Adv End After Disable

0x02

Adv Start

0x03

Adv End

0x04

Adv Report

0x05

Adv Set Terminated

0x06

Scan req received

0x07

Scan Timeout

0x08

Scan Start

0x09

Scan End

0x0A

Scan Window End

0x0B

Scan Interval End

0x0C

Scan Duration End

0x0D

Scan Period End

0x0E

LL Out of memory

0x0F

Adv Data Truncated

handle:
Size:

1 byte(s)

Range:

Adv Data Len:
Condition:

( eventID==0x0f)

Size:

2 byte(s)

Range:

Available Adv Data Len:
Condition:

( eventID==0x0f)

Size:

1 byte(s)

Range:

HCI_EXT_LE_SCAN_EVENT

Opcode:

0x0426

Event Description:

Extended Scanner event.

Event Parameters

eventID:
Size:

1 byte(s)

Range:

Value

Description

0x00

Adv Start After Enable

0x01

Adv End After Disable

0x02

Adv Start

0x03

Adv End

0x04

Adv Report

0x05

Adv Set Terminated

0x06

Scan req received

0x07

Scan Timeout

0x08

Scan Start

0x09

Scan End

0x0A

Scan Window End

0x0B

Scan Interval End

0x0C

Scan Duration End

0x0D

Scan Period End

0x0E

LL Out of memory

0x0F

Adv Data Truncated

HCI_EXT_SetPinOutputDone

Opcode:

0x042A

Event Description:

This event is sent to indicate the Enable Pin Output has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetLocationingAccuracyDone

Opcode:

0x042B

Event Description:

This event is sent to indicate the locationing accuracy has been set, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_GetActiveConnInfoDone

Opcode:

0x042C

Event Description:

This event is sent to provide active connection information as requested.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

An array of size “cmConnInfo” will be returned containing the parameters starting here:

Access Addr:
Size:

4 byte(s)

Range:

Conn Interval (in 0.625ms units):
Size:

2 byte(s)

Range:

Hop Value:
Size:

1 byte(s)

Range:

mSCA:
Size:

2 byte(s)

Range:

next chan:
Size:

1 byte(s)

Range:

Chann Map:
Size:

5 byte(s)

Range:

CrcInit:
Size:

3 byte(s)

Range:

The array of parameters ends here.

HCI_EXT_CoexEnableDone

Opcode:

0x042E

Event Description:

This event is sent to indicate the Enable Coex feature, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetDefaultChannelMapDone

Opcode:

0x042F

Event Description:

This event is sent to indicate the Set Default Channel Map feature, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_SetConnectionChannelMapDone

Opcode:

0x0430

Event Description:

This event is sent to indicate the Set Connection Channel Map feature, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

HCI_EXT_GetRxStatisticsDone

Opcode:

0x0431

Event Description:

This event is sent to indicate the RX statistics Reset or Read command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

RX Statistics Command Type:

Read or Reset

Size:

1 byte(s)

Range:

Value

Description

0

Reset Statistics Counters

1

Read Statistics Counters

RX OK Pkts:

Number of ok received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX OK Control Pkts:

Number of ok received control packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX OK Control Pkts ACKed:

Number of ok received control packets that were ACKed.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX CRC Error Pkts:

Number of CRC error received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX Ignored Pkts:

Number of ignored received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX Empty Pkts:

Number of Empty received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

RX Discarded Pkts:

Number of discarded received packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_GetTxStatisticsDone

Opcode:

0x0432

Event Description:

This event is sent to indicate the TX statistics Reset or Read command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

TX Statistics Command Type:

Read or Reset

Size:

1 byte(s)

Range:

Value

Description

0

Reset Statistics Counters

1

Read Statistics Counters

TX OK Pkts:

Number of transmitted packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

TX OK Pkts ACKed:

Number of transmitted packets that were ACKed.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

TX Control Pkts:

Number of transmitted control packets.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

TX Control Pkts Acked:

Number of transmitted control packets that were ACKed.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

TX Control Pkts Acked that were ACKed:

Number of transmitted control packets ACKed that were ACKed.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

TX Retransmissions:

Number of packets retransmissions.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

TX Queue Finished Pkts:

Number of on Tx queue that are finished.

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_GetCoexStatisticsDone

Opcode:

0x0433

Event Description:

This event is sent to indicate the COEX statistics Reset or Read command has completed, or that there was an error.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

COEX Statistics Command Type:

Read or Reset

Size:

1 byte(s)

Range:

Value

Description

0

Reset Statistics Counters

1

Read Statistics Counters

Num of Grants:

Total number of grants (CC33xx: grants_asserted).

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

4 byte(s)

Range:

Any 4 byte value

Num of Rejects:

Total number of rejects (CC33xx: grants_asserted).

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

4 byte(s)

Range:

Any 4 byte value

Continuously rejects:

Total number of continuously rejected requests (CC33xx: grants_deasserted).

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

Max continuously rejects:

Max continuously rejected requests (CC33xx: request_assrted).

Condition:

( cmdVal!=0x00 && cmdStat==0x00)

Size:

2 byte(s)

Range:

Any 2 byte value

HCI_EXT_LLTestModeDone

Opcode:

0x0470

Event Description:

LL Test Mode event.

Event Parameters

Status:
Size:

1 byte(s)

Range:

See Status Table

Command Opcode:
Size:

2 byte(s)

Range:

See Command Table

CommandStatus

Opcode:

0x067F

Event Description:

The Command Status event is used to indicate that the command given by opCode parameter has been received and is being processed. If successful, an HCI vendor specific event that corresponds to the command will follow if applicable. Otherwise, no event will follow since the command was not started.

Event Parameters

Status:
Size:

1 byte(s)

Range:

Value

Description

0x00

SUCCESS

0x12

bleIncorrectMode

0x02

INVALIDPARAMETER

opCode:

opCode from the corresponding command

Size:

2 byte(s)

Range:

See Command Table

length:

Payload length

Condition:

(StatOpCode!=0x010C && StatOpCode!=0xFCF3 && StatOpCode!=0xFCF4 && StatOpCode!=0xFCF5 && StatOpCode!=0xFE84 && StatOpCode!=0xFE87 && StatOpCode!=0xFE3E && StatOpCode!=0xFE54 && StatOpCode!=0xFE56 && StatOpCode!=0xFE58 && StatOpCode!=0xFE61 && StatOpCode!=0x0682 && StatOpCode!=0xFE43 && StatOpCode!=0xFE37 && StatOpCode!=0xFE49)

Size:

1 byte(s)

payload:

See the corresponding command for payload parsing information if it exists.

Condition:

(StatOpCode!=0x010C && StatOpCode!=0xFCF3 && StatOpCode!=0xFCF4 && StatOpCode!=0xFCF5 && StatOpCode!=0xFE84 && StatOpCode!=0xFE87 && StatOpCode!=0xFE3E && StatOpCode!=0xFE54 && StatOpCode!=0xFE56 && StatOpCode!=0xFE58 && StatOpCode!=0xFE61 && StatOpCode!=0x0682 && StatOpCode!=0xFE43 && StatOpCode!=0xFE37 && StatOpCode!=0xFE49)

Size:

length byte(s)