Changelog
Table of Contents
New Features
BLE5-Stack
ID | Summary |
---|---|
BLE_AGAMA-4505 | [BASIC BLE] [Profiles] Included Glucose Profile support in Basic BLE Profiles on CC13X4 |
BLE_AGAMA-4129 | [BASIC BLE] [Profiles] Included Health Thermometer Profile support in Basic BLE Profiles on CC13X4 |
Proprietary RF
ID | Summary |
---|---|
PROPRF-1228 | Improvements targeting SysConfig migration |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-4381 | Migrate the 15.4 stack CC13x4/CC26x4 examples (collector and sensor) to TFMv1.8 |
TI154STACK-4347 | integrate the GenOpt features with 15.4 examples |
TI Wi-SUN FAN
ID | Summary |
---|---|
WISUN-933 | [SPS] optimize the FH Neighbor Table to improve network join time. |
WISUN-927 | Enable disconnection detection configuration in sysconfig |
WISUN-918 | Enable low latency multicast configuration |
WISUN-910 | Enable Wi-SUN Production Test Mode using wisundirect spinel command |
WISUN-904 | Enable selective border router joining via joiner EUI |
WISUN-902 | Enable preshared key security mode |
WISUN-899 | Enable rapid join sysconfig configuration |
WISUN-886 | Enable Make file for WiSUN examples |
TI Z-Stack
ID | Summary |
---|---|
ZIGBEE-2063 | Improvements targeting SysConfig migration |
DMM
ID | Summary |
---|---|
DMM-1383 | Improvements targeting SysConfig migration |
SimpleLink Common Components Module (SCCM)
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-6194 | Add I2S SysConfig support for “not in use” GPIO state and deprecate controllerTargetSelection |
TIDRIVERS-6178 | Add volatile key KeyStore support to ECJPAKE drivers |
TIDRIVERS-6134 | Include FreeRTOS kernel source files in Core SDK |
TIDRIVERS-6099 | Add MessageQueueP DPL module |
TIDRIVERS-6075 | Remove unused Power function prototypes |
TIDRIVERS-5998 | Update Power driver APIs to use uint32_t for resource IDs instead of uint_fast16_t |
TIDRIVERS-5993 | Port SimpleLink KeyStore to mbedTLS 3.4.0 |
TIDRIVERS-5964 | Migrate to TF-M v1.8 including Key Store |
TIDRIVERS-5935 | Add CANFD driver support for CC26x1 and CC26x2 |
TIDRIVERS-5913 | Add Power_getConstraintCount |
TIDRIVERS-5495 | Add LogSinkUART |
TIDRIVERS-5342 | Add ECJPAKE driver to TFM v1.8 |
FREERTOS-12 | Allow configuration of FreeRTOS source location |
FREERTOS-10 | Add support for custom tickrate in FreeRTOS Sysconfig Module |
FREERTOS-6 | FreeRTOS GCC standard library re-entrancy support causes task control block size of 340 bytes |
Radio Software Bundle (RFLib)
ID | Summary |
---|---|
RFDRIVER-782 | Change RF driver SWTCXO command termination from abort to graceful stop |
RFCORE-987 | cc13x4_cc26x4: Settings Release - 5/20 dBm: WB-DSSS - Release Candidate |
RFCORE-1009 | CC1312PSIP: PA Table Update - New High PA Entries |
RFCORE-981 | cc13x4_cc26x4: Settings Release - 10 dBm: IEEE 802.15.4 (ZigBee) - Functional Candidate |
RFCORE-980 | CC1314R, CC1354P/R: PA Table Update - Increased Sub-1GHz Granularity |
RFCORE-1016 | cc13x4_cc26x4: Settings Release - 20dBm: IEEE 802.15.4 (ZigBee) - Characterized |
RFCORE-993 | cc13x4: Settings Release - 5/20dBm: Sub1GHz WB-DSSS, 50Kbps - Characterized |
RFCORE-982 | CC2674R10: Settings Release - 5 dBm: ZigBee Frontend ID - Characterized |
RFCORE-979 | CC1311R: PA Table Update - New entries for 868/915 MHz PHYs |
Fixed Issues
BLE5-Stack
ID | Summary |
---|---|
BLE_AGAMA-4839 | Critical Section order not optimal in ICall_leaveCSImpl & ICall_enterCSImpl functions |
BLE_AGAMA-4785 | In rare occasions, DUT does not respond to LLCP Encryption Request |
BLE_AGAMA-4724 | Extended disconnect/reconnect test sometimes leads to exception in Multirole with one peripheral and two centrals |
BLE_AGAMA-4723 | Stack generates unexpected RPA |
BLE_AGAMA-4710 | [Multi-Connection] CC1354P10-1 Fails to save 16th bond as peripheral and 15th bond as central |
BLE_AGAMA-4585 | Connection handle and timestamp for GAP_CB_PHY_UPDATE may be incorrect when multiple connections are maintained |
BLE_AGAMA-4580 | Connection Event Report reports incorrect channel |
BLE_AGAMA-4573 | [CC2642] Peripheral fails to respond to CON_IND when using GAP_ADV_WL_POLICY_WL_ALL_REQ and connected to Central using RPA with Random ID |
BLE_AGAMA-4559 | Under certain conditions, incorrect channel is calculated for connection event as peripheral |
BLE_AGAMA-4480 | [Basic Example] Basic Broadcaster Doesn't Advertise |
BLE_AGAMA-4425 | BLE Stack does not dequeue ATT msg during fuzzing test |
BLE_AGAMA-4250 | The rtls_coordinator mixes up scanned extended advertisements' device address |
BLE_AGAMA-3838 | host_test may raise a UTIL_SystemErrorEvent with status INVALID_INTERRUPT_ID when UART data overflow |
BLE_AGAMA-3169 | Connecting twice to the same device causing wrong count of connections and a memory leakage |
Proprietary RF
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
TI154STACK-4391 | Support device migration from CC1314RSK to CC1314RGZ |
TI154STACK-4360 | FH broadcast interval cannot be set to more than 130 seconds |
TI154STACK-4341 | IEEE 2.4 GHz not protecting RfCbCntIndex in FreeRTOS and IEEE 2.4GHz not handling when both rxBufFull and rxDoneOK event are received at same event callback |
TI Wi-SUN FAN
ID | Summary |
---|---|
WISUN-939 | Wi-SUN channel mask in Brazil region does not follow the Spec |
TI Z-Stack
ID | Summary |
---|---|
None | None |
DMM
ID | Summary |
---|---|
None | None |
SimpleLink Common Components Module (SCCM)
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-6062 | Add a critical section for Linked-List manipulation to avoid conflicts |
TIDRIVERS-5969 | GPIO_resetConfig permanently clears IO callbacks set through SysConfig |
TIDRIVERS-5968 | The ChipSelect signal gets asserted after SPI_open( ) is called on CC13X4/CC26X4 devices |
LPRFXXWARE-904 | Fix CPUdelay() compilation issue when TICLANG Link-Time Optimization (LTO) is enabled |
Radio Software Bundle (RFLib)
ID | Summary |
---|---|
RFDRIVER-820 | SYSCFG: GPIO compatibility break on callback function configuration |
RFDRIVER-800 | Make sure RF_cancelCmd issued on an IEEE 802.15.4 foreground command does not also stop the underlying background command |
RFDRIVER-743 | cc13x2_cc26x2: SysConfig generates incorrect pOverrides_ble2Mbps when enabling BLE 2M PHY and Coexistence |
RFCORE-983 | cc13x4_cc26x4: Incorrect interrupt priorities cause IEEE CSMA command to stall indefinitely |
Known Issues
BLE5-Stack
ID | Summary |
---|---|
BLE_AGAMA-4855 | [Multi Connect] CC2651P3 Central fails to connect to more than 5 testers with privacy enable |
BLE_AGAMA-4846 | [Data Stream][Display] display_printf() is fail when try to print data larger then threshold of 300-500 bytes |
BLE_AGAMA-4837 | [IOP][Android 14][One Plus 11] With privacy enabled, reconnection fails after after Pairing & Bonding |
BLE_AGAMA-4830 | [SWAT] Scanner failes after receiving an incorrect event type |
BLE_AGAMA-4484 | multi_role FreeRTOS support removed from CC13XX / CC26XX |
BLE_AGAMA-4354 | Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager |
BLE_AGAMA-4324 | [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar |
BLE_AGAMA-4029 | Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set. |
BLE_AGAMA-4009 | [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands |
BLE_AGAMA-3896 | [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands |
BLE_AGAMA-3774 | Under certain conditions the CC2652R1 failed to synchronize to periodic advertising |
BLE_AGAMA-3752 | [CC2651] Host_test memory limitation using CCS+TI-CLANG |
BLE_AGAMA-3540 | [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC |
BLE_AGAMA-3486 | Device asserts upon connection when HeapMem and HeapTrack is used |
BLE_AGAMA-3427 | System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued |
BLE_AGAMA-3381 | Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration |
BLE_AGAMA-3107 | [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms |
BLE_AGAMA-3077 | [RTLS] CTE reception on the 2M PHY do not meet spec requirements |
BLE_AGAMA-3076 | [RTLS] CTEs sent on the 2M PHY do not meet spec requirements |
BLE_AGAMA-2266 | Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
Proprietary RF
ID | Summary |
---|---|
None | None |
TI 15.4-Stack
ID | Summary |
---|---|
None | None |
TI Wi-SUN FAN
ID | Summary |
---|---|
None | None |
TI Z-Stack
ID | Summary |
---|---|
None | None |
DMM
ID | Summary |
---|---|
None | None |
SimpleLink Common Components Module (SCCM)
ID | Summary |
---|---|
None | None |
TI-RTOS and Drivers
ID | Summary |
---|---|
TIDRIVERS-4844 | Implement restrictions in errata note IOC_01 in SysConfig |
TIDRIVERS-4127 | ADCBuf causes jitter when switching clock sources |
SYSBIOS-642 | Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field |
SYSBIOS-446 | Reported CPU load is not 100% when a task is in “while 1 {}” loop |
SYSBIOS-98 | Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432 |
FREERTOS-8 | Tasks view in ROV for FreeRTOS does not show if a task is blocked on a semaphore or mutex |
Radio Software Bundle (RFLib)
ID | Summary |
---|---|
None | None |