Z-Stack 3.1.0 to Z-Stack 3.2.0¶
This section will describe a way to migrate a project from Z-Stack 3.1.0 to a Z-Stack 3.2.0 project.
For this guide, samplelight from Z-Stack 3.1.0 will be ported over to Z-Stack 3.2.0. The two releases have minor differences mostly pertaining to bug fixes listed in the Z-Stack release notes, however one change to note is Z-Stack’s transition from a SDK Plugin to being a part of the SDK itself. The recommended approach is to start with a Z-Stack 3.1.0 project that contains the same base application as the porting target project and merge any custom functionality
Choose a Z-Stack 3.2.0 example project that contains your target project’s base functionality. For reference and use in this example, zc_light from simplelink_<device>_sdk_2_30_00_xx\examples\rtos\CC13xx or CC26xx_LAUNCHXL\zstack is chosen as a starting point.
No changes are required for the Z-Stack 3.2.0
zcl_samplelight_data.c
file unless clusters, attributes, or simple descriptors were added or altered in the Z-Stack 3.1.0 project. Note thatSAMPLELIGHT_ZCLVERSION
has been redefined asBASIC_ZCL_VERSION
.In
zcl_samplelight.h
, User Interface and Green Power events have been redefined:// UI Events #define SAMPLEAPP_UI_AUTO_REFRESH_EVT 0x0010 #define SAMPLEAPP_UI_INPUT_EVT 0x0040 #define SAMPLEAPP_PROCESS_UI_GPP_EVT 0x0080 // Green Power Events #define SAMPLEAPP_PROCESS_GP_DATA_SEND_EVT 0x0100 #define SAMPLEAPP_PROCESS_GP_EXPIRE_DUPLICATE_EVT 0x0200 #define SAMPLEAPP_PROCESS_GP_TEMP_MASTER_EVT 0x0400
macCryptoDriverTable
is used instread ofcryptoDriverTable
inmain.c
The following items specifically concern zcl_samplelight.c
:
Include
timer.h
has been renamedutil_timer.h
andstring.h
is added by defaultUser interface functions have changed due to deprecated LCD functionality:
zclSampleLight_UiUpdateLcd
is nowzclSampleLight_UiRefresh
UI_Init
and events inzclSampleLight_process_loop
have updated to reflect the new definitions fromzcl_samplelight.h
UI_UpdateLcd
is nowUI_Refresh
3. Green Power Sink support can be optionally added by defining
ENABLE_GREENPOWER_COMBO_BASIC
and including several additions to the application code:
Includes and definitions
#ifdef ENABLE_GREENPOWER_COMBO_BASIC #include "gp_sink.h" #define UI_STATE_GP_SINK_SET_COMMISSIONING 2 static uint8 zclSampleLight_SetSinkCommissioningMode = 0; static void zclSampleLight_setGPSinkCommissioningMode(uint16 keys); static void zclSampleLight_GPSink_Toggle(zclGpNotification_t *zclGpNotification); static void zclSampleLight_GPSink_On(zclGpNotification_t *zclGpNotification); static void zclSampleLight_GPSink_Off(zclGpNotification_t *zclGpNotification); static void zclSampleLight_GPSink_Identify(zclGpNotification_t *zclGpNotification); const uiState_t zclSampleLight_UiStatesMain[] = { /* UI_STATE_BACK_FROM_APP_MENU */ {UI_STATE_DEFAULT_MOVE, UI_STATE_GP_SINK_SET_COMMISSIONING, UI_KEY_SW_5_PRESSED, &UI_ActionBackFromAppMenu}, //do not change this line, except for the second item, which should point to the last entry in this menu /* UI_STATE_TOGGLE_LIGHT */ {UI_STATE_DEFAULT_MOVE, UI_STATE_DEFAULT_MOVE, UI_KEY_SW_5_PRESSED, &zclSampleLight_UiActionToggleLight}, /* UI_STATE_GP_SINK_SET_COMMISSIONING */ {UI_STATE_BACK_FROM_APP_MENU, UI_STATE_DEFAULT_MOVE, UI_KEY_SW_5_PRESSED, &zclSampleLight_setGPSinkCommissioningMode}, }; const char sGpSink[] = "GREEN POWER SINK"; const char sGpSinkCommissioning[] = " COMMISSIONING "; const char sGpSinkEnabled[] = "< ENABLED >"; const char sGpSinkDisabled[] = "< DISABLED >"; #else #define UI_STATE_TOGGLE_LIGHT 1 //UI_STATE_BACK_FROM_APP_MENU is item #0, so app item numbers should start from 1 const uiState_t zclSampleLight_UiStatesMain[] = { /* UI_STATE_BACK_FROM_APP_MENU */ {UI_STATE_DEFAULT_MOVE, UI_STATE_TOGGLE_LIGHT, UI_KEY_SW_5_PRESSED, &UI_ActionBackFromAppMenu}, //do not change this line, except for the second item, which should point to the last entry in this menu /* UI_STATE_TOGGLE_LIGHT */ {UI_STATE_BACK_FROM_APP_MENU, UI_STATE_DEFAULT_MOVE, UI_KEY_SW_5_PRESSED, &zclSampleLight_UiActionToggleLight}, }; #endifApplication Callbacks
#if defined (ENABLE_GREENPOWER_COMBO_BASIC) GpSink_AppCallbacks_t zclSampleLight_GpSink_AppCallbacks = { #ifdef ZCL_IDENTIFY zclSampleLight_GPSink_Identify, //IdentifyCmd; #endif #ifdef ZCL_SCENES NULL, //RecallSceneCmd; NULL, //StoreSceneCmd; #endif #ifdef ZCL_ON_OFF zclSampleLight_GPSink_Off, //OffCmd; zclSampleLight_GPSink_On, //OnCmd; zclSampleLight_GPSink_Toggle, //ToggleCmd; #endif #ifdef ZCL_LEVEL_CTRL NULL, //LevelControlStopCmd; NULL, //MoveUpCmd; NULL, //MoveDownCmd; NULL, //StepUpCmd; NULL, //StepDownCmd; NULL, //MoveUpWithOnOffCmd; NULL, //MoveDownWithOnOffCmd; NULL, //StepUpWithOnOffCmd; NULL, //StepDownWithOnOffCmd; #endif NULL, //MoveHueStopCmd; NULL, //MoveHueUpCmd; NULL, //MoveHueDownCmd; NULL, //StepHueUpCmd; NULL, //StepHueDownCmd; NULL, //MoveSaturationStopCmd; NULL, //MoveSaturationUpCmd; NULL, //MoveSaturationDownCmd; NULL, //StepSaturationUpCmd; NULL, //StepSaturationDownCmd; NULL, //MoveColorCmd; NULL, //StepColorCmd; #ifdef ZCL_DOORLOCK NULL, //LockDoorCmd; NULL, //UnlockDoorCmd; #endif NULL, //AttributeReportingCmd; NULL, //MfrSpecificReportingCmd; NULL, //MultiClusterReportingCmd; NULL, //MfrSpecificMultiReportingCmd; NULL, //RequestAttributesCmd; NULL, //ReadAttributeRspCmd; NULL, //zclTunnelingCmd; }; #endifEndpoint registration and initialization in
zclSampleLight_Init
#if defined (ENABLE_GREENPOWER_COMBO_BASIC) zclGp_RegisterCBForGPDCommand(&zclSampleLight_GpSink_AppCallbacks); gp_endpointInit(zclSampleLight_Entity); #endif
zstackmsg_CmdIDs_GP_COMMISSIONING_MODE_IND
case inzclSampleLight_processZStackMsgs
#ifdef BOARD_DISPLAY_USE_UART case zstackmsg_CmdIDs_GP_COMMISSIONING_MODE_IND: { zstackmsg_gpCommissioningModeInd_t *pInd; pInd = (zstackmsg_gpCommissioningModeInd_t*)pMsg; UI_SetGPPCommissioningMode( &(pInd->Req) ); } #endifUI Commissioning lines in
zclSampleLight_UiRefresh
void zclSampleLight_UiRefresh(uint8 UiState, char * line[3]) { #if defined (BOARD_DISPLAY_USE_UART) #if defined (ENABLE_GREENPOWER_COMBO_BASIC) if(UiState == UI_STATE_GP_SINK_SET_COMMISSIONING) { line[0] = (char *)sGpSink; line[1] = (char *)sGpSinkCommissioning; if(zclSampleLight_SetSinkCommissioningMode) { line[2] = (char*) sGpSinkEnabled; } else { line[2] = (char*) sGpSinkDisabled; } } else { #ifdef ZCL_LEVEL_CTRL zclHA_uint8toa( zclSampleLight_LevelCurrentLevel, &sLightLevel[9] ); line[0] = (char *)sLightLevel; #endif // ZCL_LEVEL_CTRL line[1] = (char *)(zclSampleLight_OnOff ? sLightOn : sLightOff); line[2] = "< TOGGLE LIGHT >"; } #else #ifdef ZCL_LEVEL_CTRL zclHA_uint8toa( zclSampleLight_LevelCurrentLevel, &sLightLevel[9] ); line[0] = (char *)sLightLevel; #endif // ZCL_LEVEL_CTRL line[1] = (char *)(zclSampleLight_OnOff ? sLightOn : sLightOff); line[2] = "< TOGGLE LIGHT >"; #endif #endif }Local functions
#if defined (ENABLE_GREENPOWER_COMBO_BASIC) static void zclSampleLight_setGPSinkCommissioningMode(uint16 keys) { zclSampleLight_SetSinkCommissioningMode ^= 1; gp_SetCommissioningMode(zclSampleLight_SetSinkCommissioningMode); } /********************************************************************* * @fn zclSampleLight_GPSink_Identify * * @brief Callback to process Identify command from a GPD * * @param zclGpNotification * * @return none */ static void zclSampleLight_GPSink_Identify(zclGpNotification_t *zclGpNotification) { afAddrType_t dstAddr; dstAddr.endPoint = SAMPLELIGHT_ENDPOINT; dstAddr.panId = 0; dstAddr.addrMode = afAddr16Bit; dstAddr.addr.shortAddr = _NIB.nwkDevAddress; //Identify is a payloadless command which triggers a 60 seconds identify in the device (doc 14-0563-16 GP spec Table 49) zclGeneral_SendIdentify(SAMPLELIGHT_ENDPOINT,&dstAddr,60,TRUE, 1); } /********************************************************************* * @fn zclSampleLight_GPSink_Off * * @brief Callback to process Off command from a GPD * * @param zclGpNotification * * @return none */ static void zclSampleLight_GPSink_Off(zclGpNotification_t *zclGpNotification) { zclSampleLight_OnOffCB(COMMAND_OFF); } /********************************************************************* * @fn zclSampleLight_GPSink_On * * @brief Callback to process On command from a GPD * * @param zclGpNotification * * @return none */ static void zclSampleLight_GPSink_On(zclGpNotification_t *zclGpNotification) { zclSampleLight_OnOffCB(COMMAND_ON); } /********************************************************************* * @fn zclSampleLight_GPSink_Toggle * * @brief Callback to process Toggle command from a GPD * * @param zclGpNotification * * @return none */ static void zclSampleLight_GPSink_Toggle(zclGpNotification_t *zclGpNotification) { zclSampleLight_OnOffCB(COMMAND_TOGGLE); } #endif
Code can optionally be added to
zclSampleLight_initialization
to clear the NV if the right push-button is pressed on startup:static void zclSampleLight_initialization(void) { uint8 key; /* Initialize user clocks */ zclSampleLight_initializeClocks(); /* Initialize keys */ key = Board_Key_initialize(zclSampleLight_changeKeyCallback); /* Initialize the LEDS */ Board_Led_initialize(); // Register the current thread as an ICall dispatcher application // so that the application can send and receive messages. ICall_registerApp(&zclSampleLight_Entity, &sem); if(key == KEY_RIGHT) { Zstackapi_bdbResetLocalActionReq(zclSampleLight_Entity); } //Initialize stack zclSampleLight_Init(); }
Add any other Z-Stack 3.1.0 application changes to the Z-Stack 3.2.0 file if not pertaining to the items listed above
Note
Difference comparison software is recommended for discerning all differences between software stacks.