Wireshark¶
Install the Required Software¶
Download and install the following software:
Wireshark software, version 2.6.x stable release
Warning
It is important that Wireshark 2.6.x version is used. Older or newer versions may not be compatible.
SmartRF Packet Sniffer 2, which contains sniffer firmware for the CC13xx and CC26xx family
Uniflash, used to program devices from the CC13xx and CC26xx family
Required Hardware¶
Any device from the CC13xx and CC26xx family which supports IEEE commands can be used as a sniffer. Following is a list of all supported development boards:
Hardware Setup¶
Connect the device to the computer with Wireshark installed.
If the device is not programmed with the sniffer firmware, use Uniflash to program the sniffer firmware.
The firmware image is called
sniffer_fw.hex.Depending on which device, the firmware image is found in
sniffer_fw/bin/{Device Family}/under the SmartRF Packet Sniffer 2 installation.For example, the firmware image for the CC26x2R LaunchPad is found under
sniffer_fw/bin/cc26x2r1lp/.
Running the Packet Sniffer¶
Connect the sniffer device.
Start the Sniffer Agent from SmartRF Packet Sniffer 2.
Figure 47. Open Sniffer Agent¶
Configure the sniffer device in the Sniffer Agent.
The sniffer device needs to be enabled, and the frequency band and channel must be configured. Select the
IEEE 802.15.4 - O-QPSK - 2405 MHz - Freq BandPHY, and select a channel number which matches the Thread Network channel. Click OK.
Figure 48. Configure device in Sniffer Agent¶
Start sniffer capture in the Sniffer Agent by clicking Start.
Open Wireshark with the modified target arguments.
This is detailed in the Software Setup Section in the SmartRF Packet Sniffer 2 User’s Guide. If done correctly, the Sniffer Agent is now connected to Wireshark.
Figure 51. Wireshark opened and connected to the Sniffer Agent.¶
Goto preferences in Wireshark with
Edit→Preferences.Goto the Thread Protocol dissector configuration by expanding Protocols on the right and navigating to Thread. Set the
Decode CoAP for Threadoption.
Figure 52. Edit Wireshark Thread Preferences¶
Goto the CoAP Protocol dissector configuration by navigating to CoAP. Make sure that the port matches as shown below.
Figure 53. Edit Wireshark CoAP Preferences¶
Goto the IEEE 802.15.4 Protocol dissector configuration by navigating to IEEE 802.15.4. Make sure that the configuration matches as shown below.
Figure 54. Edit Wireshark IEEE 802.15.4 Preferences¶
In the IEEE 802.15.4 Protocol dissector configuration, add a Thread Master key by selecting the
Edit...button next toDecryption Keysand clicking the+button. Set a key entry with the following values:Decryption Key
00112233445566778899aabbccddeeffDecryption Key Index
0Key hash
Thread hashNote
The Decryption Key is the default value for OpenThread. This should be set to a random value in production. You may have to determine the actual Thread Master Key for a given network. The Thread Test Harness does change these keys in the course of its tests.
Figure 55. Add IEEE 802.15.4 Decryption Key¶
The packets in Wireshark should now be decrypted and dissected correctly.
Figure 56. Dissected Thread traffic¶