OAD Storage & Security

There are a couple of aspects with OAD that one must take into account when choosing which type of OAD implementation that suits your application.

One aspect is where a new downloaded image is to be stored during the OAD process, for which you have two methods: on-chip and off-chip. On-chip OAD stores the downloaded image to internal flash, while off-chip OAD stores the downloaded image to external flash.

Another aspect is security, which is to whether or not authenticate a new downloaded image to be from a trusted source. There are two methods of security: Unsecure and Secure. Unsecure OAD does not apply new image security before executing it on the device. Secure OAD authenticates new images using an Elliptic Curve Digital Signature Algorithm (ECDSA) before it is installed and executed on-chip.

Note

Both OAD storage and OAD security can be configured independently.

OAD Storage

During an OAD procedure the candidate image is stored either in the internal flash, which is called on-chip OAD, or in external flash, which is called off-chip OAD. On-chip and off-chip OAD has associated trade-offs and benefits, which are summarized in Table 15.

Note

Due to flash constraints, on-chip OAD is only supported by some stacks. Refer to the stack-specific OAD chapter whether on-chip OAD is supported.

The biggest advantage of using on-chip OAD is allowing a single-chip OAD solution. However, on-chip OAD does put restrictions on application size in terms of flash usage.

Off-chip OAD does not have these restrictions, and can store multiple application images and a factory image in the external flash without limiting the application size on the internal flash. This, of course, comes at the cost of requiring an additional component.

Despite their differences, both on-chip and off-chip OAD are invariant to the transport of candidate images.

Table 15. OAD storage comparison

Storage

Advantages

Limitations

On-chip

  • No external flash required

  • Application size restriction

Off-chip

  • Ability to store multiple / backup images

  • App + Stack merged update supported

  • Maximum application size available to customer

  • Low power external flash required

OAD Security

When talking about security in the context of OAD, it is referred to whether or not new downloaded images must be authenticated as part of the OAD process. It does not refer to the security level of the actual transport mechanism of the OAD image. The main purpose for authenticating new downloaded images is to verify the image is from an entrusted source.

The only difference between secure OAD and unsecure OAD is that secure OAD will always authenticate new images as part of the OAD process when properly implemented along with the secure BIM. What it means for unsecure OAD to be unsecure, is that the problem of not verifying new OAD images could potentially allow untrusted sources to compromise the OAD Target.

Secure OAD uses Elliptic Curve Digital Signature Algorithm (ECDSA) to sign and verify secure OAD images. More specifically, the ECDSA-P256 algorithm is implemented. The underlying authentication mechanisms for ECDSA is that a suitable private and public key pair are generated, and that the private key used for image signing is thoroughly protected. Only the public key is stored on Target device.

Secure OAD affects multiple portions of the system including the following modules, the details of how secure OAD interacts with particular module can be found in its associated section.

Warning

It is imperative that the system developer protect the corresponding private key. Since any party that has access to the private key can generate signed images, these images will be treated as a valid authentic image and executed by the device. Likewise, if the private key is lost, the ability to generate new valid firmware images is lost.

Table 16. OAD security comparison

Security

Advantages

Limitations

Unsecure

  • Less complexity runtime

  • Requires less flash

  • Will naively accept, install and execute any downloaded images with valid CRC

Secure

  • Verifies OAD image authenticity before installing and enabling device execution of the new image

  • All downloaded images are required to be signed

  • Requires more flash for the for the OAD Image Header

  • Takes longer time (more energy) to perform the firmware upgrade