ECDSA.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
348 #ifndef ti_drivers_ECDSA__include
349 #define ti_drivers_ECDSA__include
350 
351 #include <stdbool.h>
352 #include <stddef.h>
353 #include <stdint.h>
354 
357 
358 #ifdef __cplusplus
359 extern "C" {
360 #endif
361 
374 #define ECDSA_STATUS_RESERVED (-32)
375 
382 #define ECDSA_STATUS_SUCCESS (0)
383 
390 #define ECDSA_STATUS_ERROR (-1)
391 
401 #define ECDSA_STATUS_RESOURCE_UNAVAILABLE (-2)
402 
409 #define ECDSA_STATUS_R_LARGER_THAN_ORDER (-3)
410 
417 #define ECDSA_STATUS_S_LARGER_THAN_ORDER (-4)
418 
425 #define ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVE (-5)
426 
434 #define ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME (-6)
435 
441 #define ECDSA_STATUS_POINT_AT_INFINITY (-7)
442 
446 #define ECDSA_STATUS_CANCELED (-8)
447 
456 #define ECDSA_STATUS_INVALID_KEY_SIZE (-10)
457 
469 typedef struct
470 {
472  void *object;
473 
475  void const *hwAttrs;
476 } ECDSA_Config;
477 
482 
505 typedef enum
506 {
522 
526 typedef struct
527 {
532  const uint8_t *hash;
536  uint8_t *r;
542  uint8_t *s;
548 
552 typedef struct
553 {
558  const uint8_t *hash;
562  const uint8_t *r;
568  const uint8_t *s;
575 
579 typedef union
580 {
584 
588 typedef enum
589 {
593 
613 typedef void (*ECDSA_CallbackFxn)(ECDSA_Handle handle,
614  int_fast16_t returnStatus,
615  ECDSA_Operation operation,
616  ECDSA_OperationType operationType);
617 
626 typedef struct
627 {
632  uint32_t timeout;
635  void *custom;
638 } ECDSA_Params;
639 
645 extern const ECDSA_Params ECDSA_defaultParams;
646 
655 void ECDSA_init(void);
656 
666 void ECDSA_close(ECDSA_Handle handle);
667 
685 ECDSA_Handle ECDSA_open(uint_least8_t index, const ECDSA_Params *params);
686 
700 
710 
720 
740 int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation);
741 
768 int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation);
769 
783 int_fast16_t ECDSA_cancelOperation(ECDSA_Handle handle);
784 
809 ECDSA_Handle ECDSA_construct(ECDSA_Config *config, const ECDSA_Params *params);
810 
811 #ifdef __cplusplus
812 }
813 #endif
814 
815 #endif /* ti_drivers_ECDSA__include */
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:505
ADC_Params params
Definition: Driver_Init.h:11
uint8_t * s
Definition: ECDSA.h:542
The CryptoKey type is an opaque representation of a cryptographic key.
const CryptoKey * myPrivateKey
Definition: ECDSA.h:529
Definition: ECDSA.h:591
const uint8_t * hash
Definition: ECDSA.h:532
void ECDSA_OperationSign_init(ECDSA_OperationSign *operation)
Function to initialize an ECDSA_OperationSign struct to its defaults.
void const * hwAttrs
Definition: ECDSA.h:475
const CryptoKey * theirPublicKey
Definition: ECDSA.h:555
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:613
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSA.h:628
const uint8_t * s
Definition: ECDSA.h:568
CryptoKey datastructure.
Definition: CryptoKey.h:192
ECDSA Global configuration.
Definition: ECDSA.h:469
void ECDSA_close(ECDSA_Handle handle)
Function to close an ECDSA peripheral specified by the ECDSA handle.
void ECDSA_init(void)
This function initializes the ECDSA module.
Struct containing the parameters required for signing a message.
Definition: ECDSA.h:526
const ECDSA_Params ECDSA_defaultParams
Default ECDSA_Params structure.
ECDSA Parameters.
Definition: ECDSA.h:626
const ECCParams_CurveParams * curve
Definition: ECDSA.h:528
ECDSA_OperationType
Enum for the operation types supported by the driver.
Definition: ECDSA.h:588
void ECDSA_Params_init(ECDSA_Params *params)
Function to initialize the ECDSA_Params struct to its defaults.
const uint8_t * r
Definition: ECDSA.h:562
Union containing pointers to all supported operation structs.
Definition: ECDSA.h:579
Definition: ECDSA.h:517
int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation)
Signs a hashed message.
void * custom
Definition: ECDSA.h:635
ECDSA_Config * ECDSA_Handle
A handle that is returned from an ECDSA_open() call.
Definition: ECDSA.h:481
uint8_t * r
Definition: ECDSA.h:536
int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation)
Verifies a received signature matches a hash and public key.
Struct containing the parameters required for verifying a message.
Definition: ECDSA.h:552
void * object
Definition: ECDSA.h:472
ECDSA_CallbackFxn callbackFxn
Definition: ECDSA.h:631
ECDSA_OperationVerify * verify
Definition: ECDSA.h:582
Definition: ECDSA.h:513
A structure containing the parameters of an elliptic curve.
Definition: ECCParams.h:139
Definition: ECDSA.h:507
const uint8_t * hash
Definition: ECDSA.h:558
ECDSA_Handle ECDSA_open(uint_least8_t index, const ECDSA_Params *params)
This function opens a given ECDSA peripheral.
Definition: ECDSA.h:590
const ECCParams_CurveParams * curve
Definition: ECDSA.h:554
ECDSA_OperationSign * sign
Definition: ECDSA.h:581
uint32_t timeout
Definition: ECDSA.h:632
ECDSA_Handle ECDSA_construct(ECDSA_Config *config, const ECDSA_Params *params)
Constructs a new ECDSA object.
void ECDSA_OperationVerify_init(ECDSA_OperationVerify *operation)
Function to initialize an ECDSA_OperationSign struct to its defaults.
int_fast16_t ECDSA_cancelOperation(ECDSA_Handle handle)
Cancels an ongoing ECDSA operation.
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale