CPU_FPU

Instance: CPU_FPU
Component: CPU_FPU
Base address: 0xE000EF30


Cortex-M's Floating Point Unit (FPU)

TOP:CPU_FPU Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

FPCCR

RW

32

0x0000 0000

0x0000 0004

0xE000 EF34

FPCAR

RW

32

0x0000 0000

0x0000 0008

0xE000 EF38

FPDSCR

RW

32

0x0000 0000

0x0000 000C

0xE000 EF3C

MVFR0

RW

32

0x0000 0000

0x0000 0010

0xE000 EF40

MVFR1

RW

32

0x0000 0000

0x0000 0014

0xE000 EF44

MVFR2

RW

32

0x0000 0000

0x0000 0018

0xE000 EF48

TOP:CPU_FPU Register Descriptions

TOP:CPU_FPU:FPCCR

Address Offset 0x0000 0004
Physical Address 0xE000 EF34 Instance 0xE000 EF34
Description Holds control data for the Floating-point extension
Type RW
Bits Field Name Description Type Reset
31 ASPEN When this bit is set to 1, execution of a floating-point instruction sets the CONTROL.FPCA bit to 1 RW 0
30 LSPEN Enables lazy context save of floating-point state RW 0
29 LSPENS This bit controls whether the LSPEN bit is writeable from the Non-secure state RW 0
28 CLRONRET Clear floating-point caller saved registers on exception return RW 0
27 CLRONRETS This bit controls whether the CLRONRET bit is writeable from the Non-secure state RW 0
26 TS Treat floating-point registers as Secure enable RW 0
25:11 RESERVED11 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000
10 UFRDY Indicates whether the software executing when the PE allocated the floating-point stack frame was able to set the UsageFault exception to pending RW 0
9 SPLIMVIOL This bit is banked between the Security states and indicates whether the floating-point context violates the stack pointer limit that was active when lazy state preservation was activated. SPLIMVIOL modifies the lazy floating-point state preservation behavior RW 0
8 MONRDY Indicates whether the software executing when the PE allocated the floating-point stack frame was able to set the DebugMonitor exception to pending RW 0
7 SFRDY Indicates whether the software executing when the PE allocated the floating-point stack frame was able to set the SecureFault exception to pending. This bit is only present in the Secure version of the register, and behaves as RAZ/WI when accessed from the Non-secure state RW 0
6 BFRDY Indicates whether the software executing when the PE allocated the floating-point stack frame was able to set the BusFault exception to pending RW 0
5 MMRDY Indicates whether the software executing when the PE allocated the floating-point stack frame was able to set the MemManage exception to pending RW 0
4 HFRDY Indicates whether the software executing when the PE allocated the floating-point stack frame was able to set the HardFault exception to pending RW 0
3 THREAD Indicates the PE mode when it allocated the floating-point stack frame RW 0
2 S Security status of the floating-point context. This bit is only present in the Secure version of the register, and behaves as RAZ/WI when accessed from the Non-secure state. This bit is updated whenever lazy state preservation is activated, or when a floating-point instruction is executed RW 0
1 USER Indicates the privilege level of the software executing when the PE allocated the floating-point stack frame RW 0
0 LSPACT Indicates whether lazy preservation of the floating-point state is active RW 0

TOP:CPU_FPU:FPCAR

Address Offset 0x0000 0008
Physical Address 0xE000 EF38 Instance 0xE000 EF38
Description Holds the location of the unpopulated floating-point register space allocated on an exception stack frame
Type RW
Bits Field Name Description Type Reset
31:3 ADDRESS The location of the unpopulated floating-point register space allocated on an exception stack frame RW 0b0 0000 0000 0000 0000 0000 0000 0000
2:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000

TOP:CPU_FPU:FPDSCR

Address Offset 0x0000 000C
Physical Address 0xE000 EF3C Instance 0xE000 EF3C
Description Holds the default values for the floating-point status control data that the PE assigns to the FPSCR when it creates a new floating-point context
Type RW
Bits Field Name Description Type Reset
31:27 RESERVED27 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000
26 AHP Default value for FPSCR.AHP RW 0
25 DN Default value for FPSCR.DN RW 0
24 FZ Default value for FPSCR.FZ RW 0
23:22 RMode Default value for FPSCR.RMode RW 0b00
21:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000

TOP:CPU_FPU:MVFR0

Address Offset 0x0000 0010
Physical Address 0xE000 EF40 Instance 0xE000 EF40
Description Describes the features provided by the Floating-point Extension
Type RW
Bits Field Name Description Type Reset
31:28 FPRound Indicates the rounding modes supported by the FP Extension RO 0x0
27:24 RESERVED24 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
23:20 FPSqrt Indicates the support for FP square root operations RO 0x0
19:16 FPDivide Indicates the support for FP divide operations RO 0x0
15:12 RESERVED12 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
11:8 FPDP Indicates support for FP double-precision operations RO 0x0
7:4 FPSP Indicates support for FP single-precision operations RO 0x0
3:0 SIMDReg Indicates size of FP register file RO 0x0

TOP:CPU_FPU:MVFR1

Address Offset 0x0000 0014
Physical Address 0xE000 EF44 Instance 0xE000 EF44
Description Describes the features provided by the Floating-point Extension
Type RW
Bits Field Name Description Type Reset
31:28 FMAC Indicates whether the FP Extension implements the fused multiply accumulate instructions RO 0x0
27:24 FPHP Indicates whether the FP Extension implements half-precision FP conversion instructions RO 0x0
23:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
7:4 FPDNaN Indicates whether the FP hardware implementation supports NaN propagation RO 0x0
3:0 FPFtZ Indicates whether subnormals are always flushed-to-zero RO 0x0

TOP:CPU_FPU:MVFR2

Address Offset 0x0000 0018
Physical Address 0xE000 EF48 Instance 0xE000 EF48
Description Describes the features provided by the Floating-point Extension
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:4 FPMisc Indicates support for miscellaneous FP features RO 0x0
3:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0