Instance: CPU_FPB
Component: CPU_FPB
Base address: 0xE0002000
Cortex-M's Flash Patch and Breakpoint (FPB)
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0xE000 2000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0xE000 2004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0xE000 2008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0xE000 200C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0xE000 2010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0xE000 2014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0xE000 2018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0xE000 201C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0xE000 2020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0xE000 2024 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FBC |
0xE000 2FBC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FCC |
0xE000 2FCC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FD0 |
0xE000 2FD0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FD4 |
0xE000 2FD4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FD8 |
0xE000 2FD8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FDC |
0xE000 2FDC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FE0 |
0xE000 2FE0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FE4 |
0xE000 2FE4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FE8 |
0xE000 2FE8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FEC |
0xE000 2FEC |
|
RW |
32 |
0x0000 0000 |
0x0000 0FF0 |
0xE000 2FF0 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FF4 |
0xE000 2FF4 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FF8 |
0xE000 2FF8 |
|
RW |
32 |
0x0000 0000 |
0x0000 0FFC |
0xE000 2FFC |
Address Offset | 0x0000 0000 | ||
Physical Address | 0xE000 2000 | Instance | 0xE000 2000 |
Description | Provides FPB implementation information, and the global enable for the FPB unit | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:28 | REV | Flash Patch and Breakpoint Unit architecture revision | RO | 0x0 | ||
27:15 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 | ||
14:12 | NUM_CODE_14_12_ | Indicates the number of implemented instruction address comparators. Zero indicates no Instruction Address comparators are implemented. The Instruction Address comparators are numbered from 0 to NUM_CODE - 1 | RO | 0b000 | ||
11:8 | NUM_LIT | Indicates the number of implemented literal address comparators. The Literal Address comparators are numbered from NUM_CODE to NUM_CODE + NUM_LIT - 1 | RO | 0x0 | ||
7:4 | NUM_CODE_7_4_ | Indicates the number of implemented instruction address comparators. Zero indicates no Instruction Address comparators are implemented. The Instruction Address comparators are numbered from 0 to NUM_CODE - 1 | RO | 0x0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||
1 | KEY | Writes to the FP_CTRL are ignored unless KEY is concurrently written to one | RW | 0 | ||
0 | ENABLE | Enables the FPB | RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0xE000 2004 | Instance | 0xE000 2004 |
Description | Indicates whether the implementation supports Flash Patch remap and, if it does, holds the target address for remap | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | RESERVED30 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||
29 | RMPSPT | Indicates whether the FPB unit supports the Flash Patch remap function | RO | 0 | ||
28:5 | REMAP | Holds the bits[28:5] of the Flash Patch remap address | RO | 0x00 0000 | ||
4:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0xE000 2008 | Instance | 0xE000 2008 |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 000C | ||
Physical Address | 0xE000 200C | Instance | 0xE000 200C |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0xE000 2010 | Instance | 0xE000 2010 |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0xE000 2014 | Instance | 0xE000 2014 |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0xE000 2018 | Instance | 0xE000 2018 |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 001C | ||
Physical Address | 0xE000 201C | Instance | 0xE000 201C |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0xE000 2020 | Instance | 0xE000 2020 |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0xE000 2024 | Instance | 0xE000 2024 |
Description | Holds an address for comparison. The effect of the match depends on the configuration of the FPB and whether the comparator is an instruction address comparator or a literal address comparator | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | BE | Selects between flashpatch and breakpoint functionality | RW | 0 |
Address Offset | 0x0000 0FBC | ||
Physical Address | 0xE000 2FBC | Instance | 0xE000 2FBC |
Description | Provides CoreSight discovery information for the FPB | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:21 | ARCHITECT | Defines the architect of the component. Bits [31:28] are the JEP106 continuation code (JEP106 bank ID, minus 1) and bits [27:21] are the JEP106 ID code. | RO | 0b000 0000 0000 | ||
20 | PRESENT | Defines that the DEVARCH register is present | RO | 0 | ||
19:16 | REVISION | Defines the architecture revision of the component | RO | 0x0 | ||
15:12 | ARCHVER | Defines the architecture version of the component | RO | 0x0 | ||
11:0 | ARCHPART | Defines the architecture of the component | RO | 0x000 |
Address Offset | 0x0000 0FCC | ||
Physical Address | 0xE000 2FCC | Instance | 0xE000 2FCC |
Description | Provides CoreSight discovery information for the FPB | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | SUB | Component sub-type | RO | 0x0 | ||
3:0 | MAJOR | Component major type | RO | 0x0 |
Address Offset | 0x0000 0FD0 | ||
Physical Address | 0xE000 2FD0 | Instance | 0xE000 2FD0 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | SIZE | See CoreSight Architecture Specification | RO | 0x0 | ||
3:0 | DES_2 | See CoreSight Architecture Specification | RO | 0x0 |
Address Offset | 0x0000 0FD4 | ||
Physical Address | 0xE000 2FD4 | Instance | 0xE000 2FD4 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 0000 |
Address Offset | 0x0000 0FD8 | ||
Physical Address | 0xE000 2FD8 | Instance | 0xE000 2FD8 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 0000 |
Address Offset | 0x0000 0FDC | ||
Physical Address | 0xE000 2FDC | Instance | 0xE000 2FDC |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 0000 |
Address Offset | 0x0000 0FE0 | ||
Physical Address | 0xE000 2FE0 | Instance | 0xE000 2FE0 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PART_0 | See CoreSight Architecture Specification | RO | 0x00 |
Address Offset | 0x0000 0FE4 | ||
Physical Address | 0xE000 2FE4 | Instance | 0xE000 2FE4 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | DES_0 | See CoreSight Architecture Specification | RO | 0x0 | ||
3:0 | PART_1 | See CoreSight Architecture Specification | RO | 0x0 |
Address Offset | 0x0000 0FE8 | ||
Physical Address | 0xE000 2FE8 | Instance | 0xE000 2FE8 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | REVISION | See CoreSight Architecture Specification | RO | 0x0 | ||
3 | JEDEC | See CoreSight Architecture Specification | RO | 0 | ||
2:0 | DES_1 | See CoreSight Architecture Specification | RO | 0b000 |
Address Offset | 0x0000 0FEC | ||
Physical Address | 0xE000 2FEC | Instance | 0xE000 2FEC |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | REVAND | See CoreSight Architecture Specification | RO | 0x0 | ||
3:0 | CMOD | See CoreSight Architecture Specification | RO | 0x0 |
Address Offset | 0x0000 0FF0 | ||
Physical Address | 0xE000 2FF0 | Instance | 0xE000 2FF0 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PRMBL_0 | See CoreSight Architecture Specification | RO | 0x00 |
Address Offset | 0x0000 0FF4 | ||
Physical Address | 0xE000 2FF4 | Instance | 0xE000 2FF4 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:4 | CLASS | See CoreSight Architecture Specification | RO | 0x0 | ||
3:0 | PRMBL_1 | See CoreSight Architecture Specification | RO | 0x0 |
Address Offset | 0x0000 0FF8 | ||
Physical Address | 0xE000 2FF8 | Instance | 0xE000 2FF8 |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PRMBL_2 | See CoreSight Architecture Specification | RO | 0x00 |
Address Offset | 0x0000 0FFC | ||
Physical Address | 0xE000 2FFC | Instance | 0xE000 2FFC |
Description | Provides CoreSight discovery information for the FP | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | PRMBL_3 | See CoreSight Architecture Specification | RO | 0x00 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |