TI BLE5-Stack 2.02.08.01 Release Notes

Table of Contents

Introduction

The BLE5-Stack is a set of sample applications, tools, APIs and protocol stack libraries that enable engineers to develop Bluetooth ® 5 standalone or network processor LE applications on the SimpleLink™ CC13xx and CC26xx family of wireless MCUs.

This Bluetooth 5 (BLE5-Stack) release includes qualification for Bluetooth 5.2 in addition to support for the existing core specifications (4.0, 4.1, 4.2) in addition to core specification 5.0 and 5.1 LE features such as: Direction Finding (AoA - Connected and Connectionless CTE), High Speed Mode (2 Mbps PHY), Long Range (LE Coded 125kbps and 500kbps PHYs), Advertisement Extensions (AE), Periodic Advertisements, Privacy 1.2.1 and Channel Selection Algorithm #2.

As with all Bluetooth core specifications that support the Low Energy (LE) feature, devices implementing the LE feature of Bluetooth 5 are backward compatible with Bluetooth 4.2, 4.1 and 4.0 LE capable devices.

BLE5-Stack 2.02.08.01 has been Bluetooth 5.2 qualified and is available for production use.

Key features of BLE5-Stack 2.02.08.01:

Additional information about TI’s Bluetooth Low Energy solutions can be found at www.ti.com/ble

BLE5-Stack Documentation

The SimpleLink Low Power F2 Software Development Kit (SDK) allows easier product development by combining TI-RTOS and the Bluetooth LE protocol stack in one unified SDK. Key documents needed for Bluetooth LE application development include:

Installation and Usage

What’s New

Mitigations for PSIRT-143, 144 and 145 have been first introduced in SDK version 7.10.00.98:

Please refer to https://www.ti.com/PSIRT for more details.

This point release contains no core modifications to the BLE5-Stack or application from the previous version. The following tickets were implemented to add support for new devices through SysConfig.

ID Summary
None None

Fixed Issues

ID Summary
None None

Known Issues and Limitations

ID Summary
BLE_AGAMA-4710 [Multi Connect] CC1354P10_1 Fails to Save 15\16 Bonds
BLE_AGAMA-4560 [CC13x4 / CC26x4] Connection timeouts observed during data streaming with PHY changes, and MTU modifications
BLE_AGAMA-4484 multi_role FreeRTOS support removed from CC13XX / CC26XX
BLE_AGAMA-4483 [MESH] eRPC support removed due to build failure
BLE_AGAMA-4480 [Basic Example] Basic Broadcaster Doesn't Advertise
BLE_AGAMA-4406 multi_sensor project has been removed from CC13XX / CC26XX
BLE_AGAMA-4354 Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager
BLE_AGAMA-4352 simple_mesh_node_and_peripheral_oad_onchip build failed error in TI Clang for CC26X2PSIP & CC13X2P2
BLE_AGAMA-4324 [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar
BLE_AGAMA-4029 Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set.
BLE_AGAMA-4009 [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands
BLE_AGAMA-3896 [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands
BLE_AGAMA-3774 Under certain conditions the CC2652R1 failed to synchronize to periodic advertising
BLE_AGAMA-3752 [CC2651] Host_test memory limitation using CCS+TI-CLANG
BLE_AGAMA-3747 [MESH][AE][eRPC] ~100% missing packets more than 3 hops while GATT Bearer is enabled
BLE_AGAMA-3606 [Mesh][Stability] Messages might stop after ~3 hours in a network with more than ~20 nodes
BLE_AGAMA-3597 [Mesh] LPN might fail to maintain friendship with ble.scanLatency < 10, when Display module is enabled
BLE_AGAMA-3556 [Mesh][IOP] LPN fails to configure after provisioning over PB-GATT with BlueZ
BLE_AGAMA-3543 [Build] Simple Mesh and Peripheral OAD onchip example fail to compile with GATT Bearer for CCS/TICLANG due to memory limitation
BLE_AGAMA-3540 [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC
BLE_AGAMA-3486 Device asserts upon connection when HeapMem and HeapTrack is used
BLE_AGAMA-3427 System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued
BLE_AGAMA-3391 [Mesh][eRPC] Limitation - Mesh node with eRPC unable to transmit messages > 221B
BLE_AGAMA-3388 [Mesh] Relay fails to transmit segmented message without re-transmission (relay re-transmit = 0)
BLE_AGAMA-3383 Mesh stack delay work API is limited to a maximum delay of uint32 maximum value (42,949,672 milliseconds)
BLE_AGAMA-3381 Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration
BLE_AGAMA-3169 Connecting twice to the same device causing wrong count of connections and a memory leakage
BLE_AGAMA-3107 [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms
BLE_AGAMA-3077 [RTLS] CTE reception on the 2M PHY do not meet spec requirements
BLE_AGAMA-3076 [RTLS] CTEs sent on the 2M PHY do not meet spec requirements
BLE_AGAMA-3024 [MESH] [IOP] Mesh DUT is not publishing its mesh supported roles (Unable to config Mesh node) with iPhone
BLE_AGAMA-2266 Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms
BLE_AGAMA-2033 [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release)
BLE_AGAMA-2010 [Multi-Sensor] Updating Report Interval Have no effect
BLE_AGAMA-1675 IOP: Device fails to pair with Meizu Pro 7
BLE_AGAMA-1435 [Multi-Sensor] Accelerometer Service Disappears After First Connection
BLE_AGAMA-139 When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection
BLE_AGAMA-80 The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases.

Upgrade and Compatibility Information

The BLE5-Stack 2.02.08.01 only supports SimpleLink CC13xx and CC26xx devices with silicon revision E. No support for previous silicon revisions or LaunchPad™ development kits using earlier silicon revisions. If you’re unsure of the revision number of your device, please see the Package Symbolization and Revision Identification section of the Errata Note.

As a supplier of Bluetooth® Low Energy (LE) solutions with a focus on interoperability and broad market adoption, we recommend to transition from proprietary Real Time Localization Toolbox (RTLS) software examples to the new RTLS software examples based on the Bluetooth 5.2 specification. These examples are included in this software development kit. For further information please contact your local TI sales representative.

Qualification

The Bluetooth Low Energy software stack (BLE5-Stack) for CC13xx_CC26xx Bluetooth LE-enabled wireless MCUs uses Bluetooth Qualified Components, which allow customers to substantially reduce the testing required to meet Bluetooth end product listing (EPL) qualification requirements while providing flexibility to the device configuration. Bluetooth SIG rules specify that Qualified Components have a validity period of three (3) years at which time they may not be available for new End Product Listings (EPLs). For information on the applicable QDID’s for this release, please refer to the application report SWRA601 - How to Qualify Your Bluetooth Low Energy Product.

As mentioned in the Known Issues and Limitations section, the Bluetooth low energy software stack (BLE5-Stack) for CC13xx_CC26xx CTE reception and transmission for AoA on the 2M PHY is not fully compliant with the Bluetooth specifications. As a consequence, AoA enabled projects cannot be qualified to operate on the 2M PHY.

Operating System Support

Please refer to the SDK release notes.

Dependencies

The BLE5-Stack sample applications were built & tested with the IDEs and listed in the top-level SDK release notes.

Note: Earlier IDE/toolchain versions are not supported and compatibility with newer versions of supported IDEs is not assured.

Device Support

This release supports development of single-mode Bluetooth LE applications on 2.4 GHz and multi-band wireless MCUs listed in the top-level SDK release

Development Board Support

This release supports development of single-mode Bluetooth LE on 2.4 GHz and multi-band wireless MCU development kits listed in the top-level SDK release notes

Validation

The BLE5-Stack sample applications were built & tested with the IDE’s and toolchains mentioned in the SDK release notes.

Versioning

This product follows a version format, M.mm.pp.bb, where:

Technical Support and Product Updates