Simple Central
Table of Contents
Introduction
The simple_central
project implements a simple Bluetooth low energy
central device with GATT client functionality. The simple_central
application can be configured to filter and connect to peripheral
devices with the TI Simple Profile UUID, such as devices with the
simple_peripheral
project. To enable this behavior, set
Discover devices by service UUID
to TRUE
in SysConfig
(under Observer Configuration
).
This project has the following app configurations available:
App Build Configuration | Description |
---|---|
FlashROM_Release (default) | All TI-RTOS debug features disabled but application-logging to UART remains enabled. The application uses the config file ble_release.cfg and the defines are in <app name>_FlashROM_Release.opt . |
FlashROM_Debug | All TI-RTOS debug features enabled. The application uses the config file ble_debug.cfg and the defines are in <app name>_FlashROM_Debug.opt . |
All application configurations use the stack library configuration, FlashROM_Library. This build configuration will yield additional flash footprint optimizations by the linker since the application and stack can share contiguous flash pages. This configuration is further discussed in the Stack Library Configuration section of the BLE5-Stack User's Guide provided in the SDK.
Hardware Prerequisites
The default Simple Central board configuration uses the device's LaunchPad development kit. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the BLE5-Stack User's Guide.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes file provided in the SDK. For information on how to import this project into your IDE workspace and build/run, please refer to the device's Platform section in the BLE5-Stack User's Guide.
Usage
This application uses the UART peripheral to provide an interface for the application. The UART is only used for display messages.
This document will use a terminal program (Tera Term, PuTTY, etc.) to serve as the display for the output of the LaunchPad. Note that any other serial terminal can be used. The following default parameters are used for the UART peripheral for display:
UART Param | Default Values |
---|---|
Baud Rate | 115200 |
Data length | 8 bits |
Parity | None |
Stop bits | 1 bit |
Flow Control | None |
Once the Simple Central sample application starts, the output to the terminal will report its address and that it is initialized and ready to begin discovery, as shown below. On the menu, you can use the left button (BTN-1) to move to the next option and the right button (BTN-2) to select an item:
The first option can be selected to set the Scanning PHY. For more information on PHY refer to the PHY section in the BLE5-Stack User's Guide.
The second option can be selected to begin discovering devices that are
broadcasting BLE advertisements. This will report the number of discovered devices.
Select Connect to
to view the list of devices and use the left button (BTN-1)
to go through the available devices:
When you have found the device that you are trying to connect to, press the right button to connect. This will display information such as the connection timeout and the address of the connected peripheral device.
The third option can be selected to select a group to which the central will
start connecting automatically to.
After selecting the group (Group A or Group B) the menu will go back to
main menu. Then the user will have to choose Discover Devices
to start scanning
and connecting to the group members. After all members are connected , the
Work with
menu can be chosen to use one of the members. If one of the members
got disconnected along the way , as long as the AutoConnect is not disabled,
new Discover Devices
can be initiated.
Basic assumptions that need to be taken into account:
- A peripheral node is associated with a group when it advertises a group name
as part of its adv data. The peripheral should advertise the group name as
its Shortened local name (opcode 0x07) and then
GA
for Group A orGB
for Group B. - The central won't start automatically connecting to the chosen group until
all defined group members are successfully scanned and found.
Number of group members are defined by
MAX_NUM_BLE_CONNS
. Hence the user have to pre-define the number of members that wanted to be connected to. - if the user defined
MAX_NUM_BLE_CONNS
to be bigger then 8 , then all update parameters requests will be rejected.
For further information regarding the limitation and settings of scheduling and memory, please see the BLE5-Stack User's Guide.
Once connected select Work with
and select the connected device.
It will now present you with 6 options. These options will be described in the following sections:
- GATT Read
- GATT Write
- Start RSSI Reading
- Connection Update
- Set Conn PHY Preference
- Disconnect
It is also possible to browse to and select "Upper Menu" to return to the main menu.
Option: GATT Read
This option is used to send read requests to the peripheral device.
Pressing the right button once will send a read request to the
peripheral device and will print the returned value of the characteristic.
Note that this characteristic can be written to with the GATT Write
option:
Option: GATT Write
This option is used to write predetermined values (0x00, 0x55, 0xAA, etc.) to the
device's characteristic. Note that this characteristic can be read from with the
GATT Read
option:
Option: Toggle Read RSSI
This option is used to get the RSSI (signal strength) of the connected peripheral device. Selecting this option will toggle RSSI reads on and off. When it is on, the RSSI value will be printed. The value will continue to be updated as the RSSI changes:
Option: Connection Update
This option updates the connection parameters based on the values set by
the following constants in simple_central.c
:
* DEFAULT_UPDATE_MIN_CONN_INTERVAL
* DEFAULT_UPDATE_MAX_CONN_INTERVAL
* DEFAULT_UPDATE_SLAVE_LATENCY
* DEFAULT_UPDATE_CONN_TIMEOUT
The update was successful if it states that it has been "Updated" and
displays the new connection timeout value.
Option: Set Conn PHY Preference
This option is used to select the PHY preference for the current connection.
If the PHY preference is changed to include a "faster" PHY than before,
simple_central
will attempt a PHY change.
You can choose from the following options:
- 1 Mbps
- 2 Mbps
- 1 & 2 Mbps
- Coded
- 1 & 2 Mbps, & Coded
For more information on PHY refer to the PHY section in the BLE5-Stack User's Guide. The following shows a successful update to Coded PHY:
Option: Disconnect
This option will send a link termination request to terminate the connection with the connected device. The following shows a successful disconnection:
Note that this application also supports MTU exchanges. This is done
automatically by the Simple Central device after a connection is formed with a
peripheral device. A larger MTU can be negotiated by changing MAX_PDU_SIZE
. More
information on this can be found in the
Configuring for Larger MTU Values section of the BLE5-Stack User's Guide.
Also note that the application will automatically request pairing once the connection is established.