SHA2CC26X4_s.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2022 Texas Instruments Incorporated - https://www.ti.com
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_drivers_sha2_SHA2CC26X4_s__include
34 #define ti_drivers_sha2_SHA2CC26X4_s__include
35 
36 #include <stdint.h>
37 
39 #include <ti/drivers/SHA2.h>
40 
42 
43 #include <third_party/tfm/interface/include/psa/error.h>
44 #include <third_party/tfm/interface/include/psa/service.h>
45 
46 #if defined(TFM_PSA_API)
47  #include "ti_drivers_config.h" /* Sysconfig generated header */
48 #endif
49 
50 #ifdef __cplusplus
51 extern "C" {
52 #endif
53 
54 /*
55  * SHA2 secure message types
56  *
57  * Non-secure clients must register their callback after opening or
58  * constructing a driver instance with blocking or callback return behavior.
59  */
60 #define SHA2_S_MSG_TYPE_CONSTRUCT (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 0U)))
61 #define SHA2_S_MSG_TYPE_OPEN (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 1U)))
62 #define SHA2_S_MSG_TYPE_REGISTER_CALLBACK \
63  (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 2U)))
64 #define SHA2_S_MSG_TYPE_CLOSE (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 3U)))
65 #define SHA2_S_MSG_TYPE_HASH_DATA (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 4U)))
66 #define SHA2_S_MSG_TYPE_HMAC (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 5U)))
67 #define SHA2_S_MSG_TYPE_SET_HASH_TYPE (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 6U)))
68 #define SHA2_S_MSG_TYPE_SETUP_HMAC (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 7U)))
69 #define SHA2_S_MSG_TYPE_ADD_DATA (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 8U)))
70 #define SHA2_S_MSG_TYPE_FINALIZE (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 9U)))
71 #define SHA2_S_MSG_TYPE_FINALIZE_HMAC (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 10U)))
72 #define SHA2_S_MSG_TYPE_CANCEL_OPERATION \
73  (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 11U)))
74 #define SHA2_S_MSG_TYPE_RESET (CRYPTO_S_MSG_TYPE_INDEX_SHA2 | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + 12U)))
75 
76 /*
77  * Config pool size determines how many dynamic driver instances can be created
78  * by the non-secure client using SHA2_construct().
79  */
80 #ifndef CONFIG_SHA2_S_CONFIG_POOL_SIZE
81  #define CONFIG_SHA2_S_CONFIG_POOL_SIZE 1
82 #endif
83 
84 #define SHA2_SECURE_CALLBACK_COUNT (CONFIG_TI_DRIVERS_SHA2_COUNT + CONFIG_SHA2_S_CONFIG_POOL_SIZE)
85 
86 /*
87  * ========= SHA2 Secure Callback struct =========
88  */
89 typedef struct
90 {
92  /* SHA2 callback fxn parameters */
94  int_fast16_t returnStatus;
96 
97 /*
98  * ========= SHA2 Secure Message Structs =========
99  * These secure message structs correspond to the secure message types defined
100  * above. Together, they are used by non-secure client to make PSA calls to the
101  * SHA2 secure service. There is a single input vector for the PSA call
102  * which is a pointer to secure message struct. If the underlying function
103  * has a return value, there is a single output vector which is a pointer to
104  * storage for the return value.
105  */
106 typedef struct
107 {
111 
112 typedef struct
113 {
114  uint_least8_t index;
117 
118 typedef struct
119 {
123 
124 typedef struct
125 {
128 
129 typedef struct
130 {
132  const void *data;
133  size_t dataLength;
134  void *digest;
136 
137 typedef struct
138 {
141  const void *data;
142  size_t dataLength;
143  void *hmac;
145 
146 typedef struct
147 {
151 
152 typedef struct
153 {
157 
158 typedef struct
159 {
161  const void *data;
162  size_t length;
164 
165 /* For SHA2_S_MSG_TYPE_FINALIZE or SHA2_S_MSG_TYPE_FINALIZE_HMAC */
166 typedef struct
167 {
171 
172 typedef struct
173 {
176 
177 typedef struct
178 {
181 
192 psa_status_t SHA2_s_handlePsaMsg(psa_msg_t *msg);
193 
199 void SHA2_s_init(void);
200 
201 #ifdef __cplusplus
202 }
203 #endif
204 
205 #endif /* ti_drivers_sha2_SHA2CC26X4_s__include */
const void * data
Definition: SHA2CC26X4_s.h:141
Definition: SHA2CC26X4_s.h:89
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:160
psa_status_t SHA2_s_handlePsaMsg(psa_msg_t *msg)
Handles PSA messages for SHA2 secure driver.
Definition: SecureCallback.h:51
SHA2_s_SecureCallback * callback
Definition: SHA2CC26X4_s.h:121
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:179
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:126
int_fast16_t returnStatus
Definition: SHA2CC26X4_s.h:94
Definition: SHA2CC26X4_s.h:152
void * digest
Definition: SHA2CC26X4_s.h:134
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:174
const SHA2_Params * params
Definition: SHA2CC26X4_s.h:109
SHA2 Global configuration.
Definition: SHA2.h:446
CryptoKey datastructure.
Definition: CryptoKey.h:192
SHA2_HashType type
Definition: SHA2CC26X4_s.h:149
const void * data
Definition: SHA2CC26X4_s.h:132
size_t dataLength
Definition: SHA2CC26X4_s.h:142
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:168
uint_least8_t index
Definition: SHA2CC26X4_s.h:114
Definition: SHA2CC26X4_s.h:158
Secure Crypto Service.
Definition: SHA2CC26X4_s.h:166
Definition: SHA2CC26X4_s.h:146
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:131
const SHA2_Params * params
Definition: SHA2CC26X4_s.h:115
void * hmac
Definition: SHA2CC26X4_s.h:143
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:139
Definition: SHA2CC26X4_s.h:177
Definition: SHA2CC26X4_s.h:118
Definition: SHA2CC26X4_s.h:112
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:93
size_t dataLength
Definition: SHA2CC26X4_s.h:133
Definition: SHA2CC26X4_s.h:172
SHA2_HashType
Enum for the hash types supported by the driver.
Definition: SHA2.h:395
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:120
CryptoKey * key
Definition: SHA2CC26X4_s.h:155
CryptoKey * key
Definition: SHA2CC26X4_s.h:140
Definition: SHA2CC26X4_s.h:129
Definition: SHA2CC26X4_s.h:124
void SHA2_s_init(void)
Initializes the SHA2 secure driver.
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:154
SHA2 driver header.
void * digestOrHmac
Definition: SHA2CC26X4_s.h:169
SecureCallback_Object object
Definition: SHA2CC26X4_s.h:91
Definition: SHA2CC26X4_s.h:106
const void * data
Definition: SHA2CC26X4_s.h:161
SHA2 Parameters.
Definition: SHA2.h:480
SHA2_Config * config
Definition: SHA2CC26X4_s.h:108
SHA2_Handle handle
Definition: SHA2CC26X4_s.h:148
size_t length
Definition: SHA2CC26X4_s.h:162
Definition: SHA2CC26X4_s.h:137
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale