ECDSACC26X1.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2020-2022, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
53 #ifndef ti_drivers_ecdsa_ECDSACC26X1__include
54 #define ti_drivers_ecdsa_ECDSACC26X1__include
55 
56 #include <stdint.h>
57 #include <stdbool.h>
58 
59 #include <ti/drivers/ECDSA.h>
60 #include <ti/drivers/TRNG.h>
62 
63 #include <ti/devices/DeviceFamily.h>
64 #include DeviceFamily_constructPath(driverlib/rom_ecc.h)
65 
66 #ifdef __cplusplus
67 extern "C" {
68 #endif
69 
76 typedef struct
77 {
91  uint8_t trngIntPriority;
93 
99 typedef struct
100 {
101  bool isOpen;
102  ECDSA_ReturnBehavior returnBehavior; /* Callback mode is not supported */
103  ECC_State eccState;
104  uint32_t eccWorkZone[288];
106 
107 #ifdef __cplusplus
108 }
109 #endif
110 
111 #endif /* ti_drivers_ecdsa_ECDSACC26X1__include */
TI Driver for Elliptic Curve Digital Signature Algorithm.
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:505
ECDSACC26X1 Object.
Definition: ECDSACC26X1.h:99
uint8_t trngIntPriority
TRNG Peripheral&#39;s interrupt priority.
Definition: ECDSACC26X1.h:91
TRNG driver implementation for the CC26XX family.
bool isOpen
Definition: ECDSACC26X1.h:101
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSACC26X1.h:102
ECDSACC26X1 Hardware Attributes.
Definition: ECDSACC26X1.h:76
TRNG driver header.
ECC_State eccState
Definition: ECDSACC26X1.h:103
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale