ECDHCC26X4_s.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2022 Texas Instruments Incorporated - https://www.ti.com
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef ti_drivers_ecdh_ECDHCC26X4_s__include
34 #define ti_drivers_ecdh_ECDHCC26X4_s__include
35 
36 #include <stdint.h>
37 
39 #include <ti/drivers/ECDH.h>
40 
42 
43 #include <third_party/tfm/interface/include/psa/error.h>
44 #include <third_party/tfm/interface/include/psa/service.h>
45 
46 #if defined(TFM_PSA_API)
47  #include "ti_drivers_config.h" /* Sysconfig generated header */
48 #endif
49 
50 #ifdef __cplusplus
51 extern "C" {
52 #endif
53 
54 #define ECDH_S_MSG_TYPE(index) (CRYPTO_S_MSG_TYPE_INDEX_ECDH | ((int32_t)1 << (CRYPTO_S_MSG_TYPE_SHIFT + (index))))
55 
56 /*
57  * ECDH secure message types
58  */
59 #define ECDH_S_MSG_TYPE_CONSTRUCT ECDH_S_MSG_TYPE(0U)
60 #define ECDH_S_MSG_TYPE_OPEN ECDH_S_MSG_TYPE(1U)
61 #define ECDH_S_MSG_TYPE_REGISTER_CALLBACK ECDH_S_MSG_TYPE(2U)
62 #define ECDH_S_MSG_TYPE_CLOSE ECDH_S_MSG_TYPE(3U)
63 #define ECDH_S_MSG_TYPE_GENERATE_PUBLIC_KEY ECDH_S_MSG_TYPE(4U)
64 #define ECDH_S_MSG_TYPE_COMPUTE_SHARED_SECRET ECDH_S_MSG_TYPE(5U)
65 #define ECDH_S_MSG_TYPE_CANCEL_OPERATION ECDH_S_MSG_TYPE(6U)
66 
67 /*
68  * Config pool size determines how many dynamic driver instances can be created
69  * by the non-secure client using ECDH_construct().
70  */
71 #ifndef CONFIG_ECDH_S_CONFIG_POOL_SIZE
72  #define CONFIG_ECDH_S_CONFIG_POOL_SIZE 1
73 #endif
74 
75 #define ECDH_SECURE_CALLBACK_COUNT (CONFIG_TI_DRIVERS_ECDH_COUNT + CONFIG_ECDH_S_CONFIG_POOL_SIZE)
76 
77 /*
78  * ========= ECDH Secure Callback struct =========
79  * Non-secure clients must register their callback after opening or
80  * constructing a driver instance with blocking or callback return behavior.
81  */
82 typedef struct
83 {
85  /* ECDH callback fxn parameters */
87  int_fast16_t returnStatus;
91 
92 /*
93  * ========= ECDH Secure Message Structs =========
94  * These secure message structs correspond to the secure message types defined
95  * above. Together, they are used by non-secure client to make PSA calls to the
96  * ECDH secure service. There is a single input vector for the PSA call
97  * which is a pointer to secure message struct. If the underlying function
98  * has a return value, there is a single output vector which is a pointer to
99  * storage for the return value.
100  */
101 typedef struct
102 {
106 
107 typedef struct
108 {
109  uint_least8_t index;
112 
113 typedef struct
114 {
118 
119 typedef struct
120 {
123 
124 typedef struct
125 {
129 
130 typedef struct
131 {
135 
136 typedef struct
137 {
140 
151 psa_status_t ECDH_s_handlePsaMsg(psa_msg_t *msg);
152 
158 void ECDH_s_init(void);
159 
160 #ifdef __cplusplus
161 }
162 #endif
163 
164 #endif /* ti_drivers_ecdh_ECDHCC26X4_s__include */
ECDH_OperationType
Enum for the operation types supported by the driver.
Definition: ECDH.h:643
ECC Global configuration.
Definition: ECDH.h:518
ECDH_Handle handle
Definition: ECDHCC26X4_s.h:126
Definition: SecureCallback.h:51
ECDH_Handle handle
Definition: ECDHCC26X4_s.h:132
ECDH_Handle handle
Definition: ECDHCC26X4_s.h:138
uint_least8_t index
Definition: ECDHCC26X4_s.h:109
int_fast16_t returnStatus
Definition: ECDHCC26X4_s.h:87
Definition: ECDHCC26X4_s.h:101
Struct containing the parameters required to compute the shared secret.
Definition: ECDH.h:608
ECDH_Handle handle
Definition: ECDHCC26X4_s.h:121
ECDH_OperationType operationType
Definition: ECDHCC26X4_s.h:89
Definition: ECDHCC26X4_s.h:82
Secure Crypto Service.
const ECDH_Params * params
Definition: ECDHCC26X4_s.h:110
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
Definition: ECDHCC26X4_s.h:107
ECC Parameters.
Definition: ECDH.h:680
ECDH_s_SecureCallback * callback
Definition: ECDHCC26X4_s.h:116
ECDH_Handle handle
Definition: ECDHCC26X4_s.h:115
void ECDH_s_init(void)
Initializes the ECDH secure driver.
Definition: ECDHCC26X4_s.h:119
Definition: ECDHCC26X4_s.h:136
SecureCallback_Object object
Definition: ECDHCC26X4_s.h:84
const ECDH_Params * params
Definition: ECDHCC26X4_s.h:104
ECDH_OperationGeneratePublicKey * operation
Definition: ECDHCC26X4_s.h:127
Struct containing the parameters required to generate a public key.
Definition: ECDH.h:589
psa_status_t ECDH_s_handlePsaMsg(psa_msg_t *msg)
Handles PSA messages for ECDH secure driver.
Definition: ECDHCC26X4_s.h:130
Definition: ECDHCC26X4_s.h:124
ECDH_Config * config
Definition: ECDHCC26X4_s.h:103
ECDH_Operation operation
Definition: ECDHCC26X4_s.h:88
ECDH_OperationComputeSharedSecret * operation
Definition: ECDHCC26X4_s.h:133
Union containing pointers to all supported operation structs.
Definition: ECDH.h:633
Definition: ECDHCC26X4_s.h:113
ECDH_Handle handle
Definition: ECDHCC26X4_s.h:86
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale