ECDHCC26X2.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2022, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
104 #ifndef ti_drivers_ecdh_ECDHCC26X2__include
105 #define ti_drivers_ecdh_ECDHCC26X2__include
106 
107 #include <stdint.h>
108 #include <stdbool.h>
109 
110 #include <ti/drivers/Power.h>
111 #include <ti/drivers/ECDH.h>
114 
115 #include <ti/devices/DeviceFamily.h>
116 #include DeviceFamily_constructPath(driverlib/pka.h)
117 
118 #if (ENABLE_KEY_STORAGE == 1)
120 #endif
121 
122 #include <ti/drivers/dpl/HwiP.h>
123 #include <ti/drivers/dpl/SwiP.h>
124 #include <ti/drivers/dpl/SemaphoreP.h>
125 
126 #ifdef __cplusplus
127 extern "C" {
128 #endif
129 
130 /* Exit the SWI and wait until an HWI call posts the SWI again */
131 #define ECDHCC26X2_STATUS_FSM_RUN_PKA_OP ECDH_STATUS_RESERVED - 0
132 /* Execute the next FSM state immediately without waiting for the next HWI */
133 #define ECDHCC26X2_STATUS_FSM_RUN_FSM ECDH_STATUS_RESERVED - 1
134 
144 typedef enum
145 {
147 
151 
155 
159 
164 
171 typedef struct
172 {
186  uint8_t intPriority;
188 
194 typedef struct
195 {
196  bool isOpen;
199  int_fast16_t operationStatus;
204  ECDHCC26X2_FsmState fsmState;
206  uint32_t resultAddress;
208 
209 #ifdef __cplusplus
210 }
211 #endif
212 
213 #endif /* ti_drivers_ecdh_ECDHCC26X2__include */
ECDHCC26X2_FsmState
ECDHCC26X2 states.
Definition: ECDHCC26X2.h:144
ECDH_OperationType
Enum for the operation types supported by the driver.
Definition: ECDH.h:643
bool isOpen
Definition: ECDHCC26X2.h:196
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: ECDHCC26X2.h:186
The CryptoKey type is an opaque representation of a cryptographic key.
uint32_t semaphoreTimeout
Definition: ECDHCC26X2.h:205
ECDHCC26X2 Object.
Definition: ECDHCC26X2.h:194
Power Manager.
CryptoKeyKeyStore_PSA driver header.
int_fast16_t operationStatus
Definition: ECDHCC26X2.h:199
Definition: ECDHCC26X2.h:146
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:667
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
ECDH_OperationType operationType
Definition: ECDHCC26X2.h:203
bool operationInProgress
Definition: ECDHCC26X2.h:197
uint32_t resultAddress
Definition: ECDHCC26X2.h:206
bool operationCanceled
Definition: ECDHCC26X2.h:198
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X2.h:201
ECDH_Operation operation
Definition: ECDHCC26X2.h:202
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X2.h:200
ECDH_ReturnBehavior
The way in which ECDH function calls return after performing a public key generation or shared secret...
Definition: ECDH.h:558
ECDHCC26X2_FsmState fsmState
Definition: ECDHCC26X2.h:204
ECDHCC26X2 Hardware Attributes.
Definition: ECDHCC26X2.h:171
Definition: ECDHCC26X2.h:150
Union containing pointers to all supported operation structs.
Definition: ECDH.h:633
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale