AESCTRCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2018-2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
69 #ifndef ti_drivers_aesctr_AESCTRCC26XX__include
70 #define ti_drivers_aesctr_AESCTRCC26XX__include
71 
72 #include <stdint.h>
73 #include <stdbool.h>
74 
75 #include <ti/drivers/AESCTR.h>
76 
77 #include <ti/devices/DeviceFamily.h>
78 #include DeviceFamily_constructPath(driverlib/aes.h)
79 
80 #ifdef __cplusplus
81 extern "C" {
82 #endif
83 
90 typedef struct
91 {
105  uint8_t intPriority;
107 
113 typedef struct
114 {
115  uint32_t counter[AES_BLOCK_SIZE / 4];
119  const uint8_t *input;
120  uint8_t *output;
121  size_t inputLength;
123  volatile int_fast16_t returnStatus;
126  bool isOpen;
128  volatile bool cryptoResourceLocked;
129  volatile bool hwBusy;
130  volatile bool operationInProgress;
132 
138 bool AESCTR_acquireLock(AESCTR_Handle handle, uint32_t timeout);
139 void AESCTR_releaseLock(AESCTR_Handle handle);
140 void AESCTR_enableThreadSafety(AESCTR_Handle handle);
141 void AESCTR_disableThreadSafety(AESCTR_Handle handle);
144 #ifdef __cplusplus
145 }
146 #endif
147 
148 #endif /* ti_drivers_aesctr_AESCTRCC26XX__include */
volatile int_fast16_t returnStatus
Definition: AESCTRCC26XX.h:123
void(* AESCTR_CallbackFxn)(AESCTR_Handle handle, int_fast16_t returnValue, AESCTR_OperationUnion *operation, AESCTR_OperationType operationType)
The definition of a callback function used by the AESCTR driver when used in AESCTR_RETURN_BEHAVIOR_C...
Definition: AESCTR.h:666
size_t inputLength
Definition: AESCTRCC26XX.h:121
AES Global configuration.
Definition: AESCommon.h:154
const uint8_t * input
Definition: AESCTRCC26XX.h:119
AESCTR_OperationType
Enum for the operation types supported by the driver.
Definition: AESCTR.h:623
CryptoKey datastructure.
Definition: CryptoKey.h:192
AESCTR_ReturnBehavior
The way in which CTR function calls return after performing an encryption or decryption operation...
Definition: AESCTR.h:482
volatile bool cryptoResourceLocked
Definition: AESCTRCC26XX.h:128
volatile bool hwBusy
Definition: AESCTRCC26XX.h:129
uint32_t semaphoreTimeout
Definition: AESCTRCC26XX.h:116
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESCTRCC26XX.h:105
bool isOpen
Definition: AESCTRCC26XX.h:126
CryptoKey key
Definition: AESCTRCC26XX.h:122
AESCTRCC26XX Object.
Definition: AESCTRCC26XX.h:113
uint8_t * output
Definition: AESCTRCC26XX.h:120
AESCTR_ReturnBehavior returnBehavior
Definition: AESCTRCC26XX.h:124
AESCTRCC26XX Hardware Attributes.
Definition: AESCTRCC26XX.h:90
AESCTR_OperationUnion * operation
Definition: AESCTRCC26XX.h:118
Union containing a reference to a one-step and segmented operation structure.
Definition: AESCTR.h:585
AESCTR_CallbackFxn callbackFxn
Definition: AESCTRCC26XX.h:117
AESCTR_OperationType operationType
Definition: AESCTRCC26XX.h:125
volatile bool operationInProgress
Definition: AESCTRCC26XX.h:130
bool threadSafe
Definition: AESCTRCC26XX.h:127
AESCTR driver header.
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale