AESCBCCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2018-2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
70 #ifndef ti_drivers_aescbc_AESCBCCC26XX__include
71 #define ti_drivers_aescbc_AESCBCCC26XX__include
72 
73 #include <stdint.h>
74 #include <stdbool.h>
75 
76 #include <ti/drivers/AESCBC.h>
77 
78 #include <ti/drivers/dpl/SwiP.h>
79 
80 #include <ti/devices/DeviceFamily.h>
81 #include DeviceFamily_constructPath(driverlib/aes.h)
82 
83 #ifdef __cplusplus
84 extern "C" {
85 #endif
86 
93 typedef struct
94 {
108  uint8_t intPriority;
110 
116 typedef struct
117 {
118  uint32_t iv[AES_BLOCK_SIZE / 4];
123  volatile int_fast16_t returnStatus;
126  bool isOpen;
127  volatile bool operationInProgress;
129  volatile bool hwBusy;
130  volatile bool cryptoResourceLocked;
132 
140 bool AESCBC_acquireLock(AESCBC_Handle handle, uint32_t timeout);
141 void AESCBC_releaseLock(AESCBC_Handle handle);
142 void AESCBC_enableThreadSafety(AESCBC_Handle handle);
143 void AESCBC_disableThreadSafety(AESCBC_Handle handle);
146 #ifdef __cplusplus
147 }
148 #endif
149 
150 #endif /* ti_drivers_aescbc_AESCBCCC26XX__include */
AESCBC driver header.
AESCBC_OperationType operationType
Definition: AESCBCCC26XX.h:125
AES Global configuration.
Definition: AESCommon.h:154
bool threadSafe
Definition: AESCBCCC26XX.h:128
CryptoKey datastructure.
Definition: CryptoKey.h:192
AESCBC_ReturnBehavior
The way in which CBC function calls return after performing an encryption or decryption operation...
Definition: AESCBC.h:696
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESCBCCC26XX.h:108
AESCBCCC26XX Object.
Definition: AESCBCCC26XX.h:116
AESCBCCC26XX Hardware Attributes.
Definition: AESCBCCC26XX.h:93
volatile bool cryptoResourceLocked
Definition: AESCBCCC26XX.h:130
bool isOpen
Definition: AESCBCCC26XX.h:126
uint32_t semaphoreTimeout
Definition: AESCBCCC26XX.h:119
AESCBC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCBC.h:815
AESCBC_OperationUnion * operation
Definition: AESCBCCC26XX.h:121
Union containing a reference to a one step or segmented operation.
Definition: AESCBC.h:806
volatile bool hwBusy
Definition: AESCBCCC26XX.h:129
AESCBC_ReturnBehavior returnBehavior
Definition: AESCBCCC26XX.h:124
volatile bool operationInProgress
Definition: AESCBCCC26XX.h:127
volatile int_fast16_t returnStatus
Definition: AESCBCCC26XX.h:123
void(* AESCBC_CallbackFxn)(AESCBC_Handle handle, int_fast16_t returnValue, AESCBC_OperationUnion *operation, AESCBC_OperationType operationType)
The definition of a callback function used by the AESCBC driver when used in AESCBC_RETURN_BEHAVIOR_C...
Definition: AESCBC.h:843
CryptoKey key
Definition: AESCBCCC26XX.h:122
AESCBC_CallbackFxn callbackFxn
Definition: AESCBCCC26XX.h:120
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale