TI BLE5-Stack Quick Start

This section serves as a road map for users developing applications and products using the TI SimpleLink CC13xx or CC26xx wireless MCU platform for Bluetooth Low Energy applications. Whether a seasoned developer or just getting started, TI has created a variety of resources to simplify development on the CC13xx or CC26xx platform. These resources will enhance your experience with the TI SimpleLink TI BLE5-Stack 7.10.00.xx from the out-of-the-box demo to production.

To download the CC13xx or CC26xx SDK, please visit the download page: https://www.ti.com/tool/SIMPLELINK-CC13XX-CC26XX-SDK.

Figure 47. shows the suggested work flow for getting started with TI’s SimpleLink Bluetooth Low Energy (BLE) development environment.

../_images/ble5suggestedworkflow.png

Figure 47. Suggested Workflow

Note

The BLE5-Stack component of the SDK now supports secure OAD and use it by default. In order to maintain compatibility with other stacks, the Quick Start Guide will cover unsecure OAD. For more information regarding secure OAD, see the OAD Chapter of the BLE5-Stack User’s Guide.

Using BLE5-Stack Projects with CCS

For BLE5-Stack projects, the BLE5-Stack is linked as library files. The host_test project is an exception to this, and use the split Stack library configuration. This means that importing the BLE5-Stack project into CCS will also import a BLE5-Stack library project. The stack library project is a dependent project and will be automatically built when the example project is built.

Projects that contain the TI Over-the-Air Download (OAD) Profile will require you to flash your device with the Boot Image Manager (BIM) hex file. This is the first step described in section Build and Download below. For more information on the TI OAD Profile and the BIM see the OAD Chapter of the BLE5-Stack User’s Guide.

For more details and how to change configurations look at the SimpleLink TI BLE5-Stack User’s Guide.

Import Project Using Resource Explorer

A quick and easy way to start working with the SDK is to use the TI Resource Explorer in CCS.

This section describes how to import and build an existing project and references the project_zero project. All of TI BLE5-Stack projects included in the development kit have a similar structure.

  1. Open the CCS IDE from the Start Menu.

  2. Create a workspace.

    Attention

    Ensure that the CCS workspace path does not contain a whitespace.

  3. Import a CCS Project using Resource Explorer

    • Open Resource Explorer (if not open already): View -> Resource Explorer

    • Navigate to the CCS folder for your chosen example: Software → SimpleLink CC13xx/CC26xx SDK → Examples → Development Tools → CC13xx or CC26xx LaunchPad → BLE5-Stack → project_zero → TI-RTOS → CCS Compiler → project_zero

    ../_images/ble5_ccs_import_project_zero.png

    Figure 48. Import CCS Projects

  4. Select the CCS Logo button to import project into Project Explorer

    Attention

    The import process will also install the SimpleLink CC13xx/CC26xx SDK if a local version does not exist. You must accept the End User License Agreement to proceeed.

    ../_images/eula.png

    Figure 49. Install SimpleLink CC13xx/CC26xx SDK

    After the installation finishes, you must reopen CCS before importing the project.

    • If everything is successful, the project should appear in Resource Explorer: project_zero_app_CC26X2R1_LAUNCHXL_tirtos_ccs.

    ../_images/ble5_ccs_project_explorer_after_import.png

    Figure 50. Projects Imported into CCS

Build and Download Project

Note

  • For projects with the stack as a library, the Stack project should always be built before the Application project.

  • For projects containing the TI OAD Profile, it is recommended to build the BIM first. A pre-built BIM hex file is also available, and can be used as instructed below.

To build & download Project Zero:

  1. Flash the BIM hex file.

    • The hex file can be found in examples → nortos → CC13xx or CC26xx LaunchPad → bim → hexfiles → bim_offchip → Debug_unsecure

    • Use Smart RF Flash Programmer 2 or Uniflash to program the hex file.

  2. Build the Application project.

    • Set the Application project as the active project.

    • Select Project -> Build All to build the Application project.

    • As part of the prebuild process, SysConfig will run and generate code based on the .syscfg in the workspace. For more information on SysConfig, see the SysConfig chapter of the User’s Guide.

  3. Load the Application project

    • Select Run -> Debug to download the application

Before beginning execution, open a terminal window with the following settings:

Table 1. Project Zero UART Settings

UART Param

Default Values

Baud Rate

115200

Data length

8 bits

Parity

None

Stop bits

1 bit

Flow Control

None

When the debugging session opens, click the Green start button to start execution. Continue on to the Running the Demo section for information about using Project Zero.

Warning

When using CCS compiler, the Configuration file for BLE5-Stack is suffixed .cfg. When using CCS compiler, modifying .xscfg files has no effect.

Using BLE5-Stack Projects with IAR

When building with IAR, it is recommended to enable all build messages. This can be done by right-clicking in the Build window and selecting “All” as shown below:

../_images/ble5_iar_enable_build_messages.png

Figure 51. Enable All Build Messages

Warning

Standalone SysConfig tool must be installed in order to use all the IAR projects and its location has to the same as specified by SYSCONFIG_ROOT.

The SysConfig standalone package can be found here: SysConfig Standalone Installer Download Page.

Import Project Using Workspace

This section describes how to open and build an existing project and references the project_zero project.

Warning

In this release of the SimpleLink CC13xx/CC26xx SDK all of the TI BLE5-Stack examples have been converted to the same structure as the TI Drivers examples.

This means that the global argument variables should always be used.

Custom Argvars type

BLE5 Projects

Keep in mind

Common / Global

  • All BLE Examples in this SDK

Import or re-enable the global SDK argvars via Tools -> Configure Custom Argument Variables

Per-workspace

  • Older SDKs and CC2640R2 SDK

Disable the global argvars, because IAR has already imported the appropriate settings for the workspace

Below you can see how to add and enable the SDK-global argument variables:

../_images/iar_custom_argvars_menu.png

Figure 52. Select Configure Custom Argument Variables from the Tools menu

../_images/iar_custom_argvars_empty.png

Figure 53. Click on Import… with either the Workspace or Global namespace selected. For Global, the imported values will persist for other projects also.

../_images/iar_custom_argvars_file.png

Figure 54. Find the Custom Argument Variables file under <SDK root>/tools/iar

../_images/iar_custom_argvars_selected.png

Figure 55. Success! Change these paths if you have installed in a different location.

Some of the TI BLE5-Stack workspace included in the SimpleLink CC13xx/CC26xx SDK have an Application project and a Stack Library project. Some have only an Application project.

In addition, applications containing the TI Over-the-Air Download (OAD) Profile will also include the Boot Image Manager (BIM) project. For more information on the TI OAD Profile and the BIM see the OAD Chapter of the BLE5-Stack User’s Guide.

Note

If you have imported the global <SDK_INSTALL_DIR>/tools/iar/SIMPLELINK_CC13XX_CC26XX_SDK.custom_argvars, then the examples from the older SDK or CC2640R2 SDK examples will fail to build. Therefore, you must remove this custom_argvars file from your IAR global custom arguments if you are working on multiple version of SDKs.

  1. Open the IAR Embedded Workbench IDE from the Start Menu.

  2. Open an IAR workspace project: File -> Open -> Workspace…

    • For this example, select <SDK_INSTALL_DIR>\examples\rtos\|LP|\ble5stack\project_zero\tirtos\iar\project_zero_app.template.eww

  3. This will prompt you to select a folder location as a workspace for the project

This workspace file is for the project_zero project. When selected, the files associated with the workspace become visible in the Workspace pane on the left side of the screen. See Figure 56.

Select either project as the active project by clicking the respective tab at the bottom of the workspace pane. In Figure 56., the Overview tab is selected. This tab displays the file structure for both projects simultaneously. In this case, use the drop-down menu at the top of the workspace pane to select the active project. Each of these projects produces a separate downloadable object.

Build and Download Project

To build & download Project Zero:

  1. Flash the BIM hex file.

    • The hex file can be found in examples → nortos → CC13xx or CC26xx LaunchPad → bim → hexfiles → bim_offchip → Debug_unsecure

    • Use Smart RF Flash Programmer 2 or Uniflash to program the hex file.

  2. Build the Application project.

    • Select the Application project.

    • Select Project -> Make to build the Application project.

    • As part of the prebuild process, SysConfig will run and generate code based on the .syscfg in the workspace. For more information on SysConfig, see the SysConfig chapter of the User’s Guide.

  3. Load the Application project

    • To download and debug: Select Project -> Download and Debug

    • To download without debugging: Select Project -> Download -> Download Active Application

Refer to the Project Zero README for more information about this project.

Before beginning execution, open a terminal window with the following settings:

Table 2. Project Zero UART Settings

UART Param

Default Values

Baud Rate

115200

Data length

8 bits

Parity

None

Stop bits

1 bit

Flow Control

None

When the debugging session opens, click the start button to start execution. Continue on to the Running the Demo section for information about using Project Zero.

Warning

When using IAR compiler, the Configuration file for BLE5-Stack is suffixed .xscfg. When using IAR compiler, modifying .cfg file has no effect.

Running the Demo

After hitting the play button, your terminal window should display the Project Zero initialization information as shown below:

../_images/ble5_pz_terminal_initialization.png

Figure 57. Project Zero Initialization

This provides information about the services present in Project Zero. Project Zero has 4 interactive services: the LED service, the button service, the data service, and the OAD service.

Writing a non-zero value to the LED service will cause the LEDs on the LaunchPad to light up. Writing zero will turn them off. Enabling notifications on the Button service will cause the Peripheral to send notifications of current button state (0 - not pressed, 1 - pressed) to the Central device. The Data service can be used to read and write multiple bytes of data. The OAD service can be used for updating the image currently running on the LaunchPad.

Choose the Central device from the list below to connect with:

Click to Expand BTool Instructions

Host Test Setup

The easiest way to connect to Project Zero with another CC13xx/CC26xx LaunchPad is by using BTool. BTool allows you to send HCI commands to the LaunchPad to easily establish BLE communication with another device.

To use BTool, you must flash your second CC13xx or CC26xx LaunchPad with the Host Test firmware from a compatible version of the TI BLE-Stack/BLE5-Stack. Pre-built Host Test binaries are included in the ble5stack examples directory of the SDK.

Uniflash can be used to program the LaunchPad with the Host Test firmware:

../_images/ble5-uniflash-host-test.png

Figure 58. Flash Host Test using Uniflash

Open BTool from the tools\ble5stack\btool folder of the SDK_INSTALL_DIR. Start BTool by double clicking Run_BTool.bat Select the XDS110 UART COM Port for your Host Test LaunchPad:

../_images/btool_serial_port.png

Figure 59. BTool Serial Port Settings

When BTool connects to the LaunchPad, it will issue several initialization commands. If the commands succeed, you will receive multiple HCI Events with a Status of “SUCCESS”.

Connect to Project Zero

Scan for nearby advertising Bluetooth devices by selecting the Scan button in the Discovery window. Make sure your Project Zero LaunchPad is connected to power and advertising.

Compare the device addresses in the Slave BDA dropdown with the address shown in the Project Zero terminal window. Select the matching address and click “Establish” to connect to Project Zero.

../_images/btool-scan-connect.png

Figure 60. Scanning & Connecting with BTool

After the connection has established, discover & read the current value of the services and characteristics available on Project Zero by right-clicking on the Handle in the Connection Info section and selecting Read Values.

../_images/btool-read-values.png

Figure 61. BTool GATT Table Discovery

The bottom of the BTool GUI will display the Project Zero GATT Table to help you navigate and control the Project Zero services.

../_images/btool-gatt-table.png

Figure 62. BTool GATT Table Discovery

Using the LED Service

Writing 0x01 to the characteristics in the LED Service will turn on the Project Zero LaunchPad LEDs. You can write to the characteristic by double clicking the Value field of the LED0 State or LED1 State characteristics.

../_images/btool-write-item.png

Figure 63. Writing to a Characteristic

The Project Zero terminal window will update with the current LED state:

../_images/ble5_leds_on.png

Figure 64. Turning on Project Zero LEDs

Using the Button Service

You can choose to receive notifications about the current state of the Project Zero Button Service by writing 01:00 to the Client Characteristic Configuration Descriptors of the Button Service. After enabling notifications, the current value of the Button state will be displayed in BTool.

../_images/btool-enable-notifications.png

Figure 65. Enabling Notifications in BTool

../_images/ble5_button_notifications.png

Figure 66. Pressing & Releasing Buttons

Using the Data Service

You can read and write multiple bytes of data by using the Data Service. Double click on the Value field of the String Char. You can write the new value directly in ASCII or you can choose a different type by selecting from the Value Type dropdown menu.

../_images/btool-write-string.png

Figure 67. Writing to the Data Service

../_images/ble5_writing_data.png

Figure 68. Data Service Value change

Using the OAD Service

Project Zero includes the TI OAD Profile which allows you to download new firmware images over-the-air. Images must be compatible with the CC13xx or CC26xx and contain the TI OAD Profile in order to be downloaded successfully. For more information on creating a new image for OAD, please see the OAD Chapter of the BLE5-Stack User’s Guide.

Note

If Project Zero was not the first image containing the TI OAD Profile you flashed on your LaunchPad Out-of-the-Box, the factory image in your external flash may not be Project Zero. This could mean that you will be unable to return to Project Zero by using the factory reset option after performing an OAD and will have to use the debugger to load a new image.

Refer to the Project Zero README for more information about this project and resetting the factory image contained in external flash.

In BTool, choose Over The Air Download in the “Select Device Operation” box. In this demo, we will use Project Zero as our example since a valid image was created during the build process.

Select the new image to load on your CC13xx or CC26xx LaunchPad by clicking Read Image File. Navigate to your Project Zero build output directory. Select the *_oad.bin file. The *_oad.bin file will contain a valid image header.

BTool will send a connection parameter update at the beginning of an OAD to attempt a faster download. The embedded application will also attempt a parameter update (if enabled). It is recommended to wait until the application’s connection parameter update has taken place before starting an OAD. If you are experiencing a slow OAD, this may be the cause. The parameter update is complete once the following message is shown in the BTool log:

--------------------------------------------------------------------
[7] : <Rx> - 04:16:04.518
-Type           : 0x04 (Event)
-EventCode      : 0x00FF (HCI_LE_ExtEvent)
-Data Length    : 0x0B (11) bytes(s)
 Event          : 0x0607 (1543) (GAP_LinkParamUpdate)
 Status         : 0x00 (0) (SUCCESS)
 ConnHandle     : 0x0000 (0)
 ConnInterval   : 0x0024 (36)
 ConnLatency    : 0x0000 (0)
 ConnTimeout    : 0x00C8 (200)
Dump(Rx):
0000:04 FF 0B 07 06 00 00 00 24 00 00 00 C8 00       ........$.....
--------------------------------------------------------------------
../_images/btool_oad_header.png

Figure 69. Updating Firmware Image with BTool

Once you are sure this is the image you want to run, click Send to begin the OAD process.

The Status bar will provide information on the current status of the download. If the download completes successfully, you will receive a “OAD Download Successful” message in BTool.

Note

After an OAD has completed, you may need to manually hit the reset button on the CC13xx or CC26xx LaunchPad in order to trigger a full reset and jump to BIM. This step is only required after first programming the device.

This will disconnect the debugger and terminate the debugging section.

Click to Expand iOS Instructions

Download the latest version of the TI SimpleLink Starter app from the iOS app store. When the download completes, open the app:

../_images/ble5_simplelink_starter_app.png

Figure 70. SimpleLink Starter App

Connect to Project Zero

When the app opens, nearby Bluetooth Low Energy devices will appear. You should see ProjectZero advertising as shown below:

../_images/ble5_simplelink_starter_advertising.png

Figure 71. Project Zero Advertising

Press the Project Zero item and select Sensor View. The services present in Project Zero will appear as shown below:

../_images/ble5_simplelink_starter_sensor_view.png

Figure 72. Project Zero Advertising

The Project Zero terminal information will also update with connection information including the peer device address, PHY, and MTU Size. For more information about these parameters, see the BLE5-Stack User’s Guide.

../_images/ble5_pz_terminal_connection.png

Figure 73. Project Zero After Connection

Using the LED Service

To turn on an LED, press one of the buttons on the LED service. The left button turns on the Red LED (DIO6). The right button turns on the Green LED (DIO7). Pressing the button again will turn the LED off. The Project Zero terminal window will update with the current LED state.

../_images/ble5_simplelink_starter_led_service.png

Figure 74. Project Zero LED Service

../_images/ble5_leds_on.png

Figure 75. Turning on Project Zero LEDs

Using the Button Service

Button press notifications are automatically enabled when connecting through the Sensor View. If you press and release either button, the Sensor View will update with the current state and the button state graph will show the button state over time (High corresponds to button pressed, low corresponds with button released).

../_images/ble5_simplelink_starter_button_service.png

Figure 76. Project Zero Button Service

../_images/ble5_button_notifications.png

Figure 77. Pressing & Releasing Buttons

Using the Data Service

The Data Service is not displayed in Sensor View. To use the Data Service, close the Sensor View by pressing the < Sensor Tag button in the upper left. This returns you to the main SensorTag view. Press the ProjectZero icon again and now select Service Explorer. The Data Service is the service with the UUID that begins with F0001130 (List Item 3). Press the item and you will see two characteristics. The first characteristic can be used to read and write multiple bytes of data. You can do this by pressing Read characteristic to get data from ProjectZero and Write w/response characteristic to send multiple bytes of data to ProjectZero.

../_images/ble5_simplelink_starter_data_service.png

Figure 78. Project Zero Data Service

../_images/ble5_writing_data.png

Figure 79. Writing to the Data Service

Using the OAD Service

Return to the Sensor View by returning to the main SensorTag view and reconnecting to Project Zero using the Sensor View. Select FW Download (Enhanced) to use the TI OAD Profile to download a new image to your LaunchPad Over-the-Air.

Note

If Project Zero was not the first image containing the TI OAD Profile you flashed on your LaunchPad Out-of-the-Box, the factory image in your external flash may not be Project Zero. This could mean that you will be unable to return to Project Zero by using the factory reset option after performing an OAD and will have to use the debugger to load a new image.

Refer to the Project Zero README for more information about this project and resetting the factory image contained in external flash.

Select a new image to load on your CC13xx or CC26xx LaunchPad by pressing Select FW File. This will display a selection of available firmware images. To select a new BLE5-Stack image, choose either Project Zero or Simple BLE Peripheral, then select Start OAD. To select a new image for a different wireless technology, choose the firmware image of choice, select Start OAD and skip to the applicable Running the Demo section of the Quick Start Guide.

After selecting Start OAD, the SimpleLink Starter app will display download progress:

../_images/ble5_simplelink_starter_oad_progress.png

Figure 80. Performing an OAD

Note

After an OAD has completed, you may need to manually hit the reset button on the CC13xx or CC26xx LaunchPad in order to trigger a full reset and jump to BIM This step is only required after first programming the device.

This will disconnect the debugger and terminate the debugging section.

Click to Expand Android Instructions

Download the latest version of the TI SimpleLink Starter app from your app store. When the download completes, open the app:

../_images/ble5_android_starter_app.png

Figure 81. SimpleLink Starter App

Enable location permissions to allow the app to function properly:

../_images/ble5_android_starter_permissions.png

Figure 82. SimpleLink Starter Location Permissions

Connect to Project Zero

Open the SimpleLink Starter app on your device. The app should begin scanning for BLE devices automatically but you can force a refresh by pulling down on the device list. Make sure your Project Zero LaunchPad is nearby and advertising. Project Zero should appear in the Bluetooth low energy devices list:

../_images/ble5_android_advertising.png

Figure 83. Discovering Project Zero

Establish a connection to the Project Zero by clicking on its name in the devices list. The SimpleLink Starter application will display the Project Zero services and displays GUI widgets to interact.

../_images/ble5_android_services.png

Figure 84. Project Zero Services

Using the LED Service

To turn on an LED, press one of the buttons on the LED service. The left button turns on the Red LED (DIO6). The right button turns on the Green LED (DIO7). Pressing the button again will turn the LED off. The Project Zero terminal window will update with the current LED state.

../_images/ble5_simplelink_starter_led_service.png

Figure 85. Project Zero LED Service

../_images/ble5_leds_on.png

Figure 86. Turning on Project Zero LEDs

Using the Button Service

Button press notifications are automatically enabled when connecting through the Sensor View. If you press and release either button, the Sensor View will update with the current state and the button state graph will show the button state over time (High corresponds to button pressed, low corresponds with button released).

../_images/ble5_simplelink_starter_button_service.png

Figure 87. Project Zero Button Service

../_images/ble5_button_notifications.png

Figure 88. Pressing & Releasing Buttons

Using the Data Service

The Data Service is not displayed in Sensor View. To use the Data Service, you will need to switch to the Service Explorer view. Tap Service Explorer in the top right of the screen to switch views. The Data Service is the service with the UUID that begins with F0001130 (Project Zero Stream Service). Tap the item and you will see two characteristics. The first characteristic can be used to read and write multiple bytes of data. You can do this by pressing Read characteristic to get data from ProjectZero and Write w/response characteristic to send multiple bytes of data to ProjectZero.

../_images/ble5_simplelink_starter_data_service.png

Figure 89. Project Zero Data Service

../_images/ble5_writing_data.png

Figure 90. Writing to the Data Service

Using the OAD Service

Return to the Sensor View by returning to the main SensorTag view and reconnecting to Project Zero using the Sensor View. Select FW Download (Enhanced) to use the TI OAD Profile to download a new image to your LaunchPad Over-the-Air.

Note

If Project Zero was not the first image containing the TI OAD Profile you flashed on your LaunchPad Out-of-the-Box, the factory image in your external flash may not be Project Zero. This could mean that you will be unable to return to Project Zero by using the factory reset option after performing an OAD and will have to use the debugger to load a new image.

Refer to the Project Zero README for more information about this project and resetting the factory image contained in external flash.

Select a new image to load on your CC13xx or CC26xx LaunchPad by pressing Select FW File. This will display a selection of available firmware images. To select a new BLE5-Stack image, choose either Project Zero or Simple BLE Peripheral, then select Start OAD. To select a new image for a different wireless technology, choose the firmware image of choice, select Start OAD and skip to the applicable Running the Demo section of the Quick Start Guide.

After selecting Start OAD, the SimpleLink Starter app will display download progress:

../_images/ble5_simplelink_starter_oad_progress.png

Figure 91. Performing an OAD

Note

After an OAD has completed, you may need to manually hit the reset button on the CC13xx or CC26xx LaunchPad in order to trigger a full reset and jump to BIM This step is only required after first programming the device.

This will disconnect the debugger and terminate the debugging section.

Learning More About TI BLE5-Stack

Resources contained in the Learn track of Figure 47. are intended for users who are new to BLE or TI-RTOS. These modules demonstrate how to create custom applications with TI BLE5-Stack and TI’s Real Time Operation System (TI-RTOS).

SimpleLink Academy provides a comprehensive set of training tools that allow users from beginners to experienced developers to learn about the SimpleLink MCU Platform.

Using introductory material and labs, learn the fundamentals of BLE and how to develop a custom BLE profile.

SimpleLink Academy also contains modules written to demonstrate the rich debug environment and peripheral driver capability provided by TI-RTOS.

This material teaches users who are new to TI-RTOS or any RTOS programming in general about TI’s RTOS kernel implementation.

Modules within the kernel training greatly expand the information presented in the TI-RTOS Overview chapter in the TI BLE5-Stack User’s Guide.

Learn how the TI-RTOS provides the most optimal power management and design flexibly.

Developing a New BLE5-Stack Based Application

The develop track of Figure 47. is intended for programmers who are ready to start developing an end product using the CC13xx or CC26xx. To begin:

Get Familiar with the BLE5-Stack User’s Guide

This User’s Guide is meant to be used alongside the TI BLE5-Stack when developing an end product. It contains documentation on the stack architecture, APIs, and suggestions for developing applications.

Select an Example Project

The TI BLE5-Stack includes a basic set of projects to use as a starting point for development of your custom application. Click the links below to find out more information about each project:

Table 3. BLE examples available for the CC13xx or CC26xx platform

Name

Description

host_test

A network processor project that is interfaced with HCI and Vendor Specific HCI commands.

multi_role

Provides the ability to operate function in multiple simultaneous connection roles.

project_zero

Feature rich peripheral application that provides LED and button functionality OOB.

rtls_coordinator

A project implements a simple Bluetooth Low Energy central device with GATT client and angle of arrival (AoA) functionality.

rtls_responder

A project implements a simple Bluetooth Low Energy peripheral device with GATT server and sends out special angle of arrival packets to enable real time locationinig.

rtls_passive

rtls_passive is a combination of Connection Monitor (CM) and RTLS examples. It uses the connection monitor to monitor a BLE connection, receive AoA packets and measure RSSI.

simple_broadcaster

Demonstrates a simple Bluetooth Low Energy broadcaster application that implements non-connectable advertisements.

simple_central

Implements a basic BLE central device with GATT client functionality.

simple_peripheral

Demonstrates a simple Bluetooth Low Energy slave application that implements connectable advertisements and a simple profile.

simple_peripheral_oad_offchip

Same as simple_peripheral above with off-chip OAD functionality to enable wireless firmware updates.

simple_peripheral_oad_onchip

Same as simple_peripheral above with on-chip OAD functionalityto enable wireless firmware updates.

Troubleshooting Help

While developing your custom application, you may run into issues that require the use of a debugger. See the Debugging chapter in the TI BLE5-Stack User’s Guide for guidance.

Developing a New BLE Mesh Application

Get Familiar with the Bluetooth Mesh Section of the BLE5-Stack User’s Guide

Take a look at the TI Bluetooth Mesh Quick Start Guide for an overivew of our Bluetooth Mesh Application. It contains documentation on the implementation architecture, APIs, and suggestions for developing applications.

As Bluetooth Mesh builds on top of Bluetooth Low Energy v4.2, our BLE5-Stack User’s Guide should also be referenced when developing an end product.

Select an Example Project

The TI BLE5-Stack includes a basic set of projects to use as a starting point for development of your custom application. Click the links below to find out more information about each project:

Table 4. BLE Mesh examples available for the CC13xx or CC26xx platform

Name

Description

simple_mesh_node

Implements a basic BLE mesh node with Relay, Proxy, Friend, and Low Power Node capabilities using GATT/ADV bearer

simple_mesh_node_oad_offchip

Same as simple_mesh_node above with off-chip OAD functionality to enable wireless firmware updates.

simple_mesh_node_oad_onchip

Same as simple_mesh_node above with on-chip OAD functionality to enable wireless firmware updates.

mesh_app_python

A Python based network processor project that interfaces with a simple_mesh_node

Troubleshooting Help

While developing your custom application, you may run into issues that require the use of a debugger. See the Debugging chapter in the TI BLE5-Stack User’s Guide for guidance.

Enhance Your Project

The enhance track of Figure 47. is intended to take your product to the next level by leveraging TI’s web-based collateral. Additional resources found in these pages include application-specific source code examples, smart phone source code, and complete sub-system designs.

Additional sample applications created to implement specific use cases and examples. These are made to work in conjunction with the SDK.

Examples of system designs containing complete hardware and software examples, using the CC13xx or CC26xx.

Bluetooth Qualification

Texas Instruments experts have written the How to Certify Your Bluetooth Product guide to assist you through this process.

Getting Support

The support track of Figure 47. is intended to provide you additional help and resources that aren’t contained in the previous tracks

A support community providing answers to questions relating to the 7.10.00.xx and the CC13xx or CC26xx. You can browse questions from other developers or ask your own questions if you run into issues developing with 7.10.00.xx.