SimpleLink Common Commponents Module 5.10.00 Release Notes
Table of Contents
Introduction
The SimpleLink Common Components Module (SCCM) includes Common User Interface (CUI), NV Interface (Non-volatile Memory Interface), Boot Image Manager (BIM) on- and off-chip, and MCUBoot. These release notes include bug fixes, updates, and new features for the SCCM components.
Documentation
The follow table details which SCCM components are supported by the different SimpleLink stacks
| Stack | CUI | NV | BIM on-chip | BIM off-chip | MCUBoot |
|---|---|---|---|---|---|
| BLE | X | X | X | X [1] | |
| 15.4 | X | X | X | X | X [1] |
| Zigbee | X | X | X | ||
| Thread | X | X | X | ||
| DMM | X | X | X | ||
| WiSUN | X | X [2] | |||
| PropRF | X | X | X |
- [1] Only applies to CC13x4 and CC26x4 devices
- [2] Only applies to CC13x2x7, CC26x2x7, CC13x4, and CC26x4 devices
What’s New
| ID | Summary |
|---|---|
| SCCM-306 | Create universal imgtool executable for macOS |
| SCCM-295 | Enable MCUBoot Anti-Rollback for CC2340R5 and CC13x4/26x4 |
| SCCM-290 | Include split_image_tool in the relevant packages |
| SCCM-254 | Moving BIM hex file locations to BIM example folders |
| SCCM-233 | Add MCUBoot support for S/NS images |
| SCCM-215 | Add MCUBoot support for CC13x4/CC26x4 |
| SCCM-201 | Enable MCUBoot for CC13x2/26x2 R7 devices |
Fixed Issues
| ID | Summary |
|---|---|
| SCCM-288 | NVOCMP: Power loss during NV_write causes NV corruption |
| SCCM-277 | NVCOMP improved check for “all items active” condition |
| SCCM-246 | BIM does not set verification byte to pass state |
Known Issues and Limitations
| ID | Summary |
|---|---|
| None | None |
It should be noted that multiple external NVS regions are not supported. If a user attempts to create a second external NVS region, all actions on the second region will be done on the first region.
Upgrade and Compatibility Information
Dependencies
SCCM components were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.