Packet Format¶
Messages on the IEEE PHY layer always have the following structure:
- Element Length
Length of the recieved packet, including PHY Header.
- PHY Header
carries the frame length byte, which indicates the length of the PHY Service Data Unit (PSDU).
- MAC Header and Payload
which has the frame control, a Data Sequence Number, address data, and payload.
- MAC Footer (FCS)
contains a 16-bit Frame Check Sequence.
- RSSI
a byte indicating the received RSSI value (Optional).
- Status
May contain receive correlation, and crc result bit field (optional).
- Source Index
a byte giving the index of the first source matching entry that matches the header of the received packet is appended, or 0xFF if no match (optional).
- Time Stamp
a time stamp indicating the start of the frame (optional).

‘0 - 2 bytes’ |
‘0 or 1 bytes’ |
‘0 - 125 bytes’ |
‘0 or 2 bytes’ |
‘0 or 1 byte’ |
‘0 or 1 byte’ |
‘0 or 1 byte’ |
‘0 or 4 byte’ |
‘Element Length’ |
‘PHY Header’ |
MAC Header and Payload |
MAC Footer (FCS) |
RSSI |
‘Status’ |
‘Source Index’ |
‘Time Stamp’ |