Shade Example Application
Table of Contents
- SysConfig Notice
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Functional Description
- Configuration With SysConfig
- Usage
Introduction
This document discusses how to use the Shade Example App and the different parts that compose it. Shade Example Application is a standalone CoAP server example running on Thread.
Some of the areas explored are:
Setting up a network.
Bringing up the device as a Minimum Thread Device(MTD).
Initialization and use of the Constrained Application Protocol (CoAP) APIs.
Hardware Prerequisites
2 x CC13X2 / CC26X2 Wireless MCU LaunchPads
(optional) 1 x Sharp128 LCD boosterpack.
Software Prerequisites
- Code Composer Studio (CCS) v10.0 or higher
Functional Description
Software Overview
This section describes software components and the corresponding source file.
Application Files
shade.[ch]
: Contains the application's event loop, CoAP callback functions, and device initialization function calls, and all shade specific logic.otstack.[ch]
: OpenThread stack processing, instantiation and network parameters.task_config.h
: This file contains the definitions of the RTOS task priorities and stack sizes.images.[ch]
: Contains the raw binary of the images being displayed on the LCD screen.tiop_config.[ch]
: Contains OpenThread stack configurations. If using a SysConfig-enabled project (see the Configuration with SysConfig section below), these files are generated and configured through the SysConfig GUI. If using a non-SysConfig project, the files are a part of the project and parameters can be directly modified.tiop_ui.[ch]
: Contains functions and defines to enable Thread-specific functionality for the Common User Interface (CUI).tiop_app_defs.h
: Contains application-specific configurations for CUI.
Example Application
This application provides an example implementation of a shade (blinds) using the Thread wireless protocol and CoAP as the application layer protocol. The shade application is configured as a Minimal Thread Device (MTD) which supports CoAP commands to control the shade state. The shade can be in three states: open, closed, and drawn.
Configuration With SysConfig
SysConfig is a GUI configuration tool that allows for TI driver and stack
configurations. In order to configure projects using SysConfig, use the
SysConfig-enabled version of the Thread examples located in
<SDK_ROOT>/examples
To configure using SysConfig, import the SysConfig-enabled project into CCS.
Double click the *.syscfg
file from the CCS project explorer, where *
is
the name of the example project. The SysConfig GUI window will appear, where
Thread stack and TI driver configurations can be adjusted. These settings will
be reflected in the generated files tiop_config.[ch]
.
The example project comes with working default settings for SysConfig. It is not recommended to change the default driver settings, as any changes may impact the functionality of the example. The Thread stack settings may be changed as required for your use case.
One important note about TI-OpenThread SysConfig is how SysConfig settings and non-volatile storage settings are applied. If the LaunchPad non-volatile holds a valid Thread dataset, SysConfig settings will not be applied on boot. SysConfig settings are only applied when non-volatile storage does not hold a valid Thread dataset. To guarantee SysConfig settings are applied, perform a factory reset of the non-volatile storage, as described below.
Usage
This section describes how to set up and run the Shade Example Application.
Buttons
BTN-2
at boot: A factory reset of the non-volatile storage is performed. This must be pressed at the start of theOtStack_task
function.BTN-2
: Start the joining process. This may be pressed after the hold image appears on-screen.
Display
There are 2 ways that this application will display information to the user which can be used simultaneously and are described below:
Serial terminal: The shade events will be displayed through UART to a serial terminal emulator. To enable the serial terminal in CCS press
Ctrl + Shift + Alt + T
, selectSerial Terminal
underChoose terminal
, select115200
for Baud Rate and clickOK
. PuTTY may also be used as the serial terminal emulator. The serial interface implements a Common User Interface (CUI). More details are provided in the "Example Applications" section in the Thread docs of the SDK. Application-specific portions of CUI are described below.Sharp128 LCD boosterpack: There is no extra configuration needed to use the LCD boosterpack other than plugging it to the LaunchPad running the example application.
Setting up the Thread Network
This section describes how to set up a Thread network. The application supports
the ability to be commissioned into a Thread network. Commissioning may be
bypassed by setting the TIOP_CONFIG_SET_NW_ID
parameter to 1 in
tiop_config.h
and setting the network ID parameters there. This can also be
done through SysConfig in the TI-OpenThread stack module, under the Network ID
submodule. By setting the PAN ID to a valid, non-broadcast ID (not 0xFFFF), the
device can be pre-commissioned to an existing network.
Set up a LaunchPad as a CLI FTD device by following the README files in the respective application folder.
Load and run the Shade example on a second LaunchPad.
The Shade will print out the device's EUI64 and the application's PSKd (pre-shared key device identifier) over CUI. If the device has already been commissioned, skip to step 8.
Device Info: [EUI64] 0x00124b000f6e6113 [PSKD] SHADEEX1
Start a commissioner on the CLI FTD by issuing the following command:
commissioner start
. It will displayDone
if it succeeds in becoming the active commissioner.Add the Shade LaunchPad device as a joiner device by providing the EUI64 and pskd (from step 3) as credentials to the commissioner:
commissioner joiner add 00124b000f6e6113 SHADEEX1
. It will displayDone
if it is successful in adding the joiner entry.Now on the Shade LaunchPad, press
BTN-2
to start the joining process. The display will showJoining Nwk ...
.Once the joining process has successfully completed, the display will show
Nwk Joined
. If the LCD is used, it will then switch to the shade image. The green LED should turn on on the LaunchPad once it has joined the network.Next we need to get the IPv6 address of the shade LaunchPad. On the CLI, use the command
ping ff03::1
to send an ICMP echo request to the realm-local all nodes multicast address. All devices on the Thread network will respond with an ICMP echo response. You will see in the terminal a response like the one below.8 bytes from fd00:db7:0:0:0:ff:fe00:b401: icmp_seq=1 hlim=64 time=11ms
Interfacing with the Shade Example Application
The shade application hosts a simple CoAP server with one registered resource for the blind state. This resource supports CoAP GET and POST commands. Any device with scope of the shade's IPv6 address can send commands to the shade application.
Shade Attribute URI:
- Shade state:
blinds/state
Open up the serial terminal to the cli_ftd
application and also to the shade
application.
Starting the CoAP client
In the CLI FTD serial terminal, execute coap start
at the prompt to start the
CoAP service. It will display the following message if it successful in
starting the CoAP service. Coap service started: Done
Getting status from the Shade
To get the shade's blind state, execute the following command on the CLI FTD terminal.
coap get fd00:db7:0:0:0:ff:fe00:b401 /blinds/state
NOTE: The IPv6 address will be different for your setup
The shade should respond, and the cli_ftd
will print a message like the
following.
Received coap response with payload: 636c6f736564
Converting the payload from hex to ascii we get closed
.
Controlling the Shade
The shade state can be changed by sending the appropriate payload in a CoAP confirmable (con) POST command message, to the IPv6 address of the shade and the resource URI attribute.
Use the following command in the CLI FTD terminal to set the shade's blind state to open.
coap post fd00:db7:0:0:0:ff:fe00:b401 blinds/state con open
NOTE: The IPv6 address will be different for your setup
The initial command will result in the message Sending coap request: Done
.
The shade will respond, and the CLI FTD will print the following message.
Received coap response with payload: 636c6f736564
If the POST was successful, then the shade will indicate this on the LCD or UART terminal. If a LCD boosterpack is used, the shade will change the image displayed. If a UART terminal is used, the shade will print its updated state.
APP Info: [Shade State] open
The above process can be repeated with the string closed
or drawn
in place
of open
to set the shade example to those respective state.
Application-specific CUI
The application-specific actions for the Shade example are OPEN SHADE
, CLOSE
SHADE
, and DRAW SHADE
:
TI Thread Shade
< OPEN SHADE >
This action will set the state of the shade to "open". To use, hit the "Enter" key.
TI Thread Shade
< CLOSE SHADE >
This action will set the state of the shade to "closed". To use, hit the "Enter" key.
TI Thread Shade
< DRAW SHADE >
This action will set the state of the shade to "drawn".To use, hit the "Enter" key.