43 #ifndef ti_drivers_adc_ADCCC26XX__include 44 #define ti_drivers_adc_ADCCC26XX__include 53 #include <ti/devices/DeviceFamily.h> 54 #include DeviceFamily_constructPath(driverlib/aux_adc.h) ADCCC26XX_Trigger_Source triggerSource
Definition: ADCCC26XX.h:161
Definition: ADCCC26XX.h:83
Definition: ADCCC26XX.h:76
ADCCC26XX_Reference_Source refSource
Definition: ADCCC26XX.h:157
ADCCC26XX Object.
Definition: ADCCC26XX.h:169
Definition: ADCCC26XX.h:120
bool returnAdjustedVal
Definition: ADCCC26XX.h:151
bool isProtected
Definition: ADCCC26XX.h:174
Power manager interface for CC26XX/CC13XX.
ADCCC26XX_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCCC26XX.h:69
const ADC_FxnTable ADCCC26XX_fxnTable
ADCCC26XX_Trigger_Source
List of sources the ADC can be configured to trigger off of.
Definition: ADCCC26XX.h:130
Definition: ADCCC26XX.h:82
Analog to Digital Conversion (ADC) Input Driver.
Definition: ADCCC26XX.h:77
Definition: ADCCC26XX.h:80
Definition: ADCCC26XX.h:81
uint8_t adcCompBInput
Definition: ADCCC26XX.h:149
The definition of an ADC function table that contains the required set of functions to control a spec...
Definition: ADC.h:354
Definition: ADCCC26XX.h:72
uint8_t adcDIO
Definition: ADCCC26XX.h:147
bool isOpen
Definition: ADCCC26XX.h:172
ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
Definition: ADCCC26XX.h:144
Definition: ADCCC26XX.h:75
Definition: ADCCC26XX.h:71
Definition: ADCCC26XX.h:78
Definition: ADCCC26XX.h:73
bool inputScalingEnabled
Definition: ADCCC26XX.h:153
ADCCC26XX_Sampling_Duration samplingDuration
Definition: ADCCC26XX.h:159
Definition: ADCCC26XX.h:132
uint_fast32_t refVoltage
Definition: ADCCC26XX.h:155
Definition: ADCCC26XX.h:74
Definition: ADCCC26XX.h:79
ADCCC26XX_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCCC26XX.h:118
Definition: ADCCC26XX.h:121