GATTServApp layer interface.
|
#define | GATT_ALL_SERVICES 0xFFFFFFFF |
| All profile services bit fields.
|
|
#define | GATT_ATT(type, permission, value) |
| GATT Custom Attribute. More...
|
|
#define | GATT_ATT_BT_UUID_TYPE(type) {ATT_BT_UUID_SIZE,type} |
| GATT BT Attribute Type format.
|
|
#define | GATT_ATT_UUID_TYPE(type) {ATT_UUID_SIZE,type} |
| GATT Custom Attribute Type format.
|
|
#define | GATT_BT_ATT(type, permission, value) |
| GATT BT Attribute. More...
|
|
#define | GATT_BT_UUID(name, UUID) |
| GATT BT UUID. More...
|
|
#define | GATT_CCC_TBL(pValue) ( (gattCharCfg_t *)(*((PTR_TYPE)(pValue))) ) |
| Client Characteristic Configuration table (from CCC attribute value pointer)
|
|
#define | GATT_CFG_NO_OPERATION 0x0000 |
| No operation.
|
|
#define | GATT_CLIENT_CFG_INDICATE 0x0002 |
| The Characteristic Value shall be indicated.
|
|
#define | GATT_CLIENT_CFG_NOTIFY 0x0001 |
| The Characteristic Value shall be notified.
|
|
#define | GATT_CLIENT_CHAR_CFG_UPDATED_EVENT 0x00 |
| Sent when a Client Characteristic Configuration is updated. This event is sent as an OSAL message defined as gattCharCfgUpdatedEvent_t.
|
|
#define | GATT_EXT_PROP_RELIABLE_WRITE 0x0001 |
| Permits reliable writes of the Characteristic Value.
|
|
#define | GATT_EXT_PROP_WRITABLE_AUX 0x0002 |
| Permits writes to the characteristic descriptor.
|
|
#define | GATT_FORMAT_2BIT 0x02 |
| Unsigned 2 bit integer.
|
|
#define | GATT_FORMAT_BOOL 0x01 |
| Unsigned 1 bit; 0 = false, 1 = true.
|
|
#define | GATT_FORMAT_DUINT16 0x18 |
| IEEE-20601 format.
|
|
#define | GATT_FORMAT_FLOAT 0x17 |
| IEEE-11073 32 bit FLOAT.
|
|
#define | GATT_FORMAT_FLOAT32 0x14 |
| IEEE-754 32 bit floating point.
|
|
#define | GATT_FORMAT_FLOAT64 0x15 |
| IEEE-754 64 bit floating point.
|
|
#define | GATT_FORMAT_NIBBLE 0x03 |
| Unsigned 4 bit integer.
|
|
#define | GATT_FORMAT_SFLOAT 0x16 |
| IEEE-11073 16 bit SFLOAT.
|
|
#define | GATT_FORMAT_SINT12 0x0d |
| Signed 12 bit integer.
|
|
#define | GATT_FORMAT_SINT128 0x13 |
| Signed 128 bit integer.
|
|
#define | GATT_FORMAT_SINT16 0x0e |
| Signed 16 bit integer.
|
|
#define | GATT_FORMAT_SINT24 0x0f |
| Signed 24 bit integer.
|
|
#define | GATT_FORMAT_SINT32 0x10 |
| Signed 32 bit integer.
|
|
#define | GATT_FORMAT_SINT48 0x11 |
| Signed 48 bit integer.
|
|
#define | GATT_FORMAT_SINT64 0x12 |
| Signed 64 bit integer.
|
|
#define | GATT_FORMAT_SINT8 0x0c |
| Signed 8 bit integer.
|
|
#define | GATT_FORMAT_STRUCT 0x1b |
| Opaque structure.
|
|
#define | GATT_FORMAT_UINT12 0x05 |
| Unsigned 12 bit integer.
|
|
#define | GATT_FORMAT_UINT128 0x0b |
| Unsigned 128 bit integer.
|
|
#define | GATT_FORMAT_UINT16 0x06 |
| Unsigned 16 bit integer.
|
|
#define | GATT_FORMAT_UINT24 0x07 |
| Unsigned 24 bit integer.
|
|
#define | GATT_FORMAT_UINT32 0x08 |
| Unsigned 32 bit integer.
|
|
#define | GATT_FORMAT_UINT48 0x09 |
| Unsigned 48 bit integer.
|
|
#define | GATT_FORMAT_UINT64 0x0a |
| Unsigned 64 bit integer.
|
|
#define | GATT_FORMAT_UINT8 0x04 |
| Unsigned 8 bit integer.
|
|
#define | GATT_FORMAT_UTF16S 0x1a |
| UTF-16 string.
|
|
#define | GATT_FORMAT_UTF8S 0x19 |
| UTF-8 string.
|
|
#define | GATT_INCLUDED_HANDLE(attrs, i) ( *((uint16 *)((attrs)[(i)].pValue)) ) |
| The handle of the first included service (i = 1) is the value of the second attribute.
|
|
#define | GATT_LOCAL_READ 0xFF |
| GATT local read.
|
|
#define | GATT_LOCAL_WRITE 0xFE |
| GATT local write.
|
|
#define | GATT_NS_BT_DESC_UNKNOWN 0x0000 |
| The description is unknown.
|
|
#define | GATT_NS_BT_SIG 0x01 |
| Bluetooth SIG namespace.
|
|
#define | GATT_NS_NONE 0x00 |
| No namespace.
|
|
#define | GATT_NUM_ATTRS(attrs) ( sizeof( attrs ) / sizeof( gattAttribute_t ) ) |
| The number of attribute records in a given attribute table.
|
|
#define | GATT_PARAM_NUM_PREPARE_WRITES 0 |
| RW uint8.
|
|
#define | GATT_PROP_AUTHEN 0x40 |
| Permits signed writes to the Characteristic Value.
|
|
#define | GATT_PROP_BCAST 0x01 |
| Permits broadcasts of the Characteristic Value.
|
|
#define | GATT_PROP_EXTENDED 0x80 |
| Additional characteristic properties are defined in the Characteristic Extended Properties Descriptor.
|
|
#define | GATT_PROP_INDICATE 0x20 |
| Permits indications of a Characteristic Value with acknowledgement.
|
|
#define | GATT_PROP_NOTIFY 0x10 |
| Permits notifications of a Characteristic Value without acknowledgement.
|
|
#define | GATT_PROP_READ 0x02 |
| Permits reads of the Characteristic Value.
|
|
#define | GATT_PROP_WRITE 0x08 |
| Permits writes of the Characteristic Value with response.
|
|
#define | GATT_PROP_WRITE_NO_RSP 0x04 |
| Permits writes of the Characteristic Value without response.
|
|
#define | GATT_SERV_CFG_BCAST 0x0001 |
| The Characteristic Value shall be broadcast when the server is in the broadcast procedure if advertising data resources are available.
|
|
#define | GATT_SERVICE 0x00000001 |
| GATT Services bit fields.
|
|
#define | GATT_SERVICE_HANDLE(attrs) ( (attrs)[0].handle ) |
| The handle of a service is the handle of the first attribute.
|
|
#define | GATT_UUID(name, UUID) |
| GATT Custom UUID. More...
|
|
|
typedef bStatus_t(* | pfnGATTAuthorizeAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode) |
| Callback function prototype to authorize a Read or Write operation on a given attribute. More...
|
|
typedef bStatus_t(* | pfnGATTReadAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method) |
| Callback function prototype to read an attribute value. More...
|
|
typedef bStatus_t(* | pfnGATTWriteAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint8 method) |
| Callback function prototype to write an attribute value. More...
|
|
typedef struct _serviceCBsList | serviceCBsList_t |
| Service callbacks list item.
|
|
|
bStatus_t | GATTServApp_AddService (uint32 services) |
| Add function for the GATT Service. More...
|
|
bStatus_t | GATTServApp_DelService (uint32 services) |
| Delete function for the GATT Service. More...
|
|
bStatus_t | GATTServApp_DeregisterService (uint16 handle, gattAttribute_t **p2pAttrs) |
| Deregister a service's attribute list and callback functions from the GATT Server Application. More...
|
|
gattAttribute_t * | GATTServApp_FindAttr (gattAttribute_t *pAttrTbl, uint16 numAttrs, uint8 *pValue) |
| Find the attribute record within a service attribute table for a given attribute value pointer. More...
|
|
bStatus_t | GATTServApp_GetParameter (uint8 param, void *pValue) |
| Get a GATT Server parameter. More...
|
|
uint16 | GATTServApp_GetParamValue (void) |
| Get a GATT Server Application Parameter value. More...
|
|
void | GATTServApp_InitCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl) |
| Initialize the client characteristic configuration table. More...
|
|
bStatus_t | GATTServApp_ProcessCCCWriteReq (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint16 validCfg) |
| Process the client characteristic configuration write request for a given client. More...
|
|
bStatus_t | GATTServApp_ProcessCharCfg (gattCharCfg_t *charCfgTbl, uint8 *pValue, uint8 authenticated, gattAttribute_t *attrTbl, uint16 numAttrs, uint8 taskId, pfnGATTReadAttrCB_t pfnReadAttrCB) |
| Process Client Characteristic Configuration change. More...
|
|
uint8 | GATTServApp_ReadAttr (uint16 connHandle, gattAttribute_t *pAttr, uint16 service, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method) |
| Read an attribute. If the format of the attribute value is unknown to GATT Server, use the callback function provided by the Service. More...
|
|
uint16 | GATTServApp_ReadCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl) |
| Read the client characteristic configuration for a given client. More...
|
|
bStatus_t | GATTServApp_ReadRsp (uint16 connHandle, uint8 *pValue, uint16 pLen, uint16 offset) |
| If a service returns blePending to the read attribute call back invoked from GATTServApp, the service can later respond to with the value to be read using this API. More...
|
|
void | GATTServApp_RegisterForMsg (uint8 taskID) |
| Register your task ID to receive event messages from the GATT Server Application. More...
|
|
bStatus_t | GATTServApp_RegisterService (gattAttribute_t *pAttrs, uint16 numAttrs, uint8 encKeySize, CONST gattServiceCBs_t *pServiceCBs) |
| Register a service's attribute list and callback functions with the GATT Server Application. More...
|
|
void | GATTServApp_SendCCCUpdatedEvent (uint16 connHandle, uint16 attrHandle, uint16 value) |
| Build and send the GATT_CLIENT_CHAR_CFG_UPDATED_EVENT to the application. More...
|
|
bStatus_t | GATTServApp_SendServiceChangedInd (uint16 connHandle, uint8 taskId) |
| Send out a Service Changed Indication. More...
|
|
bStatus_t | GATTServApp_SetParameter (uint8 param, uint8 len, void *pValue) |
| Set a GATT Server parameter. More...
|
|
void | GATTServApp_SetParamValue (uint16 value) |
| Set a GATT Server Application Parameter value. Use this function to change the default GATT parameter values. More...
|
|
bStatus_t | GATTServApp_UpdateCharCfg (uint16 connHandle, uint16 attrHandle, uint16 value) |
| Update the Client Characteristic Configuration for a given Client. More...
|
|
uint8 | GATTServApp_WriteAttr (uint16 connHandle, uint16 handle, uint8 *pValue, uint16 len, uint16 offset, uint8 method) |
| Write attribute data. More...
|
|
uint8 | GATTServApp_WriteCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl, uint16 value) |
| Write the client characteristic configuration for a given client. More...
|
|