103 #ifndef ti_drivers_UDMACC26XX__include 104 #define ti_drivers_UDMACC26XX__include 112 #include <ti/devices/DeviceFamily.h> 113 #include DeviceFamily_constructPath(inc/hw_types.h) 114 #include DeviceFamily_constructPath(driverlib/udma.h) 149 #if !defined(UDMACC26XX_CONFIG_BASE) 150 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2) 155 #define UDMACC26XX_CONFIG_BASE 0x20001800 156 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X1_CC26X1) 162 #define UDMACC26XX_CONFIG_BASE 0x20000400 163 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 169 #if (SPE_ENABLED == 0) 170 #define UDMACC26XX_CONFIG_BASE 0x20000400 172 #define UDMACC26XX_CONFIG_BASE 0x2000C400 175 #define UDMACC26XX_CONFIG_BASE 0x20000400 180 #if (UDMACC26XX_CONFIG_BASE & 0x3FF) 181 #error "Base address for DMA control table 'UDMACC26XX_CONFIG_BASE' must be 1024 bytes aligned." 185 #if defined(__IAR_SYSTEMS_ICC__) 186 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \ 187 __no_init __root static volatile tDMAControlTable ENTRY_NAME @UDMACC26XX_CONFIG_BASE + \ 188 (CHANNEL_INDEX) * sizeof(tDMAControlTable) 189 #elif defined(__TI_COMPILER_VERSION__) || defined(__clang__) 190 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \ 191 static volatile tDMAControlTable ENTRY_NAME \ 192 __attribute__((retain, location((UDMACC26XX_CONFIG_BASE) + (CHANNEL_INDEX) * sizeof(tDMAControlTable)))) 193 #elif defined(__GNUC__) 194 #define ALLOCATE_CONTROL_TABLE_ENTRY(ENTRY_NAME, CHANNEL_INDEX) \ 195 extern int UDMACC26XX_##ENTRY_NAME##_is_placed; \ 196 __attribute__((section("." #ENTRY_NAME), used)) static volatile tDMAControlTable ENTRY_NAME = { \ 197 &UDMACC26XX_##ENTRY_NAME##_is_placed} 199 #error "don't know how to define ALLOCATE_CONTROL_TABLE_ENTRY for this toolchain" 203 #define UDMACC26XX_SET_TRANSFER_SIZE(SIZE) (((SIZE - 1) << UDMA_XFER_SIZE_S) & UDMA_XFER_SIZE_M) 205 #define UDMACC26XX_GET_TRANSFER_SIZE(CONTROL) (((CONTROL & UDMA_XFER_SIZE_M) >> UDMA_XFER_SIZE_S) + 1) 327 HWREG(hwAttrs->
baseAddr + UDMA_O_SETCHANNELEN) = channelBitMask;
356 return (uDMAIntStatus(hwAttrs->
baseAddr) & channelBitMask) ?
true :
false;
384 uDMAIntClear(hwAttrs->
baseAddr, channelBitMask);
411 HWREG(hwAttrs->
baseAddr + UDMA_O_CLEARCHANNELEN) = channelBitMask;
441 uDMAChannelAttributeDisable(hwAttrs->
baseAddr, channelNum, attr);
bool isOpen
Definition: UDMACC26XX.h:212
HwiP_Struct hwi
Definition: UDMACC26XX.h:213
void UDMACC26XX_hwiIntFxn(uintptr_t callbacks)
PowerCC26XX_Resource powerMngrId
Definition: UDMACC26XX.h:222
void UDMACC26XX_close(UDMACC26XX_Handle handle)
Function to close the DMA driver.
UDMACC26XX_Handle UDMACC26XX_open(void)
Function to initialize the CC26XX DMA peripheral.
__STATIC_INLINE void UDMACC26XX_clearInterrupt(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:376
__STATIC_INLINE void UDMACC26XX_channelEnable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:319
uint8_t intNum
Definition: UDMACC26XX.h:223
__STATIC_INLINE void UDMACC26XX_init(UDMACC26XX_Handle handle)
Function to initialize the CC26XX DMA driver.
Definition: UDMACC26XX.h:278
__STATIC_INLINE void UDMACC26XX_disableAttribute(UDMACC26XX_Handle handle, uint32_t channelNum, uint32_t attr)
Definition: UDMACC26XX.h:434
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:252
Power manager interface for CC26XX/CC13XX.
UDMACC26XX hardware attributes.
Definition: UDMACC26XX.h:219
void * object
Definition: UDMACC26XX.h:254
uint8_t intPriority
UDMACC26XX error interrupt priority. intPriority is the DMA peripheral's interrupt priority...
Definition: UDMACC26XX.h:246
__STATIC_INLINE void UDMACC26XX_channelDisable(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:404
__STATIC_INLINE bool UDMACC26XX_channelDone(UDMACC26XX_Handle handle, uint32_t channelBitMask)
Definition: UDMACC26XX.h:348
uint32_t baseAddr
Definition: UDMACC26XX.h:221
UDMACC26XX object.
Definition: UDMACC26XX.h:210
UDMACC26XX_Config * UDMACC26XX_Handle
A handle that is returned from a UDMACC26XX_open() call.
Definition: UDMACC26XX.h:261
void const * hwAttrs
Definition: UDMACC26XX.h:255