TRNGCC26X4_ns.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2022, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!****************************************************************************
33  * @file TRNGCC26X4_ns.h
34  *
35  * @brief TRNG Nonsecure driver implementation for the CC26X4 family
36  *
37  */
38 
39 #ifndef ti_drivers_TRNG_TRNGCC26X4_ns__include
40 #define ti_drivers_TRNG_TRNGCC26X4_ns__include
41 
42 #include <stdint.h>
43 
44 #include <ti/drivers/TRNG.h>
46 
47 #ifdef __cplusplus
48 extern "C" {
49 #endif
50 
58 typedef struct
59 {
60  TRNG_CryptoKeyCallbackFxn cryptoKeyCallbackFxn;
61  TRNG_RandomBytesCallbackFxn randomBytesCallbackFxn;
62  TRNG_ReturnBehavior returnBehavior;
63  SemaphoreP_Struct operationSemaphore;
64 } TRNGCC26X4_ns_Object;
65 
71 typedef struct
72 {
73  TRNG_s_CryptoKeySecureCallback cryptoKeyCallback;
74  TRNG_s_RandomBytesSecureCallback randomBytesCallback;
75 } TRNG_ns_SecureCB;
76 
90 extern int_fast16_t TRNGCC26XX_setSamplesPerCycle(TRNG_Handle handle, uint32_t samplesPerCycle);
91 
94 #ifdef __cplusplus
95 }
96 #endif
97 
98 #endif /* ti_drivers_TRNG_TRNGCC26X4_ns__include */
Definition: TRNGCC26X4_s.h:82
TRNG Global configuration.
Definition: TRNG.h:328
Definition: TRNGCC26X4_s.h:91
void(* TRNG_CryptoKeyCallbackFxn)(TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy)
The definition of a callback function used by the TRNG driver when TRNG_generateKey() is called with ...
Definition: TRNG.h:394
TRNG_ReturnBehavior
The way in which TRNG function calls return after generating the requested entropy.
Definition: TRNG.h:363
int_fast16_t TRNGCC26XX_setSamplesPerCycle(TRNG_Handle handle, uint32_t samplesPerCycle)
Sets the number of entropy generation cycles before the results are returned.
TRNG driver header.
void(* TRNG_RandomBytesCallbackFxn)(TRNG_Handle handle, int_fast16_t returnValue, uint8_t *randomBytes, size_t randomBytesSize)
The definition of a callback function used by the TRNG driver when TRNG_getRandomBytes() is called wi...
Definition: TRNG.h:409
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale