348 #ifndef ti_drivers_pdm_PDMCC26XX__include 349 #define ti_drivers_pdm_PDMCC26XX__include 351 #include <ti/drivers/dpl/HwiP.h> 352 #include <ti/drivers/dpl/SemaphoreP.h> 372 #ifndef PDM_TASK_STACK_SIZE 373 #define PDM_TASK_STACK_SIZE 850 377 #define PCM_SAMPLE_SIZE 16 // Only 16 bits supported for now 380 #define PCM_COMPRESSION_RATE 4 383 #define MINIMUM_PDM_BUFFER_QUEUE_DEPTH 3 389 #define PCM_METADATA_SIZE sizeof(PDMCC26XX_metaData) 415 typedef void *(*PDMCC26XX_MallocFxn)(
size_t memSize);
437 uint32_t *decimationState,
438 const int32_t *biquadCoefficients,
439 int16_t *pcmOutBuffer);
void PDMCC26XX_close(PDMCC26XX_Handle handle)
Function to close a given CC26XX PDM peripheral specified by the PDM handle.
size_t decimationFilterStateSize
Definition: PDMCC26XX.h:595
PDMCC26XX_Gain
Predefined gain settings.
Definition: PDMCC26XX.h:518
ADC_Params params
Definition: Driver_Init.h:11
PDMCC26XX_pcmBuffer * buffer
Definition: PDMCC26XX.h:563
const int32_t * decimationFilter
Definition: PDMCC26XX.h:593
PDMCC26XX_Handle PDMCC26XX_open(PDMCC26XX_Params *params)
Function to initialize the CC26XX PDM peripheral specified by the particular handle. The parameter specifies which mode the PDM will operate.
size_t decimationFilterStateSize
Definition: PDMCC26XX.h:639
bool PDMCC26XX_startStream(PDMCC26XX_Handle handle)
Function to start streaming PDM data.
A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors.
Definition: PDMCC26XX.h:533
void * arg
Definition: PDMCC26XX.h:535
void *(* PDMCC26XX_MallocFxn)(size_t memSize)
PDMCC26XX_MallocFxn is a function pointer for the malloc function to be used by the driver...
Definition: PDMCC26XX.h:415
Definition: PDMCC26XX.h:491
bool applyCompression
Definition: PDMCC26XX.h:625
Power manager interface for CC26XX/CC13XX.
PDMCC26XX_MallocFxn mallocFxn
Definition: PDMCC26XX.h:645
bool PDMCC26XX_stopStream(PDMCC26XX_Handle handle)
Function to stop streaming PDM data.
int taskPriority
Definition: PDMCC26XX.h:469
HwiP_Struct hwi
Definition: PDMCC26XX.h:648
const PDMCC26XX_Config PDMCC26XX_config[]
PDMCC26XX_PcmSampleRate pcmSampleRate
Definition: PDMCC26XX.h:604
PDMCC26XX_CallbackFxn callbackFxn
Definition: PDMCC26XX.h:644
PCM buffer pointed to in a PDMCC26XX_BufferRequest.
Definition: PDMCC26XX.h:404
uint8_t pdmBufferQueueDepth
Definition: PDMCC26XX.h:583
Definition: PDMCC26XX.h:483
bool PDMCC26XX_requestBuffer(PDMCC26XX_Handle handle, PDMCC26XX_BufferRequest *bufferRequest)
Function for requesting buffer.
Definition: PDMCC26XX.h:523
void PDMCC26XX_init(PDMCC26XX_Handle handle)
PDM CC26XX initialization.
Definition: PDMCC26XX.h:489
PDMCC26XX_metaData metaData
Definition: PDMCC26XX.h:406
PDMCC26XX_StreamNotification * streamNotification
Definition: PDMCC26XX.h:643
void const * hwAttrs
Definition: PDMCC26XX.h:452
Definition: PDMCC26XX.h:504
PDMCC26XX_Pdm2PcmFxn pdm2pcmFxn
Definition: PDMCC26XX.h:647
bool micPowerActiveHigh
Definition: PDMCC26XX.h:624
Definition: PDMCC26XX.h:525
uint16_t pcmBufferSizeInBytes
Definition: PDMCC26XX.h:630
uint32_t micPower
Definition: PDMCC26XX.h:467
bool micPowerActiveHigh
Definition: PDMCC26XX.h:579
A PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer().
Definition: PDMCC26XX.h:561
Definition: PDMCC26XX.h:484
PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters ...
Definition: PDMCC26XX.h:576
uint16_t retBufSizeInBytes
Definition: PDMCC26XX.h:590
uint32_t startupDelayWithClockInSamples
Definition: PDMCC26XX.h:632
Definition: PDMCC26XX.h:522
Definition: PDMCC26XX.h:521
uint32_t startupDelayWithClockInSamples
Definition: PDMCC26XX.h:605
The PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver i...
Definition: PDMCC26XX.h:446
uint16_t retBufSizeInBytes
Definition: PDMCC26XX.h:629
Definition: PDMCC26XX.h:520
Definition: PDMCC26XX.h:492
void * object
Definition: PDMCC26XX.h:449
bool streamStarted
Definition: PDMCC26XX.h:623
void(* PDMCC26XX_CallbackFxn)(PDMCC26XX_Handle handle, PDMCC26XX_StreamNotification *streamNotification)
The definition of a callback function used when buffers are ready.
Definition: PDMCC26XX.h:544
Definition: PDMCC26XX.h:482
PDMCC26XX_Status status
Definition: PDMCC26XX.h:566
PDMCC26XX_MallocFxn mallocFxn
Definition: PDMCC26XX.h:610
PDMCC26XX_Gain defaultFilterGain
Definition: PDMCC26XX.h:602
const int32_t * decimationFilter
Definition: PDMCC26XX.h:636
uint32_t * decimationFilterState
Definition: PDMCC26XX.h:638
PDMCC26XX_Status status
Definition: PDMCC26XX.h:536
bool(* PDMCC26XX_Pdm2PcmFxn)(const void *pdmInBuffer, uint32_t *decimationState, const int32_t *biquadCoefficients, int16_t *pcmOutBuffer)
Function that converts PDM input buffer to PCM output.
Definition: PDMCC26XX.h:436
Definition: PDMCC26XX.h:503
bool isOpen
Definition: PDMCC26XX.h:628
PDMCC26XX_FreeFxn freeFxn
Definition: PDMCC26XX.h:611
PDMCC26XX_PcmSampleRate
PCM output sample rates supported by the driver.
Definition: PDMCC26XX.h:501
PDMCC26XX Object.
Definition: PDMCC26XX.h:620
PDMCC26XX_Status
Status codes that are set by the PDM driver.
Definition: PDMCC26XX.h:480
Definition: PDMCC26XX.h:524
PDMCC26XX_Config * PDMCC26XX_Handle
A handle that is returned from a PDMCC26XX_open() call.
Definition: PDMCC26XX.h:475
bool applyCompression
Definition: PDMCC26XX.h:580
PDMCC26XX_FreeFxn freeFxn
Definition: PDMCC26XX.h:646
uintptr_t custom
Definition: PDMCC26XX.h:612
void PDMCC26XX_Params_init(PDMCC26XX_Params *params)
void(* PDMCC26XX_FreeFxn)(void *ptr, size_t memSize)
PDMCC26XX_FreeFxn is a function pointer for the free function to be used by the driver. This is needed for memory clean up, if something goes wrong.
Definition: PDMCC26XX.h:423
PDMCC26XX Hardware attributes.
Definition: PDMCC26XX.h:464
Definition: PDMCC26XX.h:486
PDMCC26XX_CallbackFxn callbackFxn
Definition: PDMCC26XX.h:609