#include "../inc/hw_types.h"
#include "../inc/hw_ccfg.h"
#include "../inc/hw_ioc.h"
#include "aon_batmon.h"
#include "flash.h"
#include "gpio.h"
#include "setup_rom.h"
#include "sys_ctrl.h"
Functions | |
void | SysCtrlIdle (uint32_t vimsPdMode) |
Force the system into idle mode. More... | |
void | SysCtrlShutdownWithAbort (void) |
Try to enter shutdown but abort if wakeup event happened before shutdown. More... | |
void | SysCtrlShutdown (void) |
Enable shutdown of the device. More... | |
void | SysCtrlStandby (bool retainCache, uint32_t vimsPdMode, uint32_t rechargeMode) |
Force the system into standby mode. More... | |
void | SysCtrlSetRechargeBeforePowerDown (uint32_t xoscPowerMode) |
Set Recharge values before entering Power Down. More... | |
void | SysCtrlAdjustRechargeAfterPowerDown (uint32_t vddrRechargeMargin) |
Adjust Recharge calculations to be used next. More... | |
void | SysCtrl_DCDC_VoltageConditionalControl (void) |
Turns DCDC on or off depending of what is considered to be optimal usage. More... | |
uint32_t | SysCtrlResetSourceGet (void) |
Returns the reset source (including "wakeup from shutdown"). More... | |