TI BLE5-Stack API Documentation
2.02.07.00
.build.ble5.cc13xx_cc26xx
api-sources
ble-core
source
ti
ble5stack
osal
src
inc
comdef.h
Go to the documentation of this file.
1
/******************************************************************************
2
3
Group: WCS, LPC, BTS
4
$Target Device: DEVICES $
5
6
******************************************************************************
7
$License: BSD3 2004 $
8
******************************************************************************
9
$Release Name: PACKAGE NAME $
10
$Release Date: PACKAGE RELEASE DATE $
11
*****************************************************************************/
12
18
#ifndef COMDEF_H
19
#define COMDEF_H
20
21
#ifdef __cplusplus
22
extern
"C"
23
{
24
#endif
25
26
27
/*********************************************************************
28
* INCLUDES
29
*/
30
31
/* HAL */
32
#include "hal_types.h"
33
#include "hal_defs.h"
34
36
37
/*********************************************************************
38
* Lint Keywords
39
*/
40
#define VOID (void)
41
42
#define NULL_OK
43
#define INP
44
#define OUTP
45
#define ONLY
46
#define READONLY
47
#define SHARED
48
#define KEEP
49
#define RELAX
50
#ifndef UNUSED
51
#define UNUSED
52
#endif
53
54
/*********************************************************************
55
* CONSTANTS
56
*/
57
58
#ifndef false
59
#define false 0
60
#endif
61
62
#ifndef true
63
#define true 1
64
#endif
65
66
#ifndef CONST
67
#define CONST const
68
#endif
69
70
#ifndef GENERIC
71
#define GENERIC
72
#endif
73
75
76
/*** Generic Status Return Values ***/
77
#define SUCCESS 0x00
78
#define FAILURE 0x01
79
#define INVALIDPARAMETER 0x02
80
#define INVALID_TASK 0x03
81
#define MSG_BUFFER_NOT_AVAIL 0x04
82
#define INVALID_MSG_POINTER 0x05
83
#define INVALID_EVENT_ID 0x06
84
#define INVALID_INTERRUPT_ID 0x07
85
#define NO_TIMER_AVAIL 0x08
86
#define NV_ITEM_UNINIT 0x09
87
#define NV_OPER_FAILED 0x0A
88
#define INVALID_MEM_SIZE 0x0B
89
#define NV_BAD_ITEM_LEN 0x0C
90
91
/*********************************************************************
92
* TYPEDEFS
93
*/
94
96
97
// Generic Status return
98
typedef
uint8 Status_t;
99
100
// Data types
101
typedef
int32 int24;
102
typedef
uint32 uint24;
103
105
106
/*********************************************************************
107
* Global System Events
108
*/
109
110
#define SYS_EVENT_MSG 0x8000
111
112
/*********************************************************************
113
* Global Generic System Messages
114
*/
115
116
#define KEY_CHANGE 0xC0
117
118
// OSAL System Message IDs/Events Reserved for applications (user applications)
119
// 0xE0 - 0xFC
120
121
/*********************************************************************
122
* MACROS
123
*/
124
125
/*********************************************************************
126
* GLOBAL VARIABLES
127
*/
128
129
/*********************************************************************
130
* FUNCTIONS
131
*/
132
133
/*********************************************************************
134
*********************************************************************/
135
136
#ifdef __cplusplus
137
}
138
#endif
139
140
#endif
/* COMDEF_H */
© Copyright 1995-2023
, Texas Instruments Incorporated. All rights reserved.
Trademarks
|
Privacy policy
|
Terms of use
|
Terms of sale