CRYPTO

Instance: CRYPTO
Component: CRYPTO
Base address: 0x40024000


Crypto core with DMA capability and local key storage

TOP:CRYPTO Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

DMACH0CTL

RW

32

0x0000 0000

0x0000 0000

0x4002 4000

DMACH0EXTADDR

RW

32

0x0000 0000

0x0000 0004

0x4002 4004

DMACH0LEN

RW

32

0x0000 0000

0x0000 000C

0x4002 400C

DMASTAT

RO

32

0x0000 0000

0x0000 0018

0x4002 4018

DMASWRESET

WO

32

0x0000 0000

0x0000 001C

0x4002 401C

DMACH1CTL

RW

32

0x0000 0000

0x0000 0020

0x4002 4020

DMACH1EXTADDR

RW

32

0x0000 0000

0x0000 0024

0x4002 4024

DMACH1LEN

RW

32

0x0000 0000

0x0000 002C

0x4002 402C

DMABUSCFG

RW

32

0x0000 2400

0x0000 0078

0x4002 4078

DMAPORTERR

RO

32

0x0000 0000

0x0000 007C

0x4002 407C

DMAHWVER

RO

32

0x0101 2ED1

0x0000 00FC

0x4002 40FC

KEYWRITEAREA

RW

32

0x0000 0000

0x0000 0400

0x4002 4400

KEYWRITTENAREA

RW

32

0x0000 0000

0x0000 0404

0x4002 4404

KEYSIZE

RW

32

0x0000 0001

0x0000 0408

0x4002 4408

KEYREADAREA

RW

32

0x0000 0008

0x0000 040C

0x4002 440C

AESKEY2__0-AESKEY2__3

WO

32

0x0000 0000

0x0000 0500 - 0x0000 050C

0x4002 4500 - 0x4002 450C

AESKEY3__0-AESKEY3__3

WO

32

0x0000 0000

0x0000 0510 - 0x0000 051C

0x4002 4510 - 0x4002 451C

AESIV__0-AESIV__3

RW

32

0x0000 0000

0x0000 0540 - 0x0000 054C

0x4002 4540 - 0x4002 454C

AESCTL

RW

32

0x8000 0000

0x0000 0550

0x4002 4550

AESDATALEN0

WO

32

0x0000 0000

0x0000 0554

0x4002 4554

AESDATALEN1

WO

32

0x0000 0000

0x0000 0558

0x4002 4558

AESAUTHLEN

WO

32

0x0000 0000

0x0000 055C

0x4002 455C

AESDATAOUT0

RO

32

0x0000 0000

0x0000 0560

0x4002 4560

AESDATAIN0

WO

32

0x0000 0000

0x0000 0560

0x4002 4560

AESDATAOUT1

RO

32

0x0000 0000

0x0000 0564

0x4002 4564

AESDATAIN1

WO

32

0x0000 0000

0x0000 0564

0x4002 4564

AESDATAOUT2

RO

32

0x0000 0000

0x0000 0568

0x4002 4568

AESDATAIN2

WO

32

0x0000 0000

0x0000 0568

0x4002 4568

AESDATAOUT3

RO

32

0x0000 0000

0x0000 056C

0x4002 456C

AESDATAIN3

WO

32

0x0000 0000

0x0000 056C

0x4002 456C

AESTAGOUT__0-AESTAGOUT__3

RO

32

0x0000 0000

0x0000 0570 - 0x0000 057C

0x4002 4570 - 0x4002 457C

ALGSEL

RW

32

0x0000 0000

0x0000 0700

0x4002 4700

DMAPROTCTL

RW

32

0x0000 0000

0x0000 0704

0x4002 4704

SWRESET

RW

32

0x0000 0000

0x0000 0740

0x4002 4740

IRQTYPE

RW

32

0x0000 0000

0x0000 0780

0x4002 4780

IRQEN

RW

32

0x0000 0000

0x0000 0784

0x4002 4784

IRQCLR

WO

32

0x0000 0000

0x0000 0788

0x4002 4788

IRQSET

WO

32

0x0000 0000

0x0000 078C

0x4002 478C

IRQSTAT

RO

32

0x0000 0000

0x0000 0790

0x4002 4790

HWVER

RO

32

0x9111 8778

0x0000 07FC

0x4002 47FC

TOP:CRYPTO Register Descriptions

TOP:CRYPTO:DMACH0CTL

Address Offset 0x0000 0000
Physical Address 0x4002 4000 Instance 0x4002 4000
Description DMA Channel 0 Control
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 0000 0000 0000
1 PRIO Channel priority:

A channel with high priority will be served before a channel with low priority in cases with simultaneous access requests. If both channels have the same priority access of the channels to the external port is arbitrated using a Round Robin scheme.
Value ENUM Name Description
0x0 LOW Priority low
0x1 HIGH Priority high
RW 0
0 EN DMA Channel 0 Control
Value ENUM Name Description
0x0 DIS Channel disabled
0x1 EN Channel enabled
RW 0

TOP:CRYPTO:DMACH0EXTADDR

Address Offset 0x0000 0004
Physical Address 0x4002 4004 Instance 0x4002 4004
Description DMA Channel 0 External Address
Type RW
Bits Field Name Description Type Reset
31:0 ADDR Channel external address value.
Holds the last updated external address after being sent to the master interface.
RW 0x0000 0000

TOP:CRYPTO:DMACH0LEN

Address Offset 0x0000 000C
Physical Address 0x4002 400C Instance 0x4002 400C
Description DMA Channel 0 Length
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x0000
15:0 LEN DMA transfer length in bytes.
During configuration, this register contains the DMA transfer length in bytes. During operation, it contains the last updated value of the DMA transfer length after being sent to the master interface.
Note: Writing a non-zero value to this register field starts the transfer if the channel is enabled by setting DMACH0CTL.EN.
RW 0x0000

TOP:CRYPTO:DMASTAT

Address Offset 0x0000 0018
Physical Address 0x4002 4018 Instance 0x4002 4018
Description DMA Controller Status
Type RO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 PORT_ERR Reflects possible transfer errors on the AHB port. RO 0
16:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000
1 CH1_ACTIVE This register field indicates if DMA channel 1 is active or not.
0: Not active
1: Active
RO 0
0 CH0_ACTIVE This register field indicates if DMA channel 0 is active or not.
0: Not active
1: Active
RO 0

TOP:CRYPTO:DMASWRESET

Address Offset 0x0000 001C
Physical Address 0x4002 401C Instance 0x4002 401C
Description DMA Controller Software Reset
Type WO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b000 0000 0000 0000 0000 0000 0000 0000
0 RESET Software reset enable

0: Disable
1: Enable (self-cleared to zero).

Note: Completion of the software reset must be checked in DMASTAT.CH0_ACTIVE and DMASTAT.CH1_ACTIVE.
WO 0

TOP:CRYPTO:DMACH1CTL

Address Offset 0x0000 0020
Physical Address 0x4002 4020 Instance 0x4002 4020
Description DMA Channel 1 Control
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 0000 0000 0000
1 PRIO Channel priority:

A channel with high priority will be served before a channel with low priority in cases with simultaneous access requests. If both channels have the same priority access of the channels to the external port is arbitrated using a Round Robin scheme.
Value ENUM Name Description
0x0 LOW Priority low
0x1 HIGH Priority high
RW 0
0 EN Channel enable:

Note: Disabling an active channel will interrupt the DMA operation. The ongoing block transfer will be completed, but no new transfers will be requested.
Value ENUM Name Description
0x0 DIS Channel disabled
0x1 EN Channel enabled
RW 0

TOP:CRYPTO:DMACH1EXTADDR

Address Offset 0x0000 0024
Physical Address 0x4002 4024 Instance 0x4002 4024
Description DMA Channel 1 External Address
Type RW
Bits Field Name Description Type Reset
31:0 ADDR Channel external address value.
Holds the last updated external address after being sent to the master interface.
RW 0x0000 0000

TOP:CRYPTO:DMACH1LEN

Address Offset 0x0000 002C
Physical Address 0x4002 402C Instance 0x4002 402C
Description DMA Channel 1 Length
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x0000
15:0 LEN DMA transfer length in bytes.
During configuration, this register contains the DMA transfer length in bytes. During operation, it contains the last updated value of the DMA transfer length after being sent to the master interface.
Note: Writing a non-zero value to this register field starts the transfer if the channel is enabled by setting DMACH1CTL.EN.
RW 0x0000

TOP:CRYPTO:DMABUSCFG

Address Offset 0x0000 0078
Physical Address 0x4002 4078 Instance 0x4002 4078
Description DMA Controller Master Configuration
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x0000
15:12 AHB_MST1_BURST_SIZE Maximum burst size that can be performed on the AHB bus
Value ENUM Name Description
0x2 4_BYTE 4 bytes
0x3 8_BYTE 8 bytes
0x4 16_BYTE 16 bytes
0x5 32_BYTE 32 bytes
0x6 64_BYTE 64 bytes
RW 0x2
11 AHB_MST1_IDLE_EN Idle transfer insertion between consecutive burst transfers on AHB
Value ENUM Name Description
0x0 NO_IDLE Do not insert idle transfers.
0x1 IDLE Idle transfer insertion enabled
RW 0
10 AHB_MST1_INCR_EN Burst length type of AHB transfer
Value ENUM Name Description
0x0 UNSPECIFIED Unspecified length burst transfers
0x1 SPECIFIED Fixed length bursts or single transfers
RW 1
9 AHB_MST1_LOCK_EN Locked transform on AHB
Value ENUM Name Description
0x0 NOT_LOCKED Transfers are not locked
0x1 LOCKED Transfers are locked
RW 0
8 AHB_MST1_BIGEND Endianess for the AHB master
Value ENUM Name Description
0x0 LITTLE_ENDIAN Little Endian
0x1 BIG_ENDIAN Big Endian
RW 0
7:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x00

TOP:CRYPTO:DMAPORTERR

Address Offset 0x0000 007C
Physical Address 0x4002 407C Instance 0x4002 407C
Description DMA Controller Port Error
Type RO
Bits Field Name Description Type Reset
31:13 RESERVED13 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000
12 AHB_ERR A 1 indicates that the Crypto peripheral has detected an AHB bus error RO 0
11:10 RESERVED10 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
9 LAST_CH Indicates which channel was serviced last (channel 0 or channel 1) by the AHB master port. RO 0
8:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000

TOP:CRYPTO:DMAHWVER

Address Offset 0x0000 00FC
Physical Address 0x4002 40FC Instance 0x4002 40FC
Description DMA Controller Version
Type RO
Bits Field Name Description Type Reset
31:28 RESERVED28 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
27:24 HW_MAJOR_VER Major version number RO 0x1
23:20 HW_MINOR_VER Minor version number RO 0x0
19:16 HW_PATCH_LVL Patch level. RO 0x1
15:8 VER_NUM_COMPL Bit-by-bit complement of the VER_NUM field bits. RO 0x2E
7:0 VER_NUM Version number of the DMA Controller (209) RO 0xD1

TOP:CRYPTO:KEYWRITEAREA

Address Offset 0x0000 0400
Physical Address 0x4002 4400 Instance 0x4002 4400
Description Key Write Area
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x00 0000
7 RAM_AREA7 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
6 RAM_AREA6 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
5 RAM_AREA5 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
4 RAM_AREA4 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
3 RAM_AREA3 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
2 RAM_AREA2 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
1 RAM_AREA1 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0
0 RAM_AREA0 Represents an area of 128 bits.
Select the key store RAM area(s) where the key(s) needs to be written.

Writing to multiple RAM locations is only possible when the selected RAM areas are sequential.
Value ENUM Name Description
0x0 NOT_SEL This RAM area is not selected to be written
0x1 SEL This RAM area is selected to be written
RW 0

TOP:CRYPTO:KEYWRITTENAREA

Address Offset 0x0000 0404
Physical Address 0x4002 4404 Instance 0x4002 4404
Description Key Written Area Status
This register shows which areas of the key store RAM contain valid written keys.
When a new key needs to be written to the key store, on a location that is already occupied by a valid key, this key area must be cleared first. This can be done by writing this register before the new key is written to the key store memory.
Attempting to write to a key area that already contains a valid key is not allowed and will result in an error.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x00 0000
7 RAM_AREA_WRITTEN7 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
6 RAM_AREA_WRITTEN6 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
5 RAM_AREA_WRITTEN5 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
4 RAM_AREA_WRITTEN4 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
3 RAM_AREA_WRITTEN3 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
2 RAM_AREA_WRITTEN2 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
1 RAM_AREA_WRITTEN1 On read this bit returns the key area written status.

This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0
0 RAM_AREA_WRITTEN0 On read this bit returns the key area written status.


This bit can be reset by writing a 1.

Note: This register will be reset on a soft reset initiated by writing to DMASWRESET.RESET. After a soft reset, all keys must be rewritten to the key store memory.
Value ENUM Name Description
0x0 NOT_WRITTEN This RAM area is not written with valid key information
0x1 WRITTEN This RAM area is written with valid key information
RW 0

TOP:CRYPTO:KEYSIZE

Address Offset 0x0000 0408
Physical Address 0x4002 4408 Instance 0x4002 4408
Description Key Size
This register defines the size of the keys that are written with DMA.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 0000 0000 0000
1:0 SIZE Key size

When writing to this register, KEYWRITTENAREA will be reset.

Note: For the Crypto peripheral this field is fixed to 128 bits. For software compatibility KEYWRITTENAREA will be reset when writing to this register.
Value ENUM Name Description
0x1 128_BIT 128 bits
RW 0b01

TOP:CRYPTO:KEYREADAREA

Address Offset 0x0000 040C
Physical Address 0x4002 440C Instance 0x4002 440C
Description Key Read Area
Type RW
Bits Field Name Description Type Reset
31 BUSY Key store operation busy status flag (read only)

0: operation is completed.
1: operation is not completed and the key store is busy.
RO 0
30:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b000 0000 0000 0000 0000 0000 0000
3:0 RAM_AREA Selects the area of the key store RAM from where the key needs to be read that will be written to the AES engine.

Only RAM areas that contain valid written keys can be selected.
Value ENUM Name Description
0x0 RAM_AREA0 RAM Area 0
0x1 RAM_AREA1 RAM Area 1
0x2 RAM_AREA2 RAM Area 2
0x3 RAM_AREA3 RAM Area 3
0x4 RAM_AREA4 RAM Area 4
0x5 RAM_AREA5 RAM Area 5
0x6 RAM_AREA6 RAM Area 6
0x7 RAM_AREA7 RAM Area 7
0x8 NO_RAM No RAM
RW 0x8

TOP:CRYPTO:AESKEY2__0-AESKEY2__3

Address Offset 0x0000 0500 - 0x0000 050C
Physical Address 0x4002 4500 - 0x4002 450C Instance 0x4002 4500 - 0x4002 450C
Description Clear AES_KEY2/GHASH Key
Type WO
Bits Field Name Description Type Reset
31:0 KEY2 AESKEY2.* bits 31+x:0+x or AES_GHASH_H.* bits 31+x:0+x, where x = 0, 32, 64, 96 ordered from the LSW entry of this 4-deep register array.
The interpretation of this field depends on the crypto operation mode.
WO 0x0000 0000

TOP:CRYPTO:AESKEY3__0-AESKEY3__3

Address Offset 0x0000 0510 - 0x0000 051C
Physical Address 0x4002 4510 - 0x4002 451C Instance 0x4002 4510 - 0x4002 451C
Description Clear AES_KEY3
Type WO
Bits Field Name Description Type Reset
31:0 KEY3 AESKEY3.* bits 31+x:0+x or AESKEY2.* bits 159+x:128+x, where x = 0, 32, 64, 96 ordered from the LSW entry of this 4-deep register arrary.
The interpretation of this field depends on the crypto operation mode.
WO 0x0000 0000

TOP:CRYPTO:AESIV__0-AESIV__3

Address Offset 0x0000 0540 - 0x0000 054C
Physical Address 0x4002 4540 - 0x4002 454C Instance 0x4002 4540 - 0x4002 454C
Description AES Initialization Vector
Type RW
Bits Field Name Description Type Reset
31:0 IV The interpretation of this field depends on the crypto operation mode. RW 0x0000 0000

TOP:CRYPTO:AESCTL

Address Offset 0x0000 0550
Physical Address 0x4002 4550 Instance 0x4002 4550
Description AES Input/Output Buffer Control
Type RW
Bits Field Name Description Type Reset
31 CONTEXT_RDY If 1, this status bit indicates that the context data registers can be overwritten and the Host is permitted to write the next context. Writing a context means writing either a mode, the crypto length or AESDATALEN1.LEN_MSW, AESDATALEN0.LEN_LSW length registers RO 1
30 SAVED_CONTEXT_RDY If read as 1, this status bit indicates that an AES authentication TAG and/or IV block(s) is/are available for the Host to retrieve. This bit is only asserted if SAVE_CONTEXT is set to 1. The bit is mutually exclusive with CONTEXT_RDY.

Writing 1 clears the bit to zero, indicating the Crypto peripheral can start its next operation. This bit is also cleared when the 4th word of the output TAG and/or IV is read.

Note: All other mode bit writes will be ignored when this mode bit is written with 1.

Note: This bit is controlled automatically by the Crypto peripheral for TAG read DMA operations.

For typical use, this bit does NOT need to be written, but is used for status reading only. In this case, this status bit is automatically maintained by the Crypto peripheral.
RW 0
29 SAVE_CONTEXT IV must be read before the AES engine can start a new operation. RW 0
28:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x0
24:22 CCM_M Defines M that indicates the length of the authentication field for CCM operations; the authentication field length equals two times the value of CCM_M plus one.
Note: The Crypto peripheral always returns a 128-bit authentication field, of which the M least significant bytes are valid. All values are supported.
RW 0b000
21:19 CCM_L Defines L that indicates the width of the length field for CCM operations; the length field in bytes equals the value of CMM_L plus one. All values are supported. RW 0b000
18 CCM AES-CCM mode enable.
AES-CCM is a combined mode, using AES for both authentication and encryption.
Note: Selecting AES-CCM mode requires writing of AESDATALEN1.LEN_MSW and AESDATALEN0.LEN_LSW after all other registers.
Note: The CTR mode bit in this register must also be set to 1 to enable AES-CTR; selecting other AES modes than CTR mode is invalid.
RW 0
17:16 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00
15 CBC_MAC MAC mode enable.
The DIR bit must be set to 1 for this mode.
Selecting this mode requires writing the AESDATALEN1.LEN_MSW and AESDATALEN0.LEN_LSW registers after all other registers.
RW 0
14:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000
8:7 CTR_WIDTH Specifies the counter width for AES-CTR mode
Value ENUM Name Description
0x0 32_BIT 32 bits
0x1 64_BIT 64 bits
0x2 96_BIT 96 bits
0x3 128_BIT 128 bits
RW 0b00
6 CTR AES-CTR mode enable
This bit must also be set for CCM, when encryption/decryption is required.
RW 0
5 CBC CBC mode enable RW 0
4:3 KEY_SIZE This field specifies the key size.
The key size is automatically configured when a new key is loaded via the key store module.
00 = N/A - reserved
01 = 128 bits
10 = N/A - reserved
11 = N/A - reserved
For the Crypto peripheral this field is fixed to 128 bits.
RO 0b00
2 DIR Direction.
0 : Decrypt operation is performed.
1 : Encrypt operation is performed.

This bit must be written with a 1 when CBC-MAC is selected.
RW 0
1 INPUT_RDY If read as 1, this status bit indicates that the 16-byte AES input buffer is empty. The Host is permitted to write the next block of data.

Writing a 0 clears the bit to zero and indicates that the AES engine can use the provided input data block.

Writing a 1 to this bit will be ignored.

Note: For DMA operations, this bit is automatically controlled by the Crypto peripheral.
After reset, this bit is 0. After writing a context (note 1), this bit will become 1.

For typical use, this bit does NOT need to be written, but is used for status reading only. In this case, this status bit is automatically maintained by the Crypto peripheral.
RW 0
0 OUTPUT_RDY If read as 1, this status bit indicates that an AES output block is available to be retrieved by the Host.

Writing a 0 clears the bit to zero and indicates that output data is read by the Host. The AES engine can provide a next output data block.

Writing a 1 to this bit will be ignored.

Note: For DMA operations, this bit is automatically controlled by the Crypto peripheral.

For typical use, this bit does NOT need to be written, but is used for status reading only. In this case, this status bit is automatically maintained by the Crypto peripheral.
RW 0

TOP:CRYPTO:AESDATALEN0

Address Offset 0x0000 0554
Physical Address 0x4002 4554 Instance 0x4002 4554
Description Crypto Data Length LSW
Type WO
Bits Field Name Description Type Reset
31:0 LEN_LSW Used to write the Length values to the Crypto peripheral.

This register contains bits [31:0] of the combined data length.
WO 0x0000 0000

TOP:CRYPTO:AESDATALEN1

Address Offset 0x0000 0558
Physical Address 0x4002 4558 Instance 0x4002 4558
Description Crypto Data Length MSW
Type WO
Bits Field Name Description Type Reset
31:29 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b000
28:0 LEN_MSW Bits [60:32] of the combined data length.

Bits [60:0] of the crypto length registers AESDATALEN1 and AESDATALEN0 store the cryptographic data length in bytes for all modes. Once processing with this context starts, this length decrements to zero. Data lengths up to (2^61 - 1) bytes are allowed.

A write to this register triggers the engine to start using this context. This is valid for all modes except CCM. For the combined modes (CCM), this length does not include the authentication only data; the authentication length is specified in the AESAUTHLEN.LEN. All modes must have a length > 0. For the combined modes, it is allowed to have one of the lengths equal to zero.

For the basic encryption modes (ECB/CBC/CTR) it is allowed to program zero to the length field; in that case the length is assumed infinite. All data must be byte (8-bit) aligned for stream cipher modes; bit aligned data streams are not supported by the Crypto peripheral. For block cipher modes, the data length must be programmed in multiples of the block cipher size, 16 bytes.
WO 0b0 0000 0000 0000 0000 0000 0000 0000

TOP:CRYPTO:AESAUTHLEN

Address Offset 0x0000 055C
Physical Address 0x4002 455C Instance 0x4002 455C
Description AES Authentication Length
Type WO
Bits Field Name Description Type Reset
31:0 LEN Authentication data length in bytes for combined mode, CCM only.
Supported AAD-lengths for CCM are from 0 to (216 - 28) bytes. Once processing with this context is started, this length decrements to zero.
Writing this register triggers the engine to start using this context for CCM.
WO 0x0000 0000

TOP:CRYPTO:AESDATAOUT0

Address Offset 0x0000 0560
Physical Address 0x4002 4560 Instance 0x4002 4560
Description Data Input/Output
Type RO
Bits Field Name Description Type Reset
31:0 DATA Data register 0 for output block data from the Crypto peripheral.
These bits = AES Output Data[31:0] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host read operation, these registers contain the 128-bit output block from the latest AES operation. Reading from a word-aligned offset within this address range will read one word (4 bytes) of data out the 4-word deep (16 bytes = 128-bits AES block) data output buffer. The words (4 words, one full block) should be read before the core will move the next block to the data output buffer. To empty the data output buffer, AESCTL.OUTPUT_RDY must be written.
For the modes with authentication (CBC-MAC and CCM), the invalid (message) bytes/words can be written with any data.

Note: The AAD / authentication only data is not copied to the output buffer but only used for authentication.
RO 0x0000 0000

TOP:CRYPTO:AESDATAIN0

Address Offset 0x0000 0560
Physical Address 0x4002 4560 Instance 0x4002 4560
Description AES Data Input/Output 0
Type WO
Bits Field Name Description Type Reset
31:0 DATA Data registers for input block data to the Crypto peripheral.
These bits = AES Input Data[31:0] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host write operation, these registers must be written with the 128-bit input block for the next AES operation. Writing at a word-aligned offset within this address range will store the word (4 bytes) of data into the corresponding position of 4-word deep (16 bytes = 128-bit AES block) data input buffer. This buffer is used for the next AES operation. If the last data block is not completely filled with valid data (see notes below), it is allowed to write only the words with valid data. Next AES operation is triggered by writing to AESCTL.INPUT_RDY.

Note: AES typically operates on 128 bits block multiple input data. The CTR and CCM modes form an exception. The last block of a CTR-mode message may contain less than 128 bits (refer to [NIST 800-38A]): 0 < n <= 128 bits. For CCM, the last block of both AAD and message data may contain less than 128 bits (refer to [NIST 800-38D]). The Crypto peripheral automatically pads or masks misaligned ending data blocks with zeroes for CCM and CBC-MAC. For CTR mode, the remaining data in an unaligned data block is ignored.
WO 0x0000 0000

TOP:CRYPTO:AESDATAOUT1

Address Offset 0x0000 0564
Physical Address 0x4002 4564 Instance 0x4002 4564
Description AES Data Input/Output 3
Type RO
Bits Field Name Description Type Reset
31:0 DATA Data registers for output block data from the Crypto peripheral.
These bits = AES Output Data[63:32] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host read operation, these registers contain the 128-bit output block from the latest AES operation. Reading from a word-aligned offset within this address range will read one word (4 bytes) of data out the 4-word deep (16 bytes = 128-bits AES block) data output buffer. The words (4 words, one full block) should be read before the core will move the next block to the data output buffer. To empty the data output buffer, AESCTL.OUTPUT_RDY must be written.
For the modes with authentication (CBC-MAC and CCM), the invalid (message) bytes/words can be written with any data.

Note: The AAD / authentication only data is not copied to the output buffer but only used for authentication.
RO 0x0000 0000

TOP:CRYPTO:AESDATAIN1

Address Offset 0x0000 0564
Physical Address 0x4002 4564 Instance 0x4002 4564
Description AES Data Input/Output 1
Type WO
Bits Field Name Description Type Reset
31:0 DATA Data registers for input block data to the Crypto peripheral.
These bits = AES Input Data[63:32] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host write operation, these registers must be written with the 128-bit input block for the next AES operation. Writing at a word-aligned offset within this address range will store the word (4 bytes) of data into the corresponding position of 4-word deep (16 bytes = 128-bit AES block) data input buffer. This buffer is used for the next AES operation. If the last data block is not completely filled with valid data (see notes below), it is allowed to write only the words with valid data. Next AES operation is triggered by writing to AESCTL.INPUT_RDY.

Note: AES typically operates on 128 bits block multiple input data. The CTR and CCM modes form an exception. The last block of a CTR-mode message may contain less than 128 bits (refer to [NIST 800-38A]): 0 < n <= 128 bits. For CCM, the last block of both AAD and message data may contain less than 128 bits (refer to [NIST 800-38D]). The Crypto peripheral automatically pads or masks misaligned ending data blocks with zeroes for CCM and CBC-MAC. For CTR mode, the remaining data in an unaligned data block is ignored.
WO 0x0000 0000

TOP:CRYPTO:AESDATAOUT2

Address Offset 0x0000 0568
Physical Address 0x4002 4568 Instance 0x4002 4568
Description AES Data Input/Output 2
Type RO
Bits Field Name Description Type Reset
31:0 DATA Data registers for output block data from the Crypto peripheral.
These bits = AES Output Data[95:64] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host read operation, these registers contain the 128-bit output block from the latest AES operation. Reading from a word-aligned offset within this address range will read one word (4 bytes) of data out the 4-word deep (16 bytes = 128-bits AES block) data output buffer. The words (4 words, one full block) should be read before the core will move the next block to the data output buffer. To empty the data output buffer, AESCTL.OUTPUT_RDY must be written.
For the modes with authentication (CBC-MAC and CCM), the invalid (message) bytes/words can be written with any data.

Note: The AAD / authentication only data is not copied to the output buffer but only used for authentication.
RO 0x0000 0000

TOP:CRYPTO:AESDATAIN2

Address Offset 0x0000 0568
Physical Address 0x4002 4568 Instance 0x4002 4568
Description AES Data Input/Output 2
Type WO
Bits Field Name Description Type Reset
31:0 DATA Data registers for input block data to the Crypto peripheral.
These bits = AES Input Data[95:64] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host write operation, these registers must be written with the 128-bit input block for the next AES operation. Writing at a word-aligned offset within this address range will store the word (4 bytes) of data into the corresponding position of 4-word deep (16 bytes = 128-bit AES block) data input buffer. This buffer is used for the next AES operation. If the last data block is not completely filled with valid data (see notes below), it is allowed to write only the words with valid data. Next AES operation is triggered by writing to AESCTL.INPUT_RDY.

Note: AES typically operates on 128 bits block multiple input data. The CTR and CCM modes form an exception. The last block of a CTR-mode message may contain less than 128 bits (refer to [NIST 800-38A]): 0 < n <= 128 bits. For CCM, the last block of both AAD and message data may contain less than 128 bits (refer to [NIST 800-38D]). The Crypto peripheral automatically pads or masks misaligned ending data blocks with zeroes for CCM and CBC-MAC. For CTR mode, the remaining data in an unaligned data block is ignored.
WO 0x0000 0000

TOP:CRYPTO:AESDATAOUT3

Address Offset 0x0000 056C
Physical Address 0x4002 456C Instance 0x4002 456C
Description AES Data Input/Output 3
Type RO
Bits Field Name Description Type Reset
31:0 DATA Data registers for output block data from the Crypto peripheral.
These bits = AES Output Data[127:96] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host read operation, these registers contain the 128-bit output block from the latest AES operation. Reading from a word-aligned offset within this address range will read one word (4 bytes) of data out the 4-word deep (16 bytes = 128-bits AES block) data output buffer. The words (4 words, one full block) should be read before the core will move the next block to the data output buffer. To empty the data output buffer, AESCTL.OUTPUT_RDY must be written.
For the modes with authentication (CBC-MAC and CCM), the invalid (message) bytes/words can be written with any data.

Note: The AAD / authentication only data is not copied to the output buffer but only used for authentication.
RO 0x0000 0000

TOP:CRYPTO:AESDATAIN3

Address Offset 0x0000 056C
Physical Address 0x4002 456C Instance 0x4002 456C
Description Data Input/Output
Type WO
Bits Field Name Description Type Reset
31:0 DATA Data registers for input block data to the Crypto peripheral.
These bits = AES Input Data[127:96] of [127:0]

For normal operations, this register is not used, since data input and output is transferred from and to the AES engine via DMA.

For a Host write operation, these registers must be written with the 128-bit input block for the next AES operation. Writing at a word-aligned offset within this address range will store the word (4 bytes) of data into the corresponding position of 4-word deep (16 bytes = 128-bit AES block) data input buffer. This buffer is used for the next AES operation. If the last data block is not completely filled with valid data (see notes below), it is allowed to write only the words with valid data. Next AES operation is triggered by writing to AESCTL.INPUT_RDY.

Note: AES typically operates on 128 bits block multiple input data. The CTR and CCM modes form an exception. The last block of a CTR-mode message may contain less than 128 bits (refer to [NIST 800-38A]): 0 < n <= 128 bits. For CCM, the last block of both AAD and message data may contain less than 128 bits (refer to [NIST 800-38D]). The Crypto peripheral automatically pads or masks misaligned ending data blocks with zeroes for CCM and CBC-MAC. For CTR mode, the remaining data in an unaligned data block is ignored.
WO 0x0000 0000

TOP:CRYPTO:AESTAGOUT__0-AESTAGOUT__3

Address Offset 0x0000 0570 - 0x0000 057C
Physical Address 0x4002 4570 - 0x4002 457C Instance 0x4002 4570 - 0x4002 457C
Description AES Tag Output
Type RO
Bits Field Name Description Type Reset
31:0 TAG This register contains the authentication TAG for the combined and authentication-only modes. RO 0x0000 0000

TOP:CRYPTO:ALGSEL

Address Offset 0x0000 0700
Physical Address 0x4002 4700 Instance 0x4002 4700
Description Master Algorithm Select
This register configures the internal destination of the DMA controller.
Type RW
Bits Field Name Description Type Reset
31 TAG If this bit is cleared to 0, the DMA operation involves only data.
If this bit is set, the DMA operation includes a TAG (Authentication Result / Digest).
RW 0
30:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b0 0000 0000 0000 0000 0000 0000 0000
1 AES If set to 1, the AES data is loaded via DMA
Both Read and Write maximum transfer size to DMA engine is set to 16 bytes
RW 0
0 KEY_STORE If set to 1, selects the Key Store to be loaded via DMA.
The maximum transfer size to DMA engine is set to 32 bytes (however transfers of 16, 24 and 32 bytes are allowed)
RW 0

TOP:CRYPTO:DMAPROTCTL

Address Offset 0x0000 0704
Physical Address 0x4002 4704 Instance 0x4002 4704
Description Master Protection Control
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b000 0000 0000 0000 0000 0000 0000 0000
0 EN Select AHB transfer protection control for DMA transfers using the key store area as destination.
0 : transfers use 'USER' type access.
1 : transfers use 'PRIVILEGED' type access.
RW 0

TOP:CRYPTO:SWRESET

Address Offset 0x0000 0740
Physical Address 0x4002 4740 Instance 0x4002 4740
Description Software Reset
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b000 0000 0000 0000 0000 0000 0000 0000
0 RESET If this bit is set to 1, the following modules are reset:
- Master control internal state is reset. That includes interrupt, error status register and result available interrupt generation FSM.
- Key store module state is reset. That includes clearing the Written Area flags; therefore the keys must be reloaded to the key store module.
Writing 0 has no effect.
The bit is self cleared after executing the reset.
RW 0

TOP:CRYPTO:IRQTYPE

Address Offset 0x0000 0780
Physical Address 0x4002 4780 Instance 0x4002 4780
Description Control Interrupt Configuration
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b000 0000 0000 0000 0000 0000 0000 0000
0 LEVEL If this bit is 0, the interrupt output is a pulse.
If this bit is set to 1, the interrupt is a level interrupt that must be cleared by writing the interrupt clear register.
This bit is applicable for both interrupt output signals.
RW 0

TOP:CRYPTO:IRQEN

Address Offset 0x0000 0784
Physical Address 0x4002 4784 Instance 0x4002 4784
Description Interrupt Enable
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 0000 0000 0000
1 DMA_IN_DONE This bit enables IRQSTAT.DMA_IN_DONE as source for IRQ. RW 0
0 RESULT_AVAIL This bit enables IRQSTAT.RESULT_AVAIL as source for IRQ. RW 0

TOP:CRYPTO:IRQCLR

Address Offset 0x0000 0788
Physical Address 0x4002 4788 Instance 0x4002 4788
Description Interrupt Clear
Type WO
Bits Field Name Description Type Reset
31 DMA_BUS_ERR If 1 is written to this bit, IRQSTAT.DMA_BUS_ERR is cleared. WO 0
30 KEY_ST_WR_ERR If 1 is written to this bit, IRQSTAT.KEY_ST_WR_ERR is cleared. WO 0
29 KEY_ST_RD_ERR If 1 is written to this bit, IRQSTAT.KEY_ST_RD_ERR is cleared. WO 0
28:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b000 0000 0000 0000 0000 0000 0000
1 DMA_IN_DONE If 1 is written to this bit, IRQSTAT.DMA_IN_DONE is cleared. WO 0
0 RESULT_AVAIL If 1 is written to this bit, IRQSTAT.RESULT_AVAIL is cleared. WO 0

TOP:CRYPTO:IRQSET

Address Offset 0x0000 078C
Physical Address 0x4002 478C Instance 0x4002 478C
Description Interrupt Set
Type WO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b00 0000 0000 0000 0000 0000 0000 0000
1 DMA_IN_DONE If 1 is written to this bit, IRQSTAT.DMA_IN_DONE is set.
Writing 0 has no effect.
WO 0
0 RESULT_AVAIL If 1 is written to this bit, IRQSTAT.RESULT_AVAIL is set.
Writing 0 has no effect.
WO 0

TOP:CRYPTO:IRQSTAT

Address Offset 0x0000 0790
Physical Address 0x4002 4790 Instance 0x4002 4790
Description Interrupt Status
Type RO
Bits Field Name Description Type Reset
31 DMA_BUS_ERR This bit is set when a DMA bus error is detected during a DMA operation. The value of this register is held until it is cleared via IRQCLR.DMA_BUS_ERR
Note: This error is asserted if an error is detected on the AHB master interface during a DMA operation.
Note: This is not an interrupt source.
RO 0
30 KEY_ST_WR_ERR This bit is set when a write error is detected during the DMA write operation to the key store memory. The value of this register is held until it is cleared via IRQCLR.KEY_ST_WR_ERR
Note: This error is asserted if a DMA operation does not cover a full key area or more areas are written than expected.
Note: This is not an interrupt source.
RO 0
29 KEY_ST_RD_ERR This bit will be set when a read error is detected during the read of a key from the key store, while copying it to the AES engine. The value of this register is held until it is cleared via IRQCLR.KEY_ST_RD_ERR.
Note: This error is asserted if a key location is selected in the key store that is not available.
Note: This is not an interrupt source.
RO 0
28:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000
1 DMA_IN_DONE This bit returns the status of DMA data in done interrupt. RO 0
0 RESULT_AVAIL This bit is set high when the Crypto peripheral has a result available. RO 0

TOP:CRYPTO:HWVER

Address Offset 0x0000 07FC
Physical Address 0x4002 47FC Instance 0x4002 47FC
Description CTRL Module Version
Type RO
Bits Field Name Description Type Reset
31:28 RESERVED28 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x9
27:24 HW_MAJOR_VER Major version number RO 0x1
23:20 HW_MINOR_VER Minor version number RO 0x1
19:16 HW_PATCH_LVL Patch level, starts at 0 at first delivery of this version. RO 0x1
15:8 VER_NUM_COMPL These bits simply contain the complement of VER_NUM (0x87), used by a driver to ascertain that the Crypto peripheral register is indeed read. RO 0x87
7:0 VER_NUM The version number for the Crypto peripheral, this field contains the value 120 (decimal) or 0x78. RO 0x78