Instance: AON_PMCTL
Component: AON_PMCTL
Base address: 0x40090000
This component control the Power Management controller residing in the AON domain.
Note: This module is only supporting 32 bit Read Write access from MCU
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4009 0004 |
|
RW |
32 |
0x0001 000F |
0x0000 0008 |
0x4009 0008 |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x4009 0010 |
|
RW |
32 |
0x03C0 0003 |
0x0000 0014 |
0x4009 0014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x4009 0018 |
|
RW |
32 |
0xC000 0000 |
0x0000 001C |
0x4009 001C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x4009 0020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4009 0024 |
|
RW |
32 |
0x0000 01C0 |
0x0000 0028 |
0x4009 0028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4009 002C |
|
RW |
32 |
0x0000 0100 |
0x0000 0034 |
0x4009 0034 |
|
RW |
32 |
0x0B99 A02F |
0x0000 003C |
0x4009 003C |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4009 0004 | Instance | 0x4009 0004 |
Description | AUX SCE Clock Management This register contains bitfields that are relevant for setting up the clock to the AUX domain. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||
8 | PD_SRC | Selects the clock source for the AUX domain when AUX is in powerdown mode. Note: Switching the clock source is guaranteed to be glitch-free
|
RW | 0 | |||||||||||
7:1 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | |||||||||||
0 | SRC | Selects the clock source for the AUX domain when AUX is in active mode. Note: Switching the clock source is guaranteed to be glitch-free
|
RW | 0 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4009 0008 | Instance | 0x4009 0008 |
Description | RAM Configuration This register contains power management related configuration for the SRAM in the MCU and AUX domain. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 | |||||||||||
17 | AUX_SRAM_PWR_OFF | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||
16 | AUX_SRAM_RET_EN | Internal. Only to be used through TI provided API. | RW | 1 | |||||||||||
15:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 | |||||||||||
3:0 | BUS_SRAM_RET_EN | MCU SRAM is partitioned into 1 bank . This register controls whether the bank that has retention during MCU Bus domain power off.
|
RW | 0xF |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x4009 0010 | Instance | 0x4009 0010 |
Description | Power Management Control This register controls bitfields for setting low level power management features such as selection of regulator for VDDR supply and control of IO ring where certain segments can be enabled / disabled. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 0000 0000 0000 0000 0000 | ||
2 | DCDC_ACTIVE | Select to use DCDC regulator for VDDR in active mode 0: Use GLDO for regulation of VDDR in active mode. 1: Use DCDC for regulation of VDDR in active mode. DCDC_EN must also be set for DCDC to be used as regulator for VDDR in active mode |
RW | 0 | ||
1 | EXT_REG_MODE | Status of source for VDDRsupply: 0: DCDC or GLDO are generating VDDR 1: DCDC and GLDO are bypassed and an external regulator supplies VDDR |
RO | 0 | ||
0 | DCDC_EN | Select to use DCDC regulator during recharge of VDDR 0: Use GLDO for recharge of VDDR 1: Use DCDC for recharge of VDDR Note: This bitfield should be set to the same as DCDC_ACTIVE |
RW | 0 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x4009 0014 | Instance | 0x4009 0014 |
Description | AON Power and Reset Status This register is used to monitor various power management related signals in AON. All other signals than JTAG_PD_ON, AUX_BUS_RESET_DONE, and AUX_RESET_DONE are for test, calibration and debug purpose only. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0111 1000 0000 0000 0000 0000 | ||
2 | JTAG_PD_ON | Indicates JTAG power state: 0: JTAG is powered off 1: JTAG is powered on |
RO | 0 | ||
1 | AUX_BUS_RESET_DONE | Indicates Reset Done from AUX Bus: 0: AUX Bus is being reset 1: AUX Bus reset is released |
RO | 1 | ||
0 | AUX_RESET_DONE | Indicates Reset Done from AUX: 0: AUX is being reset 1: AUX reset is released |
RO | 1 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x4009 0018 | Instance | 0x4009 0018 |
Description | Shutdown Control This register contains bitfields required for entering shutdown mode |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | EN | Shutdown control. 0: Do not write 0 to this bit. 1: Immediately start the process to enter shutdown mode |
RW | 0 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x4009 001C | Instance | 0x4009 001C |
Description | Recharge Controller Configuration This register sets all relevant parameters for controlling the recharge algorithm. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:30 | MODE | Selects recharge algorithm for VDDR when the system is running on the uLDO
|
RW | 0b11 | |||||||||||||||||
29:24 | RESERVED24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | |||||||||||||||||
23:20 | C2 | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
19:16 | C1 | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
15:11 | MAX_PER_M | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | |||||||||||||||||
10:8 | MAX_PER_E | Internal. Only to be used through TI provided API. | RW | 0b000 | |||||||||||||||||
7:3 | PER_M | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | |||||||||||||||||
2:0 | PER_E | Internal. Only to be used through TI provided API. | RW | 0b000 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x4009 0020 | Instance | 0x4009 0020 |
Description | Recharge Controller Status This register controls various status registers which are updated during recharge. The register is mostly intended for test and debug. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:20 | RESERVED20 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 | ||
19:16 | VDDR_SMPLS | The last 4 VDDR samples. For each bit: 0: VDDR was below VDDR_OK threshold when recharge started 1: VDDR was above VDDR_OK threshold when recharge started The register is updated prior to every recharge period with a shift left, and bit 0 is updated with the last VDDR sample. |
RO | 0x0 | ||
15:0 | MAX_USED_PER | Shows the maximum number of 32kHz periods that have separated two recharge cycles and VDDR still was above VDDR_OK threshold when the latter recharge started. This register can be used as an indication of the leakage current during standby. This bitfield is cleared to 0 when writing this register. |
RW | 0x0000 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x4009 0024 | Instance | 0x4009 0024 |
Description | Oscillator Configuration This register sets the period for Amplitude compensation requests sent to the oscillator control system. The amplitude compensations is only applicable when XOSC_HF is running in low power mode. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:3 | PER_M | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
2:0 | PER_E | Internal. Only to be used through TI provided API. | RW | 0b000 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x4009 0028 | Instance | 0x4009 0028 |
Description | Reset Management This register contains bitfields related to system reset such as reset source and reset request and control of brown out resets. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||
31 | SYSRESET | Cold reset register. Writing 1 to this bitfield will reset the entire chip and cause boot code to run again. 0: No effect 1: Generate system reset. Appears as SYSRESET in RESET_SRC |
WO | 0 | ||||||||||||||||||||||||||
30:26 | RESERVED26 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | ||||||||||||||||||||||||||
25 | BOOT_DET_1_CLR | Internal. Only to be used through TI provided API. | WO | 0 | ||||||||||||||||||||||||||
24 | BOOT_DET_0_CLR | Internal. Only to be used through TI provided API. | WO | 0 | ||||||||||||||||||||||||||
23:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | ||||||||||||||||||||||||||
17 | BOOT_DET_1_SET | Internal. Only to be used through TI provided API. | WO | 0 | ||||||||||||||||||||||||||
16 | BOOT_DET_0_SET | Internal. Only to be used through TI provided API. | WO | 0 | ||||||||||||||||||||||||||
15 | WU_FROM_SD | A Wakeup from SHUTDOWN on an IO event has occurred, or a wakeup from SHUTDOWN has occurred as a result of the debugger being attached.. (TCK pin being forced low) Please refer to IOC:IOCFGn.WU_CFG for configuring the IO's as wakeup sources. 0: Wakeup occurred from cold reset or brown out as seen in RESET_SRC 1: A wakeup has occurred from SHUTDOWN Note: This flag will be cleared when SLEEPCTL.IO_PAD_SLEEP_DIS is asserted. |
RO | 0 | ||||||||||||||||||||||||||
14 | GPIO_WU_FROM_SD | A wakeup from SHUTDOWN on an IO event has occurred Please refer to IOC:IOCFGn.WU_CFG for configuring the IO's as wakeup sources. 0: The wakeup did not occur from SHUTDOWN on an IO event 1: A wakeup from SHUTDOWN occurred from an IO event The case where WU_FROM_SD is asserted but this bitfield is not asserted will only occur in a debug session. The boot code will not proceed with wakeup from SHUTDOWN procedure until this bitfield is asserted as well. Note: This flag will be cleared when SLEEPCTL.IO_PAD_SLEEP_DIS is asserted. |
RO | 0 | ||||||||||||||||||||||||||
13 | BOOT_DET_1 | Internal. Only to be used through TI provided API. | RO | 0 | ||||||||||||||||||||||||||
12 | BOOT_DET_0 | Internal. Only to be used through TI provided API. | RO | 0 | ||||||||||||||||||||||||||
11:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 | ||||||||||||||||||||||||||
8 | VDDS_LOSS_EN | Controls reset generation in case VDDS is lost 0: Brown out detect of VDDS is ignored, unless VDDS_LOSS_EN_OVR=1 1: Brown out detect of VDDS generates system reset |
RW | 1 | ||||||||||||||||||||||||||
7 | VDDR_LOSS_EN | Controls reset generation in case VDDR is lost 0: Brown out detect of VDDR is ignored, unless VDDR_LOSS_EN_OVR=1 1: Brown out detect of VDDR generates system reset |
RW | 1 | ||||||||||||||||||||||||||
6 | VDD_LOSS_EN | Controls reset generation in case VDD is lost 0: Brown out detect of VDD is ignored, unless VDD_LOSS_EN_OVR=1 1: Brown out detect of VDD generates system reset |
RW | 1 | ||||||||||||||||||||||||||
5 | CLK_LOSS_EN | Controls reset generation in case SCLK_LF, SCLK_MF or SCLK_HF is lost when clock loss detection is enabled by [ANATOP_MMAP:DDI_0_OSC:CTL0.CLK_LOSS_EN] 0: Clock loss is ignored 1: Clock loss generates system reset Note: Clock loss reset generation must be disabled when changing clock source for SCLK_LF. Failure to do so may result in a spurious system reset. Clock loss reset generation is controlled by [ANATOP_MMAP:DDI_0_OSC:CTL0.CLK_LOSS_EN] |
RW | 0 | ||||||||||||||||||||||||||
4 | MCU_WARM_RESET | Internal. Only to be used through TI provided API. | RW | 0 | ||||||||||||||||||||||||||
3:1 | RESET_SRC | Shows the root cause of the last system reset. More than the reported reset source can have been active during the last system reset but only the root cause is reported. The capture feature is not rearmed until all off the possible reset sources have been released and the result has been copied to AON_PMCTL. During the copy and rearm process it is one 2MHz period in which and eventual new system reset will be reported as Power on reset regardless of the root cause.
|
RO | 0b000 | ||||||||||||||||||||||||||
0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x4009 002C | Instance | 0x4009 002C |
Description | Sleep Control This register is used to unfreeze the IO pad ring after waking up from SHUTDOWN |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | IO_PAD_SLEEP_DIS | Controls the I/O pad sleep mode. The boot code will set this bitfield automatically unless waking up from a SHUTDOWN ( RESETCTL.WU_FROM_SD is set). 0: I/O pad sleep mode is enabled, meaning all outputs and pad configurations are latched. Inputs are transparent if pad is configured as input before IO_PAD_SLEEP_DIS is set to 1 1: I/O pad sleep mode is disabled Application software must reconfigure the state for all IO's before setting this bitfield upon waking up from a SHUTDOWN to avoid glitches on pins. |
RW | 0 |
Address Offset | 0x0000 0034 | ||
Physical Address | 0x4009 0034 | Instance | 0x4009 0034 |
Description | JTAG Configuration This register contains control for configuration of the JTAG domain. This includes permissions for each TAP. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | ||
8 | JTAG_PD_FORCE_ON | Controls JTAG Power domain power state: 0: Controlled exclusively by debug subsystem. (JTAG Power domain will be powered off unless a debugger is attached) 1: JTAG Power Domain is forced on, independent of debug subsystem. Note: The reset value causes JTAG Power domain to be powered on by default. Software must clear this bit to turn off the JTAG Power domain |
RW | 1 | ||
7:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 |
Address Offset | 0x0000 003C | ||
Physical Address | 0x4009 003C | Instance | 0x4009 003C |
Description | JTAG USERCODE Boot code copies the JTAG USERCODE to this register from where it is forwarded to the debug subsystem. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:0 | USER_CODE | 32-bit JTAG USERCODE register feeding main JTAG TAP Note: This field can be locked by LOCKCFG.LOCK |
RW | 0x0B99 A02F |
© 2015 - 2016. Texas Instruments | All Rights Reserved |