| BLE_AGAMA-4033 |
Compilation with TICLANG compiler fails if a BLE5Stack API function is called without argument |
| BLE_AGAMA-4029 |
Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set. |
| BLE_AGAMA-4009 |
[RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands |
| BLE_AGAMA-3896 |
[RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands |
| BLE_AGAMA-3862 |
Stack TX queue becomes corrupted in very rare instance and stack becomes unresponsive during GATT write char operation |
| BLE_AGAMA-3774 |
Under certain conditions the CC2652R1 failed to synchronize to periodic advertising |
| BLE_AGAMA-3752 |
[CC2651] Host_test memory limitation using CCS+TI-CLANG |
| BLE_AGAMA-3747 |
[MESH][AE][eRPC] ~100% missing packets more than 3 hops while GATT Bearer is enabled |
| BLE_AGAMA-3606 |
[Mesh][Stability] Messages might stop after ~3 hours in a network with more than ~20 nodes |
| BLE_AGAMA-3597 |
[Mesh] LPN might fail to maintain friendship with ble.scanLatency < 10, when Display module is enabled |
| BLE_AGAMA-3556 |
[Mesh][IOP] LPN fails to configure after provisioning over PB-GATT with BlueZ |
| BLE_AGAMA-3543 |
[Build] Simple Mesh and Peripheral OAD onchip example fail to compile with GATT Bearer for CCS/TICLANG due to memory limitation |
| BLE_AGAMA-3540 |
[RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC |
| BLE_AGAMA-3486 |
Device asserts upon connection when HeapMem and HeapTrack is used |
| BLE_AGAMA-3427 |
System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued |
| BLE_AGAMA-3391 |
[Mesh][eRPC] Limitation - Mesh node with eRPC unable to transmit messages > 221B |
| BLE_AGAMA-3388 |
[Mesh] Relay fails to transmit segmented message without re-transmission (relay re-transmit = 0) |
| BLE_AGAMA-3383 |
Mesh stack delay work API is limited to a maximum delay of uint32 maximum value (42,949,672 milliseconds) |
| BLE_AGAMA-3381 |
Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration |
| BLE_AGAMA-3169 |
Connecting twice to the same device causing wrong count of connections and a memory leakage |
| BLE_AGAMA-3107 |
[CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms |
| BLE_AGAMA-3077 |
[RTLS] CTE reception on the 2M PHY do not meet spec requirements |
| BLE_AGAMA-3076 |
[RTLS] CTEs sent on the 2M PHY do not meet spec requirements |
| BLE_AGAMA-3024 |
[MESH] [IOP] Mesh DUT is not publishing its mesh supported roles (Unable to config Mesh node) with iPhone |
| BLE_AGAMA-2266 |
Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
| BLE_AGAMA-2033 |
[RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
| BLE_AGAMA-2010 |
[Multi-Sensor] Updating Report Interval Have no effect |
| BLE_AGAMA-1675 |
IOP: Device fails to pair with Meizu Pro 7 |
| BLE_AGAMA-1435 |
[Multi-Sensor] Accelerometer Service Disappears After First Connection |
| BLE_AGAMA-139 |
When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
| BLE_AGAMA-80 |
The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |