References¶
TI-RTOS7 Kernel (SYS/BIOS) API Reference
TI 15.4-Stack CoP Interface Guide
Arm Cortex-M3 Devices Generic User’s Guide
Terms and Acronyms¶
TI 15.4-Stack Terms and Acronyms¶
- AES¶
- Advanced Encryption Standard¶
A fast and secure form of encryption.
- AES-CCM¶
- AES Counter with CBC-MAC.¶
It is an authenticated encryption algorithm
- AES-CMAC¶
AES Cipher-based Message Authentication Code.
- CAP¶
- Contention Assessment Period¶
Part of the beacon mode superframe. During CAP a slotted CSMA-CA mechanism is used ad any node can transmit a beacon.
- CBC-MAC¶
Cipher Block Chaining Message Authentication Code.
- CBKE¶
Certificate-Based Key Establishment.
- CCFG¶
- Customer Configuration Area.¶
- Customer Configuration¶
Customer Configuration is set by the application and contains configuration parameters for the ROM boot code, device hardware, and device firmware. It contains lock-bits on the last page of flash. You can read more in the Customer Configuration section in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- CCS¶
- Code Composer Studio¶
An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio
- CFP¶
- Contention Free Period¶
Optional part of the beacon mode superframe. If the network requires certain nodes to transmit frequently, they can be assigned a slot in the CFP where they are the only node to transmit.
- CLI¶
Command Line Interface.
- CSMA-CA¶
- Carrier Sense Multiple Access with Collision Avoidance¶
This prevents nodes from talking while the air is occupied. Used in all bands except 868MHz.
- CSRK¶
Connection Signature Resolving Key.
- DFE¶
Direct Frame Exchange.
- DH1CF¶
- Direct Hash Channel Function¶
This is used to produce a psuedo-random channel sequence for frequency hopping devices.
- ECDH¶
Elliptic Curve Diffie-Hellman.
- ECHDE¶
Elliptic Curve Diffie-Hellman Ephemeral.
- ECJPAKE¶
Elliptic Curve J-PAKE.
- FAN¶
Field Area Network.
- FFD¶
Full Functionality Device.
- GCC¶
- GNU Compiler Collection¶
A compiler system produced by the GNU Project, which support various programming languages such as C and C++.
- GUI¶
Graphical User Interface.
- HIB¶
- Halt In Boot¶
A mechanism in CC13xx or CC26xx to ensure that the external emulator can take control of the device before it executes any application code.
- HMAC¶
Hash-based message authentication code.
- IAR¶
Refers to IAR Systems’ IAR Embedded Workbench, which is an integrated development environment used for building and debugging embedded applications.
- IDE¶
Integrated Development Environment.
- IEEE¶
- Institute of Electrical and Electronics Engineers¶
An organization composed of engineers, scientists, and students. Develops standards for the computer and electronics industry.
- IRK¶
Identity Resolving Key.
- J-PAKE¶
Password Authenticated Key Exchange by Juggling.
- LBT¶
- Listen Before Talk¶
This prevents nodes from talking while the air is occupied. Used in 868MHz band.
- MAC¶
Medium Access Control.
- MCU¶
- Microcontroller Unit¶
A small computer on a single integrated circuit.
- MIC¶
Message Integrity Code.
- MITM¶
Man In The Middle.
- MMO¶
Matyas-Meyer-Oseas.
- NV¶
- Non-Volatile Storage¶
Storage of data in non-volatile memory (NVM). NVM retains saved data during power cycles. In the context of CC13xx or CC26xx, NVM either refers to the internal flash or some external flash.
- OOB¶
Out-Of-Box.
- OSI¶
Open Systems Interconnection model.
- PAN¶
Personal Area Network.
- PBKDF2¶
Password-Based Key Derivation Function 2.
- PHY¶
- Physical layer¶
The physical layer is the lowest layer of the TI 15.4-Stack It configures the physical parameters of the radio transmission and reception. It determines how a bit (and its value) are represented over the air.
- PIB¶
Personal-Area-Network Information Bases.
- RAM¶
Random Access Memory.
- RCFG¶
- ROM Configuration¶
TI-RTOS in ROM Configuration Table
- RNG¶
Random Number Generator.
- RF¶
Radio Frequency.
- RFD¶
Reduced Functionality Device.
- ROM¶
- Read-only Memory¶
Type of non-volatile memory used in computers. Once data is written to ROM, the data cannot be removed and can only be read.
- RTOS¶
- Real Time Operating System¶
An operating system intended to serve applications with real-time requirements.
- SKKE¶
Symmetric-Key Key Establishment.
- SNV¶
- Simple Non Volatile¶
An abstraction layer used by the TI 15.4-Stack for reading and writing to non volatile memory. This region can also be used by the user.
- SUN¶
Smart Utility Network.
- TRNG¶
True Random Number Generator.
- VIMS¶
- Versatile Instruction Memory System¶
A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
Sensor Controller Terms and Acronyms¶
- SC¶
- Sensor Controller¶
A dedicated 16-bit CPU core on CC13xx and CC26xx devices, located in the auxiliary (AUX) power/clock domain. It can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power states.
- SCS¶
- Sensor Controller Studio¶
A stand-alone IDE used to write, test and debug code for the Sensor Controller.
TI-RTOS7 Terms and Acronyms¶
- HWI¶
- Hardware Interrupts¶
A TI-RTOS7 hardware interrupt.
- Idle Task¶
A TI-RTOS7 default task that is executes when no other higher priority thread needs to run.
- ROV¶
- Runtime Object View¶
A TI-RTOS7 kernel plugin for CCS and IAR to view a target’s instrumentation data.
- RTC¶
- Real-Time Clock¶
An accurate computer clock which keeps track of the current time.
- RTOS¶
- Real Time Operating System¶
An operating system intended to serve applications with real-time requirements.
- SWI¶
- Software Interrupts¶
A TI-RTOS7 software interrupt.
- TI-RTOS7¶
- Texas Instruments Real Time Operating System¶
An RTOS developed by TI for TI microcontrollers.
- Zero-Latency Interrupts¶
An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see the Hwi module documentation in the TI-RTOS7 Kernel (SYS/BIOS) User’s Guide.
Over-the-Air Download (OAD) Terms and Acronyms¶
- BIM¶
- Boot Image Manager¶
A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
- CRC¶
- Cyclic Redundancy Check¶
An error-detecting code used to check the integrity of blocks of data.
- ECDSA¶
- Elliptic Curve Digital Signature Algorithm¶
A variant of the Digital Signature Algorithm (DSA) which uses elliptic curve cryptography.
- Factory Image¶
The factory image is a “golden” image that resides in external flash as a fail-safe mechanism.
- HIB¶
- Halt In Boot¶
A mechanism in CC13xx or CC26xx to ensure that the external emulator can take control of the device before it executes any application code.
- OAD¶
- Over-the-Air Download¶
The process of performing a device firmware update over the air.
- OAD Target¶
The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx or CC13xx device running the TI protocol-specific transport for OAD.
- OAD Distributor¶
The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.
General Terms and Acronyms¶
- CCFG¶
- Customer Configuration¶
Customer Configuration is set by the application and contains configuration parameters for the ROM boot code, device hardware, and device firmware. It contains lock-bits on the last page of flash. You can read more in the Customer Configuration section in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- CCS¶
- Code Composer Studio¶
An integrated development environment to develop applications for Texas Instruments embedded processors. Download: Code Composer Studio
- cJTAG¶
- compact JTAG¶
Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG.
- GCC¶
- GNU Compiler Collection¶
A compiler system produced by the GNU Project, which support various programming languages such as C and C++.
- GPRAM¶
- General purpose RAM¶
This memory area is used for the cache per default, but can be configured to be used as RAM.
- IAR¶
Refers to IAR Systems’ IAR Embedded Workbench, which is an integrated development environment used for building and debugging embedded applications.
- JTAG¶
- Joint Test Action Group¶
IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG.
- MCU¶
- Microcontroller Unit¶
A small computer on a single integrated circuit.
- NVS¶
- Non-Volatile Storage¶
Storage of data in non-volatile memory (NVM). NVM retains saved data during power cycles. In the context of CC13xx and CC26xx devices, NVM either refers to the internal flash or some external flash.
- ROM¶
- Read-only Memory¶
Type of non-volatile memory used in computers. Once data is written to ROM, the data cannot be removed and can only be read.
- RTSC¶
- Real Time Software Components¶
A toolset for creating reusable code, used by TI-RTOS. See RTSC and RTSC-Pedia.
- SysConfig¶
- System Configuration Tool¶
SysConfig is a graphical interface for configuring software projects. Configuration files, C source files and header files are generated based on the parameters configured in the SysConfig dashboard. See Get started with SysConfig.
- TI-CLANG¶
- TI Arm Clang Compiler Toolchain¶
The TI Arm Clang Compiler Toolchain (tiarmclang) is the next generation TI Arm compiler, replacing the previous TI Arm Compiler Tools (armcl). You can use the tiarmclang compiler toolchain to build applications from C, C++, and/or assembly source files to be loaded and run on one of the Cortex-M or Cortex-R Arm processors that are supported by the toolchain. You can find more information here.
- VIMS¶
- Versatile Instruction Memory System¶
A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
- .bss¶
Block started by symbol. This memory section usually contains uninitialized variables including the task stacks.