SimpleLink Common Commponents Module 4.30.00 Release Notes
Table of Contents
Introduction
The SimpleLink Common Components Module (SCCM) includes Common User Interface (CUI), NV Interface (Non-volatile Memory Interface), Boot Image Manager (BIM) on- and off-chip, and Universal Network Processor Interface (UNPI). These release notes include bug fixes, updates, and new features for the SCCM components.
Documentation
The follow table details which SCCM components are supported by the different SimpleLink stacks
Stack | CUI | NV | BIM on-chip | BIM off-chip | UNPI |
---|---|---|---|---|---|
BLE | X | X | X | X | |
15.4 | X | X | X | X | |
Zigbee | X | X | X | ||
Thread | X | X | X | ||
DMM | X | X | X | ||
WiSUN | X | ||||
PropRF | X | X | X |
What’s New
ID | Summary |
---|---|
SCCM-215 | Add MCUBoot support for CC13x4/CC26x4 (on-chip & off-chip) |
SCCM-209 | Add BIM support for the CC1312PSIP |
SCCM-201 | Enable MCUBoot example generation for CC13x2/26x2 R7 devices |
SCCM-170 | Provide an interface to report that there was an error with NV driver operation |
Fixed Issues
ID | Summary |
---|---|
None | None |
Known Issues and Limitations
ID | Summary |
---|---|
None | None |
It should be noted that multiple external NVS regions are not supported. If a user attempts to create a second external NVS region, all actions on the second region will be done on the first region.
Upgrade and Compatibility Information
Dependencies
SCCM components were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.