679 #ifndef ti_drivers_spi_SPICC26X2DMA__include 680 #define ti_drivers_spi_SPICC26X2DMA__include 688 #include <ti/drivers/dpl/HwiP.h> 689 #include <ti/drivers/dpl/SemaphoreP.h> 690 #include <ti/drivers/dpl/SwiP.h> 728 #define SPICC26X2DMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 737 #define SPICC26X2DMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 750 #define SPICC26X2DMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 761 #define SPICC26X2DMA_CMD_CLEAR_CSN_PIN (SPI_CMD_RESERVED + 3) 776 #define SPICC26X2DMA_CMD_SET_MANUAL (SPI_CMD_RESERVED + 4) 787 #define SPICC26X2DMA_CMD_CLR_MANUAL (SPI_CMD_RESERVED + 5) 799 #define SPICC26X2DMA_CMD_MANUAL_START (SPI_CMD_RESERVED + 6) 804 #define SPICC26X2DMA_RETURN_PARTIAL_ENABLE SPICC26X2DMA_CMD_RETURN_PARTIAL_ENABLE 805 #define SPICC26X2DMA_RETURN_PARTIAL_DISABLE SPICC26X2DMA_CMD_RETURN_PARTIAL_DISABLE 806 #define SPICC26X2DMA_SET_CSN_PIN SPICC26X2DMA_CMD_SET_CSN_PIN Definition: SPICC26X2DMA.h:842
uint_least8_t csnPin
Definition: SPICC26X2DMA.h:999
uint16_t defaultTxBufValue
Definition: SPICC26X2DMA.h:930
uint32_t minDmaTransferSize
Definition: SPICC26X2DMA.h:961
SPI_Transaction * headPtr
Definition: SPICC26X2DMA.h:977
Serial Peripheral Interface (SPI) Driver Interface.
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:586
uint32_t txChannelBitMask
Definition: SPICC26X2DMA.h:934
SPI_Transaction * completedTransfers
Definition: SPICC26X2DMA.h:979
uint32_t bitRate
Definition: SPICC26X2DMA.h:988
uint_least8_t misoPin
Definition: SPICC26X2DMA.h:954
uint32_t rxChannelBitMask
Definition: SPICC26X2DMA.h:932
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:623
SPI_Transaction * tailPtr
Definition: SPICC26X2DMA.h:978
uint_least8_t clkPin
Definition: SPICC26X2DMA.h:956
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:252
Power manager interface for CC26XX/CC13XX.
int32_t rxPinMux
Definition: SPICC26X2DMA.h:946
Power_NotifyObj spiPostObj
Definition: SPICC26X2DMA.h:972
uint16_t rxScratchBuf
Definition: SPICC26X2DMA.h:993
uint32_t transferTimeout
Definition: SPICC26X2DMA.h:990
volatile tDMAControlTable * dmaTxTableEntryAlt
Definition: SPICC26X2DMA.h:940
uint32_t activeChannel
Definition: SPICC26X2DMA.h:987
volatile tDMAControlTable * dmaRxTableEntryAlt
Definition: SPICC26X2DMA.h:942
size_t altTransferSize
Definition: SPICC26X2DMA.h:985
SPI_Mode mode
Definition: SPICC26X2DMA.h:997
uint8_t intNum
Definition: SPICC26X2DMA.h:904
SPI_TransferMode transferMode
Definition: SPICC26X2DMA.h:996
const SPI_FxnTable SPICC26X2DMA_fxnTable
Definition: SPICC26X2DMA.h:827
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:712
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26X2DMA.h:926
SPICC26X2DMA_ReturnPartial returnPartial
Definition: SPICC26X2DMA.h:1000
size_t framesQueued
Definition: SPICC26X2DMA.h:982
SPICC26X2DMA Hardware attributes.
Definition: SPICC26X2DMA.h:899
uint8_t format
Definition: SPICC26X2DMA.h:998
SwiP_Struct swi
Definition: SPICC26X2DMA.h:973
volatile tDMAControlTable * dmaRxTableEntryPri
Definition: SPICC26X2DMA.h:938
volatile tDMAControlTable * dmaTxTableEntryPri
Definition: SPICC26X2DMA.h:936
UDMACC26XX driver implementation.
uint32_t busyBit
Definition: SPICC26X2DMA.h:991
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:564
Power notify object structure.
Definition: Power.h:442
Definition: SPICC26X2DMA.h:840
SPI_Mode
Definitions for various SPI modes of operation.
Definition: SPI.h:591
UDMACC26XX_Handle udmaHandle
Definition: SPICC26X2DMA.h:980
SemaphoreP_Struct transferComplete
Definition: SPICC26X2DMA.h:974
SPICC26X2DMA_ReturnPartial
Definition: SPICC26X2DMA.h:838
int32_t clkPinMux
Definition: SPICC26X2DMA.h:948
uint_least8_t mosiPin
Definition: SPICC26X2DMA.h:952
uint_least8_t csnPin
Definition: SPICC26X2DMA.h:958
Definition: SPICC26X2DMA.h:828
size_t framesTransferred
Definition: SPICC26X2DMA.h:983
uint16_t txScratchBuf
Definition: SPICC26X2DMA.h:994
SPICC26X2DMA_FrameSize
Definition: SPICC26X2DMA.h:825
int32_t csnPinMux
Definition: SPICC26X2DMA.h:950
size_t priTransferSize
Definition: SPICC26X2DMA.h:984
int32_t txPinMux
Definition: SPICC26X2DMA.h:944
bool manualStart
Definition: SPICC26X2DMA.h:1002
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26X2DMA.h:976
bool isOpen
Definition: SPICC26X2DMA.h:1001
PowerCC26XX_Resource powerMngrId
Definition: SPICC26X2DMA.h:928
SPICC26X2DMA Object.
Definition: SPICC26X2DMA.h:969
Definition: SPICC26X2DMA.h:841
HwiP_Struct hwi
Definition: SPICC26X2DMA.h:971
uint32_t dataSize
Definition: SPICC26X2DMA.h:989
uint8_t intPriority
SPI CC26XXDMA Peripheral's interrupt priority.
Definition: SPICC26X2DMA.h:919
uint32_t baseAddr
SPI Peripheral's base address.
Definition: SPICC26X2DMA.h:902